<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic iMX6 Camera Parallel Interface - BT1120  in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-Camera-Parallel-Interface-BT1120/m-p/508913#M82866</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I need to read frames from a camera connected to the camera parallel interface of an imx6.&lt;/P&gt;&lt;P&gt;The camera begins to write full hd progressive frames to the parallel interface following the bt1120 standard as soon as the board boots.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've started to study some v4l2 tutorials and to look for some examples, but I have no experience at all in writing drivers. &lt;/P&gt;&lt;P&gt;I write to ask some help :smileyhappy: A few hints or pointers to useful documentation or a driver I can use as a starting point would be greatly appreciated!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 09 May 2016 16:15:05 GMT</pubDate>
    <dc:creator>lucazini</dc:creator>
    <dc:date>2016-05-09T16:15:05Z</dc:date>
    <item>
      <title>iMX6 Camera Parallel Interface - BT1120</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-Camera-Parallel-Interface-BT1120/m-p/508913#M82866</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I need to read frames from a camera connected to the camera parallel interface of an imx6.&lt;/P&gt;&lt;P&gt;The camera begins to write full hd progressive frames to the parallel interface following the bt1120 standard as soon as the board boots.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've started to study some v4l2 tutorials and to look for some examples, but I have no experience at all in writing drivers. &lt;/P&gt;&lt;P&gt;I write to ask some help :smileyhappy: A few hints or pointers to useful documentation or a driver I can use as a starting point would be greatly appreciated!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 May 2016 16:15:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-Camera-Parallel-Interface-BT1120/m-p/508913#M82866</guid>
      <dc:creator>lucazini</dc:creator>
      <dc:date>2016-05-09T16:15:05Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 Camera Parallel Interface - BT1120</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-Camera-Parallel-Interface-BT1120/m-p/508914#M82867</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;for bt1120 inprogressive mode, you can refer to the link as below, hope helpful for you.&lt;/P&gt;&lt;P&gt;&amp;lt;&lt;A href="https://community.nxp.com/thread/314211"&gt;Support BT1120 progressive mode in Mx6Q&lt;/A&gt; &amp;gt;.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 May 2016 08:02:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-Camera-Parallel-Interface-BT1120/m-p/508914#M82867</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2016-05-12T08:02:18Z</dc:date>
    </item>
  </channel>
</rss>