<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Is there source code for communication between i.MX6SX dual ENETs. in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Is-there-source-code-for-communication-between-i-MX6SX-dual/m-p/508743#M82846</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a question about i.MX6SX ENET.&lt;/P&gt;&lt;P&gt;I want to know whether Linux BSP for i.MX6SX (L3.14.38) provide the source codes for TCP or UDP communication between 2 ENETs.&lt;/P&gt;&lt;P&gt;(e.g. transmit/receive a packet, bridge, routing, etc..)&lt;/P&gt;&lt;P&gt;I did not find these desription in Linux BSP release not for L3.14.38, so I belive thease are not provided.&lt;/P&gt;&lt;P&gt;Is my understanding correct?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Satoshi Shimoda&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 28 Dec 2015 09:39:52 GMT</pubDate>
    <dc:creator>satoshishimoda</dc:creator>
    <dc:date>2015-12-28T09:39:52Z</dc:date>
    <item>
      <title>Is there source code for communication between i.MX6SX dual ENETs.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-there-source-code-for-communication-between-i-MX6SX-dual/m-p/508743#M82846</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a question about i.MX6SX ENET.&lt;/P&gt;&lt;P&gt;I want to know whether Linux BSP for i.MX6SX (L3.14.38) provide the source codes for TCP or UDP communication between 2 ENETs.&lt;/P&gt;&lt;P&gt;(e.g. transmit/receive a packet, bridge, routing, etc..)&lt;/P&gt;&lt;P&gt;I did not find these desription in Linux BSP release not for L3.14.38, so I belive thease are not provided.&lt;/P&gt;&lt;P&gt;Is my understanding correct?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Satoshi Shimoda&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Dec 2015 09:39:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-there-source-code-for-communication-between-i-MX6SX-dual/m-p/508743#M82846</guid>
      <dc:creator>satoshishimoda</dc:creator>
      <dc:date>2015-12-28T09:39:52Z</dc:date>
    </item>
    <item>
      <title>Re: Is there source code for communication between i.MX6SX dual ENETs.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-there-source-code-for-communication-between-i-MX6SX-dual/m-p/508744#M82847</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The BSP itself only provides a low-level hardware drivers for Etrhernet interfaces. All higher level tasks, such as packets routing, interfaces bridging etc. are done by a higher level software tools that are not hardware specific, but are the parts or applications for the Linux OS itself. For example:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://www.cyberciti.biz/faq/debian-network-interfaces-bridge-eth0-eth1-eth2/" rel="nofollow"&gt;http://www.cyberciti.biz/faq/debian-network-interfaces-bridge-eth0-eth1-eth2/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Dec 2015 11:57:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-there-source-code-for-communication-between-i-MX6SX-dual/m-p/508744#M82847</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2015-12-28T11:57:51Z</dc:date>
    </item>
  </channel>
</rss>