<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MQS example schematic in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MQS-example-schematic/m-p/508328#M82793</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: Arial;"&gt;&amp;nbsp; The i.MX6UL&amp;nbsp; MQS is used to generate medium quality audio via standard GPIO&lt;BR /&gt;and produces PWM signal, fixed in amplitude and frequence, but varying in &lt;BR /&gt;duty cycle. So additional RC filter is needed at output, this will produce &lt;BR /&gt;medium quality sound without an additional DAC.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 11 Mar 2016 06:57:10 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2016-03-11T06:57:10Z</dc:date>
    <item>
      <title>MQS example schematic</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MQS-example-schematic/m-p/508326#M82791</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Are there an example schematics for i.MX6UL MQS (Medium quality sound)?&amp;nbsp; Is this really as simple as connecting the output directly to an audio amp?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, is there a linux driver available for MQS?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Cliff&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Mar 2016 19:30:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MQS-example-schematic/m-p/508326#M82791</guid>
      <dc:creator>cbrake</dc:creator>
      <dc:date>2016-03-04T19:30:59Z</dc:date>
    </item>
    <item>
      <title>Re: MQS example schematic</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MQS-example-schematic/m-p/508327#M82792</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;No. We have no such schematic example.&lt;/P&gt;&lt;P&gt;You are supposed to create a schematic yourself.&lt;/P&gt;&lt;P&gt;Sorry for the inconvenience.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i.MX6UL processor have such interface: MQS_LEFT and MQS_RIGHT pins.&lt;/P&gt;&lt;P&gt;They are PWM encoded. So you can connect audio amplifier to them with a filter.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Mar 2016 03:22:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MQS-example-schematic/m-p/508327#M82792</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2016-03-11T03:22:56Z</dc:date>
    </item>
    <item>
      <title>Re: MQS example schematic</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MQS-example-schematic/m-p/508328#M82793</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: Arial;"&gt;&amp;nbsp; The i.MX6UL&amp;nbsp; MQS is used to generate medium quality audio via standard GPIO&lt;BR /&gt;and produces PWM signal, fixed in amplitude and frequence, but varying in &lt;BR /&gt;duty cycle. So additional RC filter is needed at output, this will produce &lt;BR /&gt;medium quality sound without an additional DAC.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Mar 2016 06:57:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MQS-example-schematic/m-p/508328#M82793</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-03-11T06:57:10Z</dc:date>
    </item>
  </channel>
</rss>