<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Imx6ul deploy folder files deleted in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Imx6ul-deploy-folder-files-deleted/m-p/508148#M82759</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using imx6ul eval board. I followed the "yocto project user guide" to create the images. but few files are deleted from ~/tmp/delpoy/images/imx6ulevk" folder. when i try to recreate the images i am getting the following error.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;WARNING: log_check: There is a warn message in the logfile&lt;/P&gt;&lt;P&gt;WARNING: log_check: Matched keyword: [WARNING:]&lt;/P&gt;&lt;P&gt;WARNING: log_check: WARNING: The license listed Firmware-atheros_firmware was not in the licenses collected for linux-firmware&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ERROR: Error: The image creation script '/home/srinivasulu/Freescale_BSP/Build/tmp/work/imx6ulevk-poky-linux-gnueabi/core-image-base/1.0-r0/temp/create_image.sdcard' returned 1:&lt;/P&gt;&lt;P&gt;0+0 records in&lt;/P&gt;&lt;P&gt;0+0 records out&lt;/P&gt;&lt;P&gt;0 bytes (0 B) copied, 7.8307e-05 s, 0.0 kB/s&lt;/P&gt;&lt;P&gt;Model:&amp;nbsp; (file)&lt;/P&gt;&lt;P&gt;Disk /home/srinivasulu/Freescale_BSP/Build/tmp/deploy/images/imx6ulevk/core-image-base-imx6ulevk-20151228075336.rootfs.sdcard: 88.1MB&lt;/P&gt;&lt;P&gt;Sector size (logical/physical): 512B/512B&lt;/P&gt;&lt;P&gt;Partition Table: msdos&lt;/P&gt;&lt;P&gt;Disk Flags: &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Number&amp;nbsp; Start&amp;nbsp;&amp;nbsp; End&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Size&amp;nbsp;&amp;nbsp;&amp;nbsp; Type&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; File system&amp;nbsp; Flags&lt;/P&gt;&lt;P&gt; 1&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 4194kB&amp;nbsp; 12.6MB&amp;nbsp; 8389kB&amp;nbsp; primary&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; lba&lt;/P&gt;&lt;P&gt; 2&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 12.6MB&amp;nbsp; 83.9MB&amp;nbsp; 71.3MB&amp;nbsp; primary&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;dd: failed to open '/home/srinivasulu/Freescale_BSP/Build/tmp/deploy/images/imx6ulevk/u-boot-imx6ulevk.imx': No such file or directory&lt;/P&gt;&lt;P&gt;WARNING: exit code 1 from a shell command.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ERROR: Function failed: do_rootfs&lt;/P&gt;&lt;P&gt;ERROR: Logfile of failure stored in: /home/srinivasulu/Freescale_BSP/Build/tmp/work/imx6ulevk-poky-linux-gnueabi/core-image-base/1.0-r0/temp/log.do_rootfs.5870&lt;/P&gt;&lt;P&gt;ERROR: Task 7 (/home/srinivasulu/Freescale_BSP/sources/poky/meta/recipes-core/images/core-image-base.bb, do_rootfs) failed with exit code '1'&lt;/P&gt;&lt;P&gt;NOTE: Tasks Summary: Attempted 2427 tasks of which 2426 didn't need to be rerun and 1 failed.&lt;/P&gt;&lt;P&gt;No currently running tasks (2426 of 2428)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Summary: 1 task failed:&lt;/P&gt;&lt;P&gt;&amp;nbsp; /home/srinivasulu/Freescale_BSP/sources/poky/meta/recipes-core/images/core-image-base.bb, do_rootfs&lt;/P&gt;&lt;P&gt;Summary: There were 3 WARNING messages shown.&lt;/P&gt;&lt;P&gt;Summary: There were 2 ERROR messages shown, returning a non-zero exit code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please let me know how to resolve the above problem?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 28 Dec 2015 10:02:21 GMT</pubDate>
    <dc:creator>srinivasulured1</dc:creator>
    <dc:date>2015-12-28T10:02:21Z</dc:date>
    <item>
      <title>Imx6ul deploy folder files deleted</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Imx6ul-deploy-folder-files-deleted/m-p/508148#M82759</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using imx6ul eval board. I followed the "yocto project user guide" to create the images. but few files are deleted from ~/tmp/delpoy/images/imx6ulevk" folder. when i try to recreate the images i am getting the following error.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;WARNING: log_check: There is a warn message in the logfile&lt;/P&gt;&lt;P&gt;WARNING: log_check: Matched keyword: [WARNING:]&lt;/P&gt;&lt;P&gt;WARNING: log_check: WARNING: The license listed Firmware-atheros_firmware was not in the licenses collected for linux-firmware&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ERROR: Error: The image creation script '/home/srinivasulu/Freescale_BSP/Build/tmp/work/imx6ulevk-poky-linux-gnueabi/core-image-base/1.0-r0/temp/create_image.sdcard' returned 1:&lt;/P&gt;&lt;P&gt;0+0 records in&lt;/P&gt;&lt;P&gt;0+0 records out&lt;/P&gt;&lt;P&gt;0 bytes (0 B) copied, 7.8307e-05 s, 0.0 kB/s&lt;/P&gt;&lt;P&gt;Model:&amp;nbsp; (file)&lt;/P&gt;&lt;P&gt;Disk /home/srinivasulu/Freescale_BSP/Build/tmp/deploy/images/imx6ulevk/core-image-base-imx6ulevk-20151228075336.rootfs.sdcard: 88.1MB&lt;/P&gt;&lt;P&gt;Sector size (logical/physical): 512B/512B&lt;/P&gt;&lt;P&gt;Partition Table: msdos&lt;/P&gt;&lt;P&gt;Disk Flags: &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Number&amp;nbsp; Start&amp;nbsp;&amp;nbsp; End&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Size&amp;nbsp;&amp;nbsp;&amp;nbsp; Type&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; File system&amp;nbsp; Flags&lt;/P&gt;&lt;P&gt; 1&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 4194kB&amp;nbsp; 12.6MB&amp;nbsp; 8389kB&amp;nbsp; primary&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; lba&lt;/P&gt;&lt;P&gt; 2&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 12.6MB&amp;nbsp; 83.9MB&amp;nbsp; 71.3MB&amp;nbsp; primary&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;dd: failed to open '/home/srinivasulu/Freescale_BSP/Build/tmp/deploy/images/imx6ulevk/u-boot-imx6ulevk.imx': No such file or directory&lt;/P&gt;&lt;P&gt;WARNING: exit code 1 from a shell command.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ERROR: Function failed: do_rootfs&lt;/P&gt;&lt;P&gt;ERROR: Logfile of failure stored in: /home/srinivasulu/Freescale_BSP/Build/tmp/work/imx6ulevk-poky-linux-gnueabi/core-image-base/1.0-r0/temp/log.do_rootfs.5870&lt;/P&gt;&lt;P&gt;ERROR: Task 7 (/home/srinivasulu/Freescale_BSP/sources/poky/meta/recipes-core/images/core-image-base.bb, do_rootfs) failed with exit code '1'&lt;/P&gt;&lt;P&gt;NOTE: Tasks Summary: Attempted 2427 tasks of which 2426 didn't need to be rerun and 1 failed.&lt;/P&gt;&lt;P&gt;No currently running tasks (2426 of 2428)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Summary: 1 task failed:&lt;/P&gt;&lt;P&gt;&amp;nbsp; /home/srinivasulu/Freescale_BSP/sources/poky/meta/recipes-core/images/core-image-base.bb, do_rootfs&lt;/P&gt;&lt;P&gt;Summary: There were 3 WARNING messages shown.&lt;/P&gt;&lt;P&gt;Summary: There were 2 ERROR messages shown, returning a non-zero exit code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please let me know how to resolve the above problem?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Dec 2015 10:02:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Imx6ul-deploy-folder-files-deleted/m-p/508148#M82759</guid>
      <dc:creator>srinivasulured1</dc:creator>
      <dc:date>2015-12-28T10:02:21Z</dc:date>
    </item>
    <item>
      <title>Re: Imx6ul deploy folder files deleted</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Imx6ul-deploy-folder-files-deleted/m-p/508149#M82760</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Srinivasulu Reddy,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Would you know how these files were deleted? If they were manually deleted you would need to make a CleanAll and then build again from scratch. As a rule of thumb you shouldn’t delete any file from the folder in which they are deployed. For more information you may read the README that is on the same folder where the images are generated. The problem with deleting these files is that Yocto cannot keep track of what was removed and thus can generate problems.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would recommend doung a CleanAll of your image and baking again:&lt;/P&gt;&lt;P&gt;$ bitbake –c cleanall &amp;lt;IMAGE&amp;gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Jan 2016 17:38:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Imx6ul-deploy-folder-files-deleted/m-p/508149#M82760</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2016-01-07T17:38:38Z</dc:date>
    </item>
  </channel>
</rss>