<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Gigabit Ethernet speed constraint for i.Mx6Q</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Gigabit-Ethernet-speed-constraint-for-i-Mx6Q/m-p/506788#M82431</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp; The known erratum ERR004512 (ENET : 1 Gb Ethernet MAC (ENET) system limitation) &lt;/P&gt;&lt;P&gt;relates to general system performance limitation. This affects PCIe Ethernet too. &lt;BR /&gt;The i.MX6 – at least initially - was not intended for best Ethernet performance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 12 Feb 2016 07:52:30 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2016-02-12T07:52:30Z</dc:date>
    <item>
      <title>Gigabit Ethernet speed constraint for i.Mx6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Gigabit-Ethernet-speed-constraint-for-i-Mx6Q/m-p/506787#M82430</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i'm using i.Mx6Q (&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;MCIMX6Q6AVT10AD)&lt;/SPAN&gt; in my design.&lt;/P&gt;&lt;P&gt;I want to interface the Gigabit Ethernet present in the i.Mx6Q.&lt;/P&gt;&lt;P&gt;As per the datasheet the maximum speed that can be achieved with Gigabit Ethernet will be 400 Mbps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;"The theoretical maximum performance of 1 Gbps ENET is limited to 470 Mbps (total for Tx and Rx) due to internal bus throughput limitations."&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using this Gigabit Ethernet for communication between two i.Mx6Q devices without using a PHY in between.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;So will the speed constraint will remain same ? or higher speed can be achieved ?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm also using the PCIe interface available with i.Mx6Q for Gigabit Ethernet with PCIe to Gigabit Ethernet converter. This will be used for separate file transfer application&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;So, Is it possible to achieve the 1000 Mbps speed with PCIe Converted Gigabit Ethernet ? &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(Note that PCIe devices/converters used are capable of handling 1Gbps speed)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please help me with this ASAP.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;Nanjunda M&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Feb 2016 07:42:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Gigabit-Ethernet-speed-constraint-for-i-Mx6Q/m-p/506787#M82430</guid>
      <dc:creator>nanjundam</dc:creator>
      <dc:date>2016-02-12T07:42:54Z</dc:date>
    </item>
    <item>
      <title>Re: Gigabit Ethernet speed constraint for i.Mx6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Gigabit-Ethernet-speed-constraint-for-i-Mx6Q/m-p/506788#M82431</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp; The known erratum ERR004512 (ENET : 1 Gb Ethernet MAC (ENET) system limitation) &lt;/P&gt;&lt;P&gt;relates to general system performance limitation. This affects PCIe Ethernet too. &lt;BR /&gt;The i.MX6 – at least initially - was not intended for best Ethernet performance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Feb 2016 07:52:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Gigabit-Ethernet-speed-constraint-for-i-Mx6Q/m-p/506788#M82431</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-02-12T07:52:30Z</dc:date>
    </item>
  </channel>
</rss>