<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IMX6 Quad and Dual boot issue from eMMC in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-Quad-and-Dual-boot-issue-from-eMMC/m-p/506175#M82257</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, it does.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to our test, it seems that eMMC loads correctly and all the DCDs&lt;BR /&gt;register settings are applied properly, the problem starts later on when the&lt;BR /&gt;ROM code moves on to initializing the DDRs - if that matters.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- I run the DDR stress test with 400MHz and 566MHz. Both clock frequency succeed with no issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- One symptom is that&lt;/P&gt;&lt;P&gt;Before loading the boot image on eMMC, our board goes into the serial boot mode. However, it doesn't start the u-boot properly from the serial boot mode with mfg-tool. It is always stuck until the POR_B is reset again.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- Another symptom is that&lt;/P&gt;&lt;P&gt;If the VDD_HIGH_IN is tied directly with VSNVS via coin-cell battery which is charged up to 1V, the board is always booting properly.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 31 May 2016 21:55:51 GMT</pubDate>
    <dc:creator>yongwoolee</dc:creator>
    <dc:date>2016-05-31T21:55:51Z</dc:date>
    <item>
      <title>IMX6 Quad and Dual boot issue from eMMC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-Quad-and-Dual-boot-issue-from-eMMC/m-p/506168#M82250</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;@Hi. I am developing the board with IMX6 Quad and Dual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Both have the boot issue when it powers on. Only when the power is on within 3 seconds or less, the board is booting from the eMMC properly. Otherwise, the board always goes into USB serial boot mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When the POR_B is reset again, then it boots normally.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This board is using&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- MCIMX6Q5EYM10AD&lt;/P&gt;&lt;P&gt;- PF0100NPEAP which is using the same script of F0 pre-programmed&lt;/P&gt;&lt;P&gt;- 4 DDR3&lt;/P&gt;&lt;P&gt;- 4G eMMC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Actually, I have done the same project with IMX6-Dual and 2 DDR3. This board is working perfectly.&lt;/P&gt;&lt;P&gt;Basically, both projects with 2 DDR3 and with 4 DDR3 are identical. Same Dual processor and same PMIC PF0100NPEAP.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, the board with 4 DDR3 has the boot issue as I described above.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to the errata, I add the 1uF on the POR_B to make a delay until the 32KHz external crystal gets stable and other power rails.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can search the similar issue related to the boot. Do you have any solution about it?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 May 2016 20:14:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-Quad-and-Dual-boot-issue-from-eMMC/m-p/506168#M82250</guid>
      <dc:creator>yongwoolee</dc:creator>
      <dc:date>2016-05-26T20:14:59Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 Quad and Dual boot issue from eMMC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-Quad-and-Dual-boot-issue-from-eMMC/m-p/506169#M82251</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yongwoo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can recheck power up sequence with oscilloscope and&lt;/P&gt;&lt;P&gt;rerun ddr test for 4 DDR3 case to obtain more accurate calibration&lt;/P&gt;&lt;P&gt;coefficients.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.freescale.com/docs/DOC-105652" title="https://community.freescale.com/docs/DOC-105652"&gt;https://community.freescale.com/docs/DOC-105652&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 May 2016 00:34:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-Quad-and-Dual-boot-issue-from-eMMC/m-p/506169#M82251</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-05-27T00:34:42Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 Quad and Dual boot issue from eMMC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-Quad-and-Dual-boot-issue-from-eMMC/m-p/506170#M82252</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I check the power sequences with the scope and it is satisfied with the requirement. As I mentioned in the first comment, I am using the "F0" script and the PF0100NPAEP's sequence is matched with it according to my test.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to our test, it seems that eMMC loads correctly and all the DCDs&lt;BR /&gt;register settings are applied properly, the problem starts later on when the&lt;BR /&gt;ROM code moves on to initializing the DDRs - if that matters.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When it fails to boot, there is no proper DDR Clock, compared to the normal operation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As you mentioned, I run the DDR test for 4 DDR3. What does the result mean below?&lt;/P&gt;&lt;P&gt;============================================&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Boot Configuration&lt;/P&gt;&lt;P&gt;SRC_SBMR1(0x020d8004) = 0x00002060&lt;/P&gt;&lt;P&gt;SRC_SBMR2(0x020d801c) = 0x21000011&lt;/P&gt;&lt;P&gt;============================================&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ARM Clock set to 1GHz&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;============================================&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; DDR configuration&lt;/P&gt;&lt;P&gt;BOOT_CFG3[5-4]: 0x00, Single DDR channel.&lt;/P&gt;&lt;P&gt;DDR type is DDR3 &lt;/P&gt;&lt;P&gt;Data width: 64, bank num: 8&lt;/P&gt;&lt;P&gt;Row size: 14, col size: 10&lt;/P&gt;&lt;P&gt;Chip select CSD0 is used &lt;/P&gt;&lt;P&gt;Density per chip select: 1024MB &lt;/P&gt;&lt;P&gt;============================================&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;DDR Stress Test Iteration 1&lt;/P&gt;&lt;P&gt;Current Temperature: 60&lt;/P&gt;&lt;P&gt;============================================&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;DDR Freq: 672 MHz&lt;/P&gt;&lt;P&gt;t0.1: data is addr test&lt;/P&gt;&lt;P&gt;Address of failure: 0x10000004&lt;/P&gt;&lt;P&gt;Data was: 0x00000014&lt;/P&gt;&lt;P&gt;But pattern&amp;nbsp; should match address &lt;/P&gt;&lt;P&gt;Error: failed to run stress test!!!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 May 2016 14:45:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-Quad-and-Dual-boot-issue-from-eMMC/m-p/506170#M82252</guid>
      <dc:creator>yongwoolee</dc:creator>
      <dc:date>2016-05-27T14:45:21Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 Quad and Dual boot issue from eMMC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-Quad-and-Dual-boot-issue-from-eMMC/m-p/506171#M82253</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;One more symptom when I tested the DDR.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When the board doesn't turn on/off/on quickly within 3 seconds, the board is stuck although it goes into the serial boot mode automatically.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;At the serial boot mode for DDR test, the freescale DDR Test tool shows the error like below when I tried to load the "init Script".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"ERROR: Write dcd failed."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;By the way, I also tested the internal oscillator instead of the external 32.768KHz followed by the errata. But, it doesn't help fix the boot issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In addition, I extend the POR_B manually up to around 1 seconds and release it to run the IMX. This doesn't help either.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is the result of the calibration when the board goes into the serial boot mode normally.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;============================================&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Chip ID&lt;/P&gt;&lt;P&gt;CHIP ID = i.MX6 Dual/Quad (0x63)&lt;/P&gt;&lt;P&gt;Internal Revision = TO1.5&lt;/P&gt;&lt;P&gt;============================================&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;============================================&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Boot Configuration&lt;/P&gt;&lt;P&gt;SRC_SBMR1(0x020d8004) = 0x00002060&lt;/P&gt;&lt;P&gt;SRC_SBMR2(0x020d801c) = 0x21000011&lt;/P&gt;&lt;P&gt;============================================&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ARM Clock set to 1GHz&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;============================================&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; DDR configuration&lt;/P&gt;&lt;P&gt;BOOT_CFG3[5-4]: 0x00, Single DDR channel.&lt;/P&gt;&lt;P&gt;DDR type is DDR3 &lt;/P&gt;&lt;P&gt;Data width: 64, bank num: 8&lt;/P&gt;&lt;P&gt;Row size: 14, col size: 10&lt;/P&gt;&lt;P&gt;Chip select CSD0 is used &lt;/P&gt;&lt;P&gt;Density per chip select: 1024MB &lt;/P&gt;&lt;P&gt;============================================&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Current Temperature: 62&lt;/P&gt;&lt;P&gt;============================================&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;DDR Freq: 528 MHz &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ddr_mr1=0x00000001&lt;/P&gt;&lt;P&gt;Start write leveling calibration...&lt;/P&gt;&lt;P&gt;running Write level HW calibration&lt;/P&gt;&lt;P&gt;Write leveling calibration completed, update the following registers in your initialization script&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; MMDC_MPWLDECTRL0 ch0 (0x021b080c) = 0x00080013&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; MMDC_MPWLDECTRL1 ch0 (0x021b0810) = 0x002B001E&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; MMDC_MPWLDECTRL0 ch1 (0x021b480c) = 0x000D0025&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; MMDC_MPWLDECTRL1 ch1 (0x021b4810) = 0x00000000&lt;/P&gt;&lt;P&gt;Write DQS delay result:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Write DQS0 delay: 19/256 CK&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Write DQS1 delay: 8/256 CK&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Write DQS2 delay: 30/256 CK&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Write DQS3 delay: 43/256 CK&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Write DQS4 delay: 37/256 CK&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Write DQS5 delay: 13/256 CK&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Write DQS6 delay: 0/256 CK&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Write DQS7 delay: 0/256 CK&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Starting DQS gating calibration&lt;/P&gt;&lt;P&gt;. . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . &lt;/P&gt;&lt;P&gt;. . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BYTE 0: &lt;/P&gt;&lt;P&gt; Start:&amp;nbsp;&amp;nbsp; HC=0x02 ABS=0x18&lt;/P&gt;&lt;P&gt; End:&amp;nbsp;&amp;nbsp; HC=0x05 ABS=0x4C&lt;/P&gt;&lt;P&gt; Mean:&amp;nbsp;&amp;nbsp; HC=0x03 ABS=0x71&lt;/P&gt;&lt;P&gt; End-0.5*tCK:&amp;nbsp; HC=0x04 ABS=0x4C&lt;/P&gt;&lt;P&gt; Final:&amp;nbsp;&amp;nbsp; HC=0x04 ABS=0x4C&lt;/P&gt;&lt;P&gt;BYTE 1: &lt;/P&gt;&lt;P&gt; Start:&amp;nbsp;&amp;nbsp; HC=0x02 ABS=0x10&lt;/P&gt;&lt;P&gt; End:&amp;nbsp;&amp;nbsp; HC=0x05 ABS=0x3C&lt;/P&gt;&lt;P&gt; Mean:&amp;nbsp;&amp;nbsp; HC=0x03 ABS=0x65&lt;/P&gt;&lt;P&gt; End-0.5*tCK:&amp;nbsp; HC=0x04 ABS=0x3C&lt;/P&gt;&lt;P&gt; Final:&amp;nbsp;&amp;nbsp; HC=0x04 ABS=0x3C&lt;/P&gt;&lt;P&gt;BYTE 2: &lt;/P&gt;&lt;P&gt; Start:&amp;nbsp;&amp;nbsp; HC=0x03 ABS=0x10&lt;/P&gt;&lt;P&gt; End:&amp;nbsp;&amp;nbsp; HC=0x05 ABS=0x48&lt;/P&gt;&lt;P&gt; Mean:&amp;nbsp;&amp;nbsp; HC=0x04 ABS=0x2C&lt;/P&gt;&lt;P&gt; End-0.5*tCK:&amp;nbsp; HC=0x04 ABS=0x48&lt;/P&gt;&lt;P&gt; Final:&amp;nbsp;&amp;nbsp; HC=0x04 ABS=0x48&lt;/P&gt;&lt;P&gt;BYTE 3: &lt;/P&gt;&lt;P&gt; Start:&amp;nbsp;&amp;nbsp; HC=0x03 ABS=0x0C&lt;/P&gt;&lt;P&gt; End:&amp;nbsp;&amp;nbsp; HC=0x05 ABS=0x4C&lt;/P&gt;&lt;P&gt; Mean:&amp;nbsp;&amp;nbsp; HC=0x04 ABS=0x2C&lt;/P&gt;&lt;P&gt; End-0.5*tCK:&amp;nbsp; HC=0x04 ABS=0x4C&lt;/P&gt;&lt;P&gt; Final:&amp;nbsp;&amp;nbsp; HC=0x04 ABS=0x4C&lt;/P&gt;&lt;P&gt;BYTE 4: &lt;/P&gt;&lt;P&gt; Start:&amp;nbsp;&amp;nbsp; HC=0x03 ABS=0x00&lt;/P&gt;&lt;P&gt; End:&amp;nbsp;&amp;nbsp; HC=0x05 ABS=0x48&lt;/P&gt;&lt;P&gt; Mean:&amp;nbsp;&amp;nbsp; HC=0x04 ABS=0x24&lt;/P&gt;&lt;P&gt; End-0.5*tCK:&amp;nbsp; HC=0x04 ABS=0x48&lt;/P&gt;&lt;P&gt; Final:&amp;nbsp;&amp;nbsp; HC=0x04 ABS=0x48&lt;/P&gt;&lt;P&gt;BYTE 5: &lt;/P&gt;&lt;P&gt; Start:&amp;nbsp;&amp;nbsp; HC=0x02 ABS=0x10&lt;/P&gt;&lt;P&gt; End:&amp;nbsp;&amp;nbsp; HC=0x05 ABS=0x3C&lt;/P&gt;&lt;P&gt; Mean:&amp;nbsp;&amp;nbsp; HC=0x03 ABS=0x65&lt;/P&gt;&lt;P&gt; End-0.5*tCK:&amp;nbsp; HC=0x04 ABS=0x3C&lt;/P&gt;&lt;P&gt; Final:&amp;nbsp;&amp;nbsp; HC=0x04 ABS=0x3C&lt;/P&gt;&lt;P&gt;BYTE 6: &lt;/P&gt;&lt;P&gt; Start:&amp;nbsp;&amp;nbsp; HC=0x02 ABS=0x64&lt;/P&gt;&lt;P&gt; End:&amp;nbsp;&amp;nbsp; HC=0x05 ABS=0x0C&lt;/P&gt;&lt;P&gt; Mean:&amp;nbsp;&amp;nbsp; HC=0x03 ABS=0x77&lt;/P&gt;&lt;P&gt; End-0.5*tCK:&amp;nbsp; HC=0x04 ABS=0x0C&lt;/P&gt;&lt;P&gt; Final:&amp;nbsp;&amp;nbsp; HC=0x04 ABS=0x0C&lt;/P&gt;&lt;P&gt;BYTE 7: &lt;/P&gt;&lt;P&gt; Start:&amp;nbsp;&amp;nbsp; HC=0x03 ABS=0x00&lt;/P&gt;&lt;P&gt; End:&amp;nbsp;&amp;nbsp; HC=0x05 ABS=0x34&lt;/P&gt;&lt;P&gt; Mean:&amp;nbsp;&amp;nbsp; HC=0x04 ABS=0x1A&lt;/P&gt;&lt;P&gt; End-0.5*tCK:&amp;nbsp; HC=0x04 ABS=0x34&lt;/P&gt;&lt;P&gt; Final:&amp;nbsp;&amp;nbsp; HC=0x04 ABS=0x34&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;DQS calibration MMDC0 MPDGCTRL0 = 0x443C044C, MPDGCTRL1 = 0x044C0448&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;DQS calibration MMDC1 MPDGCTRL0 = 0x443C0448, MPDGCTRL1 = 0x0434040C&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note: Array result[] holds the DRAM test result of each byte.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0: test pass.&amp;nbsp; 1: test fail&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 4 bits respresent the result of 1 byte.&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; result 00000001:byte 0 fail. &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; result 00000011:byte 0, 1 fail. &lt;/P&gt;&lt;P&gt;Starting Read calibration...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x00000000 result[00]=0x11111111&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x04040404 result[01]=0x11111111&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x08080808 result[02]=0x11111111&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x0C0C0C0C result[03]=0x11011111&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x10101010 result[04]=0x00011011&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x14141414 result[05]=0x00010011&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x18181818 result[06]=0x00010001&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x1C1C1C1C result[07]=0x00010000&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x20202020 result[08]=0x00000000&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x24242424 result[09]=0x00000000&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x28282828 result[0A]=0x00000000&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x2C2C2C2C result[0B]=0x00000000&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x30303030 result[0C]=0x00000000&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x34343434 result[0D]=0x00000000&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x38383838 result[0E]=0x00000000&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x3C3C3C3C result[0F]=0x00000000&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x40404040 result[10]=0x00000000&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x44444444 result[11]=0x00000000&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x48484848 result[12]=0x00000000&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x4C4C4C4C result[13]=0x00000100&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x50505050 result[14]=0x01100100&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x54545454 result[15]=0x11101110&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x58585858 result[16]=0x11101110&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x5C5C5C5C result[17]=0x11111111&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x60606060 result[18]=0x11111111&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x64646464 result[19]=0x11111111&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x68686868 result[1A]=0x11111111&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x6C6C6C6C result[1B]=0x11111111&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x70707070 result[1C]=0x11111111&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x74747474 result[1D]=0x11111111&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x78787878 result[1E]=0x11111111&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x7C7C7C7C result[1F]=0x11111111&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Byte 0: (0x1c - 0x58), middle value:0x3a&lt;/P&gt;&lt;P&gt;Byte 1: (0x18 - 0x50), middle value:0x34&lt;/P&gt;&lt;P&gt;Byte 2: (0x10 - 0x48), middle value:0x2c&lt;/P&gt;&lt;P&gt;Byte 3: (0x14 - 0x50), middle value:0x32&lt;/P&gt;&lt;P&gt;Byte 4: (0x20 - 0x58), middle value:0x3c&lt;/P&gt;&lt;P&gt;Byte 5: (0x0c - 0x4c), middle value:0x2c&lt;/P&gt;&lt;P&gt;Byte 6: (0x10 - 0x4c), middle value:0x2e&lt;/P&gt;&lt;P&gt;Byte 7: (0x10 - 0x50), middle value:0x30&lt;/P&gt;&lt;P&gt;MMDC0 MPRDDLCTL = 0x322C343A, MMDC1 MPRDDLCTL = 0x302E2C3C&lt;/P&gt;&lt;P&gt;Starting Write calibration...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x00000000 result[00]=0x11111111&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x04040404 result[01]=0x10111111&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x08080808 result[02]=0x10110110&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x0C0C0C0C result[03]=0x10100010&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x10101010 result[04]=0x00100000&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x14141414 result[05]=0x00000000&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x18181818 result[06]=0x00000000&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x1C1C1C1C result[07]=0x00000000&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x20202020 result[08]=0x00000000&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x24242424 result[09]=0x00000000&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x28282828 result[0A]=0x00000000&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x2C2C2C2C result[0B]=0x00000000&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x30303030 result[0C]=0x00000000&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x34343434 result[0D]=0x00000000&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x38383838 result[0E]=0x00000000&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x3C3C3C3C result[0F]=0x00000000&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x40404040 result[10]=0x00000000&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x44444444 result[11]=0x00000000&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x48484848 result[12]=0x01000000&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x4C4C4C4C result[13]=0x01000000&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x50505050 result[14]=0x01000001&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x54545454 result[15]=0x01000011&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x58585858 result[16]=0x01000011&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x5C5C5C5C result[17]=0x11000011&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x60606060 result[18]=0x11000011&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x64646464 result[19]=0x11011111&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x68686868 result[1A]=0x11111111&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x6C6C6C6C result[1B]=0x11111111&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x70707070 result[1C]=0x11111111&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x74747474 result[1D]=0x11111111&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x78787878 result[1E]=0x11111111&lt;/P&gt;&lt;P&gt;ABS_OFFSET=0x7C7C7C7C result[1F]=0x11111111&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Byte 0: (0x08 - 0x4c), middle value:0x2a&lt;/P&gt;&lt;P&gt;Byte 1: (0x10 - 0x50), middle value:0x30&lt;/P&gt;&lt;P&gt;Byte 2: (0x0c - 0x60), middle value:0x36&lt;/P&gt;&lt;P&gt;Byte 3: (0x08 - 0x60), middle value:0x34&lt;/P&gt;&lt;P&gt;Byte 4: &lt;/P&gt;&lt;P&gt;Byte 5: (0x14 - 0x64), middle value:0x3c&lt;/P&gt;&lt;P&gt;Byte 6: (0x04 - 0x44), middle value:0x24&lt;/P&gt;&lt;P&gt;Byte 7: (0x10 - 0x58), middle value:0x34&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MMDC0 MPWRDLCTL = 0x3436302A,MMDC1 MPWRDLCTL = 0x34243C36&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; MMDC registers updated from calibration &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Write leveling calibration&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; MMDC_MPWLDECTRL0 ch0 (0x021b080c) = 0x00080013&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; MMDC_MPWLDECTRL1 ch0 (0x021b0810) = 0x002B001E&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; MMDC_MPWLDECTRL0 ch1 (0x021b480c) = 0x000D0025&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; MMDC_MPWLDECTRL1 ch1 (0x021b4810) = 0x00000000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Read DQS Gating calibration&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; MPDGCTRL0 PHY0 (0x021b083c) = 0x443C044C&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; MPDGCTRL1 PHY0 (0x021b0840) = 0x044C0448&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; MPDGCTRL0 PHY1 (0x021b483c) = 0x443C0448&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; MPDGCTRL1 PHY1 (0x021b4840) = 0x0434040C&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Read calibration&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; MPRDDLCTL PHY0 (0x021b0848) = 0x322C343A&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; MPRDDLCTL PHY1 (0x021b4848) = 0x302E2C3C&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Write calibration&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; MPWRDLCTL PHY0 (0x021b0850) = 0x3436302A&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; MPWRDLCTL PHY1 (0x021b4850) = 0x34243C36&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Success: DDR calibration completed!!!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 May 2016 18:51:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-Quad-and-Dual-boot-issue-from-eMMC/m-p/506171#M82253</guid>
      <dc:creator>yongwoolee</dc:creator>
      <dc:date>2016-05-27T18:51:56Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 Quad and Dual boot issue from eMMC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-Quad-and-Dual-boot-issue-from-eMMC/m-p/506172#M82254</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yongwoo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;when boots fails could you attach jtag and check &lt;/P&gt;&lt;P&gt;SRC_SBMR1,2 registers: do they have correct values (set by boot pins)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 May 2016 04:33:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-Quad-and-Dual-boot-issue-from-eMMC/m-p/506172#M82254</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-05-30T04:33:54Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 Quad and Dual boot issue from eMMC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-Quad-and-Dual-boot-issue-from-eMMC/m-p/506173#M82255</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is the info of SRC_SBMR1/2 from Jtag.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;md 0x020d8004 1&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; 020d8004 : 0x00002060&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 8288&amp;nbsp; ` ..&lt;/P&gt;&lt;P&gt; &lt;BR /&gt;md 0x020d801c 1&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; 020d801c : 0x28000011&amp;nbsp;&amp;nbsp;&amp;nbsp; 671088657&amp;nbsp; ...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 May 2016 16:20:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-Quad-and-Dual-boot-issue-from-eMMC/m-p/506173#M82255</guid>
      <dc:creator>yongwoolee</dc:creator>
      <dc:date>2016-05-30T16:20:28Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 Quad and Dual boot issue from eMMC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-Quad-and-Dual-boot-issue-from-eMMC/m-p/506174#M82256</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yongwoo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;do they correspond values set by boot pins ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 31 May 2016 01:42:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-Quad-and-Dual-boot-issue-from-eMMC/m-p/506174#M82256</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-05-31T01:42:36Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 Quad and Dual boot issue from eMMC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-Quad-and-Dual-boot-issue-from-eMMC/m-p/506175#M82257</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, it does.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to our test, it seems that eMMC loads correctly and all the DCDs&lt;BR /&gt;register settings are applied properly, the problem starts later on when the&lt;BR /&gt;ROM code moves on to initializing the DDRs - if that matters.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- I run the DDR stress test with 400MHz and 566MHz. Both clock frequency succeed with no issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- One symptom is that&lt;/P&gt;&lt;P&gt;Before loading the boot image on eMMC, our board goes into the serial boot mode. However, it doesn't start the u-boot properly from the serial boot mode with mfg-tool. It is always stuck until the POR_B is reset again.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- Another symptom is that&lt;/P&gt;&lt;P&gt;If the VDD_HIGH_IN is tied directly with VSNVS via coin-cell battery which is charged up to 1V, the board is always booting properly.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 31 May 2016 21:55:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-Quad-and-Dual-boot-issue-from-eMMC/m-p/506175#M82257</guid>
      <dc:creator>yongwoolee</dc:creator>
      <dc:date>2016-05-31T21:55:51Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 Quad and Dual boot issue from eMMC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-Quad-and-Dual-boot-issue-from-eMMC/m-p/506176#M82258</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yongwoo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;If the VDD_HIGH_IN is tied directly with VSNVS via coin-cell battery which is&lt;/P&gt;&lt;P&gt;&amp;gt;charged up to 1V, the board is always booting properly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;this points that issue is related to power-up sequence&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Jun 2016 01:59:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-Quad-and-Dual-boot-issue-from-eMMC/m-p/506176#M82258</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-06-01T01:59:42Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 Quad and Dual boot issue from eMMC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-Quad-and-Dual-boot-issue-from-eMMC/m-p/506177#M82259</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As I mentioned, the board is using the F0 Script which is used on the Sabre reference board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The power sequence is exactly identical to F0's. Then, how could the power sequence cause the issue?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you explain it in detail?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Jun 2016 02:34:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-Quad-and-Dual-boot-issue-from-eMMC/m-p/506177#M82259</guid>
      <dc:creator>yongwoolee</dc:creator>
      <dc:date>2016-06-01T02:34:52Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 Quad and Dual boot issue from eMMC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-Quad-and-Dual-boot-issue-from-eMMC/m-p/506178#M82260</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yongwoo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please check Chapter 4 Requirements for Power Management&lt;/P&gt;&lt;P&gt;i.MX6 System Development User’s Guide&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fcache.freescale.com%2Ffiles%2F32bit%2Fdoc%2Fuser_guide%2FIMX6DQ6SDLHDG.pdf" rel="nofollow" target="_blank"&gt;http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;and sect.4.2.1 Power-Up Sequence i.MX6DQ Datasheet&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fcache.freescale.com%2Ffiles%2F32bit%2Fdoc%2Fdata_sheet%2FIMX6DQCEC.pdf" rel="nofollow" target="_blank"&gt;http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;suggest to look at below links solutions with similar problem&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fcommunity.freescale.com%2Fthread%2F338433" rel="nofollow" target="_blank"&gt;https://community.freescale.com/thread/338433&lt;/A&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/382025"&gt;IMX6SOLO initial power up boot up issue&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Jun 2016 07:40:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-Quad-and-Dual-boot-issue-from-eMMC/m-p/506178#M82260</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-06-01T07:40:14Z</dc:date>
    </item>
  </channel>
</rss>