<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: WinCE Redundant boot on I.MX28 Rom code error HTLC0x8050100f</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/WinCE-Redundant-boot-on-I-MX28-Rom-code-error-HTLC0x8050100f/m-p/183569#M8204</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;By reverse engineering in found that the redundant boot is only implemented for the E-boot section.&lt;/P&gt;&lt;P&gt;I make a new update tool for updating the WinCe section, but this is not redundant.&lt;/P&gt;&lt;P&gt;Marc&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 06 Sep 2012 07:39:41 GMT</pubDate>
    <dc:creator>MarcCoussement</dc:creator>
    <dc:date>2012-09-06T07:39:41Z</dc:date>
    <item>
      <title>WinCE Redundant boot on I.MX28 Rom code error HTLC0x8050100f</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/WinCE-Redundant-boot-on-I-MX28-Rom-code-error-HTLC0x8050100f/m-p/183566#M8201</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN class="font-size-3"&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/discussions/558-WinCeRedundantBoot.pdf" target="_self"&gt;WinCeRedundantBoot.pdf&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="font-size-3"&gt;I have a problem using the WinCE redundant boot feature as explained in the&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="font-size-3"&gt;Freescale Windows Embedded CE 6.0 reference manual" chapter 14 NAND redundant boot" see attachement on the IMX28 EVK&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="font-size-3"&gt;We get error Rom code error HTLC0x8050100f&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="font-size-3"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="font-size-3"&gt;After loading the image with the imageUpdate.exe tool.The update reports update successfully, system will reboot please wait and a restart is occurring (as expected).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;SPAN class="font-size-3"&gt;However, on&amp;nbsp; the debug port we see the following debug info:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="font-size-3"&gt;rebooting... ...&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="font-size-3"&gt;HTLC0x8050100f&lt;/SPAN&gt;&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;&lt;SPAN class="font-size-3"&gt;When we push the reset button, the only thing that is happening is a print of the same last error code.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN class="font-size-3"&gt;To recover we have to disconnect the power and reconnect it again.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="font-size-3"&gt;Now everything is starting up again but after the image starts we got the&lt;/SPAN&gt; &lt;BR /&gt;&lt;SPAN class="font-size-3"&gt;following question:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="font-size-3"&gt;Do you want to recover boot stream two? Probably as a result of the unfinished update.&amp;nbsp; (recovery works fine)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="font-size-3"&gt;Is there a list of the rom error codes for the imx28?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="font-size-3"&gt;Any help appreciated&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Nov 2011 23:25:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/WinCE-Redundant-boot-on-I-MX28-Rom-code-error-HTLC0x8050100f/m-p/183566#M8201</guid>
      <dc:creator>MarcCoussement</dc:creator>
      <dc:date>2011-11-04T23:25:08Z</dc:date>
    </item>
    <item>
      <title>Re: WinCE Redundant boot on I.MX28 Rom code error HTLC0x8050100f</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/WinCE-Redundant-boot-on-I-MX28-Rom-code-error-HTLC0x8050100f/m-p/183567#M8202</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The error 0x8050100F means "Requested data beyond the end of a section" for call.&lt;/P&gt;&lt;P&gt;Maybe in nk.bd file, you had defined "&amp;nbsp;&amp;nbsp;&amp;nbsp; call xxxxx;", but in the real nk.sb, there is no define for xxxxx, then you will get such error.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Nov 2011 06:33:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/WinCE-Redundant-boot-on-I-MX28-Rom-code-error-HTLC0x8050100f/m-p/183567#M8202</guid>
      <dc:creator>qiang_li-mpu_se</dc:creator>
      <dc:date>2011-11-09T06:33:09Z</dc:date>
    </item>
    <item>
      <title>Re: WinCE Redundant boot on I.MX28 Rom code error HTLC0x8050100f</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/WinCE-Redundant-boot-on-I-MX28-Rom-code-error-HTLC0x8050100f/m-p/183568#M8203</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is this error fixed?. Can you let me know if you've any pointers for how to boot up as redundant boot in SD Card.This is in case if it fails to boot up from the primary partition.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Sep 2012 21:11:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/WinCE-Redundant-boot-on-I-MX28-Rom-code-error-HTLC0x8050100f/m-p/183568#M8203</guid>
      <dc:creator>Gatts</dc:creator>
      <dc:date>2012-09-05T21:11:15Z</dc:date>
    </item>
    <item>
      <title>Re: WinCE Redundant boot on I.MX28 Rom code error HTLC0x8050100f</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/WinCE-Redundant-boot-on-I-MX28-Rom-code-error-HTLC0x8050100f/m-p/183569#M8204</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;By reverse engineering in found that the redundant boot is only implemented for the E-boot section.&lt;/P&gt;&lt;P&gt;I make a new update tool for updating the WinCe section, but this is not redundant.&lt;/P&gt;&lt;P&gt;Marc&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Sep 2012 07:39:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/WinCE-Redundant-boot-on-I-MX28-Rom-code-error-HTLC0x8050100f/m-p/183569#M8204</guid>
      <dc:creator>MarcCoussement</dc:creator>
      <dc:date>2012-09-06T07:39:41Z</dc:date>
    </item>
    <item>
      <title>Re: WinCE Redundant boot on I.MX28 Rom code error HTLC0x8050100f</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/WinCE-Redundant-boot-on-I-MX28-Rom-code-error-HTLC0x8050100f/m-p/183570#M8205</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Marc,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I realise this post is a few years old but I wondered if you managed to write a tool for updating Windows CE on the iMX28? We are looking to do the same thing and I have a few ideas on how to go about it but wondered if you managed to create a working tool?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Aug 2015 11:29:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/WinCE-Redundant-boot-on-I-MX28-Rom-code-error-HTLC0x8050100f/m-p/183570#M8205</guid>
      <dc:creator>markwilliams</dc:creator>
      <dc:date>2015-08-19T11:29:46Z</dc:date>
    </item>
  </channel>
</rss>