<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic usbnet kernel module missing in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/usbnet-kernel-module-missing/m-p/505404#M82020</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have successfully built latest kernel images for an IMX6q sabrelite using the 4.5.0 release and again using 3.19 release as per DOC-95015 and they seem to work fine except that the usbnet kernel module is missing. Is there a specific configuration flag that needs to be set to ensure that it gets built in?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have used u-boot v2016.03 and I am running latest Debian Jessie having followed DOC-95015 and DOC-95044.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Wishes,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Harry&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 06 May 2016 08:07:36 GMT</pubDate>
    <dc:creator>harryduncan</dc:creator>
    <dc:date>2016-05-06T08:07:36Z</dc:date>
    <item>
      <title>usbnet kernel module missing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/usbnet-kernel-module-missing/m-p/505404#M82020</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have successfully built latest kernel images for an IMX6q sabrelite using the 4.5.0 release and again using 3.19 release as per DOC-95015 and they seem to work fine except that the usbnet kernel module is missing. Is there a specific configuration flag that needs to be set to ensure that it gets built in?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have used u-boot v2016.03 and I am running latest Debian Jessie having followed DOC-95015 and DOC-95044.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Wishes,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Harry&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 May 2016 08:07:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/usbnet-kernel-module-missing/m-p/505404#M82020</guid>
      <dc:creator>harryduncan</dc:creator>
      <dc:date>2016-05-06T08:07:36Z</dc:date>
    </item>
    <item>
      <title>Re: usbnet kernel module missing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/usbnet-kernel-module-missing/m-p/505405#M82021</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Fixed it. I had cross complied but had not copied the loadable kernel modules into /lib/modules/4.5.0 on the IMX6 cards. Once I did that they were all available to load. I also included USB_NET_DRIVERS=y in the build of the kernel as this is apparently a recent make menu option. The kernel modules are also gathered in one place using make modules_install but that will be located in the /lib/modules directory of the host that the build is being performed on.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 May 2016 17:01:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/usbnet-kernel-module-missing/m-p/505405#M82021</guid>
      <dc:creator>harryduncan</dc:creator>
      <dc:date>2016-05-06T17:01:36Z</dc:date>
    </item>
  </channel>
</rss>