<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Stuck up at 'starting kernel'  in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Stuck-up-at-starting-kernel/m-p/504982#M81951</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; If a board boots u-boot but stops at “Starting kernel ...”, it may be possible to read the&lt;/P&gt;&lt;P&gt;kernel log_buffer. To view memory dump (say in ASCII) at the needed address, assuming&lt;/P&gt;&lt;P&gt;memory still contains log information from the previous boot.&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; To find the __log_buf address, please use readelf utility :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;$ readelf -s vmlinux | grep __log_buf&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then, don’t power off the board, just reset it, and read the&lt;/P&gt;&lt;P&gt;(__log_buf) address on JTAG or u-boot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Please try it.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 12 Feb 2016 03:51:36 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2016-02-12T03:51:36Z</dc:date>
    <item>
      <title>Stuck up at 'starting kernel'</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Stuck-up-at-starting-kernel/m-p/504981#M81950</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Everyone,&lt;/P&gt;&lt;P&gt;We are testing a custom board designed using imx6 dual processor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have modified the u-boot and device tree file as per our design. We have the kernel and rootfs on SD card.&lt;/P&gt;&lt;P&gt;We are loading the u-boot using mfgtool.&lt;/P&gt;&lt;P&gt;The code hangs after 'starting kernel'. The log is as follows:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/****************************************************************************************************/&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;U-Boot 2015.07 (Feb 10 2016 - 12:14:42 +0530)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CPU:&amp;nbsp;&amp;nbsp; Freescale i.MX6D rev1.5 996 MHz (running at 792 MHz)&lt;/P&gt;&lt;P&gt;Reset cause: POR&lt;/P&gt;&lt;P&gt;Board: SABRE Lite&lt;/P&gt;&lt;P&gt;I2C:&amp;nbsp;&amp;nbsp; ready&lt;/P&gt;&lt;P&gt;DRAM:&amp;nbsp; 1 GiB&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MMC:&amp;nbsp;&amp;nbsp; FSL_SDHC: 0, FSL_SDHC: 1&lt;/P&gt;&lt;P&gt;SF: Unsupported flash IDs: manuf 00, jedec 0000, ext_jedec 0000&lt;/P&gt;&lt;P&gt;*** Warning - spi_flash_probe() failed, using default environment&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;auto-detected panel hannstar7&lt;/P&gt;&lt;P&gt;Display: lvds:hannstar7 (1280x800)&lt;/P&gt;&lt;P&gt;In:&amp;nbsp;&amp;nbsp;&amp;nbsp; serial&lt;/P&gt;&lt;P&gt;Out:&amp;nbsp;&amp;nbsp; serial&lt;/P&gt;&lt;P&gt;Err:&amp;nbsp;&amp;nbsp; serial&lt;/P&gt;&lt;P&gt;Net:&amp;nbsp;&amp;nbsp; Phy 4 not found&lt;/P&gt;&lt;P&gt;using phy at 4&lt;/P&gt;&lt;P&gt;PHY reset timed out&lt;/P&gt;&lt;P&gt;FEC [PRIME]&lt;/P&gt;&lt;P&gt;Error: FEC address not set.&lt;/P&gt;&lt;P&gt;, usb_ether&lt;/P&gt;&lt;P&gt;Error: usb_ether address not set.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hit any key to stop autoboot:&amp;nbsp; 3&amp;nbsp; 2&amp;nbsp; 1&amp;nbsp; 0 &lt;/P&gt;&lt;P&gt;AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode&lt;/P&gt;&lt;P&gt;flags: ncq stag pm led clo only pmp pio slum part &lt;/P&gt;&lt;P&gt;No port device detected!&lt;/P&gt;&lt;P&gt;** Bad device size - sata 0 **&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SATA device 1: unknown device&lt;/P&gt;&lt;P&gt;** Bad device sata 1 **&lt;/P&gt;&lt;P&gt;switch to partitions #0, OK&lt;/P&gt;&lt;P&gt;mmc0 is current device&lt;/P&gt;&lt;P&gt;reading /6x_bootscript&lt;/P&gt;&lt;P&gt;2933 bytes read in 22 ms (129.9 KiB/s)&lt;/P&gt;&lt;P&gt;## Executing script at 10008000&lt;/P&gt;&lt;P&gt;reading uEnv.txt&lt;/P&gt;&lt;P&gt;** Unable to read file uEnv.txt **&lt;/P&gt;&lt;P&gt;reading /imx6q-sabrelite.dtb&lt;/P&gt;&lt;P&gt;42516 bytes read in 28 ms (1.4 MiB/s)&lt;/P&gt;&lt;P&gt;Setting bus to 1&lt;/P&gt;&lt;P&gt;Error writing the chip: -19&lt;/P&gt;&lt;P&gt;only CEA modes allowed on HDMI port&lt;/P&gt;&lt;P&gt;reading /zImage&lt;/P&gt;&lt;P&gt;4954080 bytes read in 331 ms (14.3 MiB/s)&lt;/P&gt;&lt;P&gt;Kernel image @ 0x10800000 [ 0x000000 - 0x4b97e0 ]&lt;/P&gt;&lt;P&gt;## Flattened Device Tree blob at 13000000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Booting using the fdt blob at 0x13000000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; reserving fdt memory region: addr=13000000 size=b000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Using Device Tree in place at 13000000, end 1300dfff&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Starting kernel ...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/****************************************************************************************************/&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The sd card port is USDHC2.&lt;/P&gt;&lt;P&gt;We have tried following few posts with the same issues, but with no success.&lt;/P&gt;&lt;P&gt;Please let us know the other dependencies for booting kernel image.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Feb 2016 03:28:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Stuck-up-at-starting-kernel/m-p/504981#M81950</guid>
      <dc:creator>tejummb</dc:creator>
      <dc:date>2016-02-12T03:28:13Z</dc:date>
    </item>
    <item>
      <title>Re: Stuck up at 'starting kernel'</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Stuck-up-at-starting-kernel/m-p/504982#M81951</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; If a board boots u-boot but stops at “Starting kernel ...”, it may be possible to read the&lt;/P&gt;&lt;P&gt;kernel log_buffer. To view memory dump (say in ASCII) at the needed address, assuming&lt;/P&gt;&lt;P&gt;memory still contains log information from the previous boot.&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; To find the __log_buf address, please use readelf utility :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;$ readelf -s vmlinux | grep __log_buf&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then, don’t power off the board, just reset it, and read the&lt;/P&gt;&lt;P&gt;(__log_buf) address on JTAG or u-boot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Please try it.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Feb 2016 03:51:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Stuck-up-at-starting-kernel/m-p/504982#M81951</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-02-12T03:51:36Z</dc:date>
    </item>
    <item>
      <title>Re: Stuck up at 'starting kernel'</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Stuck-up-at-starting-kernel/m-p/504983#M81952</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yuri,&lt;/P&gt;&lt;P&gt;Where do I run this command?&lt;/P&gt;&lt;P&gt;I'm using mfgtool to load the u-boot.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Feb 2016 04:16:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Stuck-up-at-starting-kernel/m-p/504983#M81952</guid>
      <dc:creator>tejummb</dc:creator>
      <dc:date>2016-02-12T04:16:15Z</dc:date>
    </item>
    <item>
      <title>Re: Stuck up at 'starting kernel'</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Stuck-up-at-starting-kernel/m-p/504984#M81953</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Readelf should be run on host Linux, where the kernel was built.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Feb 2016 05:17:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Stuck-up-at-starting-kernel/m-p/504984#M81953</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-02-12T05:17:50Z</dc:date>
    </item>
    <item>
      <title>Re: Stuck up at 'starting kernel'</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Stuck-up-at-starting-kernel/m-p/504985#M81954</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yuri,&lt;/P&gt;&lt;P&gt;I apologize for the delay in my response.&lt;/P&gt;&lt;P&gt;Currently, we have updated u-boot and dts files for some minor changes in hardware, and with this setup, we are not even reaching kernel.&lt;/P&gt;&lt;P&gt;The log is as follows:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/********************************************************************************************************************/&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;U-Boot 2015.07 (Mar 11 2016 - 17:53:03 +0530)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CPU:&amp;nbsp;&amp;nbsp; Freescale i.MX6D rev1.5 996 MHz (running at 792 MHz)&lt;/P&gt;&lt;P&gt;Reset cause: POR&lt;/P&gt;&lt;P&gt;Board: SABRE Lite&lt;/P&gt;&lt;P&gt;I2C:&amp;nbsp;&amp;nbsp; ready&lt;/P&gt;&lt;P&gt;DRAM:&amp;nbsp; 1 GiB&lt;/P&gt;&lt;P&gt;MMC:&amp;nbsp;&amp;nbsp; FSL_SDHC: 0&lt;/P&gt;&lt;P&gt;SF: Unsupported flash IDs: manuf 00, jedec 0000, ext_jedec 0000&lt;/P&gt;&lt;P&gt;*** Warning - spi_flash_probe() failed, using default environment&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;auto-detected panel hannstar7&lt;/P&gt;&lt;P&gt;Display: lvds:hannstar7 (1280x800)&lt;/P&gt;&lt;P&gt;In:&amp;nbsp;&amp;nbsp;&amp;nbsp; serial&lt;/P&gt;&lt;P&gt;Out:&amp;nbsp;&amp;nbsp; serial&lt;/P&gt;&lt;P&gt;Err:&amp;nbsp;&amp;nbsp; serial&lt;/P&gt;&lt;P&gt;Net:&amp;nbsp;&amp;nbsp; Phy 4 not found&lt;/P&gt;&lt;P&gt;using phy at 4&lt;/P&gt;&lt;P&gt;PHY reset timed out&lt;/P&gt;&lt;P&gt;FEC [PRIME]&lt;/P&gt;&lt;P&gt;Error: FEC address not set.&lt;/P&gt;&lt;P&gt;, usb_ether&lt;/P&gt;&lt;P&gt;Error: usb_ether address not set.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hit any key to stop autoboot:&amp;nbsp; 3&amp;nbsp; 2&amp;nbsp; 1&amp;nbsp; 0 &lt;/P&gt;&lt;P&gt;AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode&lt;/P&gt;&lt;P&gt;flags: ncq stag pm led clo only pmp pio slum part &lt;/P&gt;&lt;P&gt;No port device detected!&lt;/P&gt;&lt;P&gt;** Bad device size - sata 0 **&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SATA device 1: unknown device&lt;/P&gt;&lt;P&gt;** Bad device sata 1 **&lt;/P&gt;&lt;P&gt;switch to partitions #0, OK&lt;/P&gt;&lt;P&gt;mmc0 is current device&lt;/P&gt;&lt;P&gt;reading /6x_bootscript&lt;/P&gt;&lt;P&gt;3124 bytes read in 19 ms (160.2 KiB/s)&lt;/P&gt;&lt;P&gt;## Executing script at 10008000&lt;/P&gt;&lt;P&gt;reading uEnv.txt&lt;/P&gt;&lt;P&gt;** Unable to read file uEnv.txt **&lt;/P&gt;&lt;P&gt;reading /imx6q-sabrelite.dtb&lt;/P&gt;&lt;P&gt;37414 bytes read in 22 ms (1.6 MiB/s)&lt;/P&gt;&lt;P&gt;Setting bus to 1&lt;/P&gt;&lt;P&gt;Error writing the chip: -19&lt;/P&gt;&lt;P&gt;only CEA modes allowed on HDMI port&lt;/P&gt;&lt;P&gt;reading /zImage&lt;/P&gt;&lt;P&gt;** Unable to read file /zImage **&lt;/P&gt;&lt;P&gt;Error loading kernel image&lt;/P&gt;&lt;P&gt;MMC Device 1 not found&lt;/P&gt;&lt;P&gt;no mmc device at slot slot slot ::::: 1&lt;/P&gt;&lt;P&gt;MMC Device 1 not found&lt;/P&gt;&lt;P&gt;** Bad device mmc 1 **&lt;/P&gt;&lt;P&gt;starting USB...&lt;/P&gt;&lt;P&gt;USB0:&amp;nbsp;&amp;nbsp; Port not available.&lt;/P&gt;&lt;P&gt;USB1:&amp;nbsp;&amp;nbsp; USB EHCI 1.00&lt;/P&gt;&lt;P&gt;scanning bus 1 for devices... 1 USB Device(s) found&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; scanning usb for storage devices... 0 Storage Device(s) found&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; scanning usb for ethernet devices... 0 Ethernet Device(s) found&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;USB device 0: unknown device&lt;/P&gt;&lt;P&gt;** Bad device usb 0 **&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;USB device 1: unknown device&lt;/P&gt;&lt;P&gt;** Bad device usb 1 **&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;6x_bootscript not found&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;serial console at 115200, 8N1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;details at &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.freescale.com/external-link.jspa?url=http%3A%2F%2Fboundarydevices.com%2F6q_bootscript" rel="nofollow" target="_blank"&gt;http://boundarydevices.com/6q_bootscript&lt;/A&gt;&lt;/P&gt;&lt;P&gt;AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode&lt;/P&gt;&lt;P&gt;flags: ncq stag pm led clo only pmp pio slum part &lt;/P&gt;&lt;P&gt;No port device detected!&lt;/P&gt;&lt;P&gt;AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode&lt;/P&gt;&lt;P&gt;flags: ncq stag pm led clo only pmp pio slum part &lt;/P&gt;&lt;P&gt;No port device detected!&lt;/P&gt;&lt;P&gt;switch to partitions #0, OK&lt;/P&gt;&lt;P&gt;mmc0 is current device&lt;/P&gt;&lt;P&gt;expose mmc 0 over USB&lt;/P&gt;&lt;P&gt;UMS: disk start sector: 0x0, count: 0x1dacc00&lt;/P&gt;&lt;P&gt;|/-\|/-\/-\|/-\/-\|/-\/-\|/-\/-\|/-\/-\|/-\/-\|/-\/-\|/-\/-\|/&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/*******************************************************************************************************************/&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the log shown above, the 6x_bootscript and dtb is read, but reading zImage fails.&lt;/P&gt;&lt;P&gt;Sometimes, even reading bootscript/dtb itself gives error.&lt;/P&gt;&lt;P&gt;Kindly, let us know what could be the issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Teju M M B&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Mar 2016 04:39:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Stuck-up-at-starting-kernel/m-p/504985#M81954</guid>
      <dc:creator>tejummb</dc:creator>
      <dc:date>2016-03-23T04:39:49Z</dc:date>
    </item>
    <item>
      <title>Re: Stuck up at 'starting kernel'</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Stuck-up-at-starting-kernel/m-p/504986#M81955</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; What is Your procedure to prepare boot device ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 May 2016 08:40:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Stuck-up-at-starting-kernel/m-p/504986#M81955</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-05-18T08:40:17Z</dc:date>
    </item>
  </channel>
</rss>