<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: I.MX6Q Linux Remote Processor Framework OpenAMP</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6Q-Linux-Remote-Processor-Framework-OpenAMP/m-p/504239#M81798</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tarek&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;unfortunately AMP is not supported for i.MX6DQ/SDL on official BSPs, one can look at&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-94513"&gt;Boot The i.mx6 dual With Linux+uC/OS-II AMP&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://community.arm.com/message/15766" rel="nofollow"&gt;http://community.arm.com/message/15766&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 11 Feb 2016 12:28:44 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2016-02-11T12:28:44Z</dc:date>
    <item>
      <title>I.MX6Q Linux Remote Processor Framework OpenAMP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6Q-Linux-Remote-Processor-Framework-OpenAMP/m-p/504238#M81797</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it possible to run the Linux driver "remoteproc" on iMX6Q SabreSD board?&lt;/P&gt;&lt;P&gt;I want Linux to run on cores0,1 and 2 while core 3 is dedicated to an RTOS.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The latest&amp;nbsp; Freescale kernel linux-imx does provide Remoteproc as a module and a modified Rpmsg.&lt;/P&gt;&lt;P&gt;In chapter 53, in the Linux reference manual there is a brief description on&amp;nbsp; how to use RPmsg for i.MX7 and i.MX6SoloX but nothing about i.MX6Q.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there a similar example for i.MX6Q? If not can you please give me some guide to port the existing code from i.MX7 to i.MX6Q?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Tarek&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Feb 2016 09:54:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6Q-Linux-Remote-Processor-Framework-OpenAMP/m-p/504238#M81797</guid>
      <dc:creator>Tarek</dc:creator>
      <dc:date>2016-02-11T09:54:45Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX6Q Linux Remote Processor Framework OpenAMP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6Q-Linux-Remote-Processor-Framework-OpenAMP/m-p/504239#M81798</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tarek&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;unfortunately AMP is not supported for i.MX6DQ/SDL on official BSPs, one can look at&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-94513"&gt;Boot The i.mx6 dual With Linux+uC/OS-II AMP&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://community.arm.com/message/15766" rel="nofollow"&gt;http://community.arm.com/message/15766&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Feb 2016 12:28:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6Q-Linux-Remote-Processor-Framework-OpenAMP/m-p/504239#M81798</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-02-11T12:28:44Z</dc:date>
    </item>
  </channel>
</rss>