<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックethernet: Varying network bandwith @TCP/IP stack level</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/ethernet-Varying-network-bandwith-TCP-IP-stack-level/m-p/504212#M81795</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working on a custom platform based on i.MX6Q Sabresd SD. The software running on the platform is Yocto BSP kernel version 3.14.28 from Freescale.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The custom platform has an on board ethernet controller which is connected to i.MX6Q via local bus(EIM) and we were&amp;nbsp; able to establish network connectivity. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to understand on how to vary the network bandwidth at TCP/IP stack level inside kernel. Say for example, I would like to&amp;nbsp; vary the link bandwidth from Gigabit to 10Mbpps Half/Full Duplex. Many people used ethtool to vary the bandwidth, However it hides the kernel internals. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any pointers on how to vary the bandwidth @ TCP/IP level would be appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Shajin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 26 May 2016 09:58:23 GMT</pubDate>
    <dc:creator>shajinas</dc:creator>
    <dc:date>2016-05-26T09:58:23Z</dc:date>
    <item>
      <title>ethernet: Varying network bandwith @TCP/IP stack level</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ethernet-Varying-network-bandwith-TCP-IP-stack-level/m-p/504212#M81795</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working on a custom platform based on i.MX6Q Sabresd SD. The software running on the platform is Yocto BSP kernel version 3.14.28 from Freescale.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The custom platform has an on board ethernet controller which is connected to i.MX6Q via local bus(EIM) and we were&amp;nbsp; able to establish network connectivity. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to understand on how to vary the network bandwidth at TCP/IP stack level inside kernel. Say for example, I would like to&amp;nbsp; vary the link bandwidth from Gigabit to 10Mbpps Half/Full Duplex. Many people used ethtool to vary the bandwidth, However it hides the kernel internals. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any pointers on how to vary the bandwidth @ TCP/IP level would be appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Shajin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 May 2016 09:58:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ethernet-Varying-network-bandwith-TCP-IP-stack-level/m-p/504212#M81795</guid>
      <dc:creator>shajinas</dc:creator>
      <dc:date>2016-05-26T09:58:23Z</dc:date>
    </item>
    <item>
      <title>Re: ethernet: Varying network bandwith @TCP/IP stack level</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ethernet-Varying-network-bandwith-TCP-IP-stack-level/m-p/504213#M81796</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There is nothing special to i.MX.&lt;/P&gt;&lt;P&gt;You can limit network bandwidth using Linux "tc" utility.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 May 2016 08:47:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ethernet-Varying-network-bandwith-TCP-IP-stack-level/m-p/504213#M81796</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2016-05-27T08:47:27Z</dc:date>
    </item>
  </channel>
</rss>