<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: iMX6 Boot Pin configuration, USB OTG</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-Boot-Pin-configuration-USB-OTG/m-p/503785#M81677</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Enrique&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;right, with BOOT [1:0] = 10 and other boot cfg pins set to boot from SD&lt;/P&gt;&lt;P&gt;image will be executed from the SD Card.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 24 Dec 2015 01:38:42 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2015-12-24T01:38:42Z</dc:date>
    <item>
      <title>iMX6 Boot Pin configuration, USB OTG</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-Boot-Pin-configuration-USB-OTG/m-p/503784#M81676</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;When I designed my IMX6 board I made the USB OTG port permanently configured to be a host, as this is how it will be used in our product.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In bringing up the board I see that the i.MX6 uses this port in OTG mode to make the board a device and to be able to download the bootloader using this USB port.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to confirm that if the BOOT PINS are configured as BOOT [1:0] = 10 and the rest of the boot cfg pins are set to boot from SD Card that we should still be able to compile and build an image that can be executed from the SD Card?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Dec 2015 18:16:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-Boot-Pin-configuration-USB-OTG/m-p/503784#M81676</guid>
      <dc:creator>enriqueencarnac</dc:creator>
      <dc:date>2015-12-23T18:16:22Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 Boot Pin configuration, USB OTG</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-Boot-Pin-configuration-USB-OTG/m-p/503785#M81677</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Enrique&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;right, with BOOT [1:0] = 10 and other boot cfg pins set to boot from SD&lt;/P&gt;&lt;P&gt;image will be executed from the SD Card.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Dec 2015 01:38:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-Boot-Pin-configuration-USB-OTG/m-p/503785#M81677</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-12-24T01:38:42Z</dc:date>
    </item>
  </channel>
</rss>