<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: imx6 increase sched_clock resolution in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx6-increase-sched-clock-resolution/m-p/503689#M81663</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi arash&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please refer to attached Linux Manual&lt;/P&gt;&lt;P&gt;sect.3.3.3 Timer Source Code Structure&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 23 Dec 2015 12:20:46 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2015-12-23T12:20:46Z</dc:date>
    <item>
      <title>imx6 increase sched_clock resolution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-increase-sched-clock-resolution/m-p/503688#M81662</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My Env.:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Board: Boundary Device Nitrogen Max&lt;/P&gt;&lt;P&gt;Kernel: 3.14.28&lt;/P&gt;&lt;P&gt;OS:&amp;nbsp; Debian 8&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;right now my Sched_clock read from dmesg is:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655765682ns&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;how/where in kernel source can i increase the timer resolution?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Dec 2015 11:03:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-increase-sched-clock-resolution/m-p/503688#M81662</guid>
      <dc:creator>arashjavanmard</dc:creator>
      <dc:date>2015-12-23T11:03:14Z</dc:date>
    </item>
    <item>
      <title>Re: imx6 increase sched_clock resolution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-increase-sched-clock-resolution/m-p/503689#M81663</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi arash&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please refer to attached Linux Manual&lt;/P&gt;&lt;P&gt;sect.3.3.3 Timer Source Code Structure&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Dec 2015 12:20:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-increase-sched-clock-resolution/m-p/503689#M81663</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-12-23T12:20:46Z</dc:date>
    </item>
  </channel>
</rss>