<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Customizing Kernel</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Customizing-Kernel/m-p/503364#M81554</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Senthil &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which BSP you are using?&lt;/P&gt;&lt;P&gt;There is configuration file in the kernel ,which is used to enable and disable feature in kernel.&lt;/P&gt;&lt;P&gt;check kernel_imx/arch/arm/configs/imx_v7_defconfig&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Saurabh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 06 May 2016 05:43:05 GMT</pubDate>
    <dc:creator>saurabh206</dc:creator>
    <dc:date>2016-05-06T05:43:05Z</dc:date>
    <item>
      <title>Customizing Kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Customizing-Kernel/m-p/503363#M81553</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Which parameters I need to change on Kernel(Or any related Files) if I need to customize my OS{Linux},like I don't want few process to run always in my machine,which is affecting my performance?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 May 2016 03:52:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Customizing-Kernel/m-p/503363#M81553</guid>
      <dc:creator>senthilkumar_s1</dc:creator>
      <dc:date>2016-05-06T03:52:11Z</dc:date>
    </item>
    <item>
      <title>Re: Customizing Kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Customizing-Kernel/m-p/503364#M81554</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Senthil &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which BSP you are using?&lt;/P&gt;&lt;P&gt;There is configuration file in the kernel ,which is used to enable and disable feature in kernel.&lt;/P&gt;&lt;P&gt;check kernel_imx/arch/arm/configs/imx_v7_defconfig&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Saurabh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 May 2016 05:43:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Customizing-Kernel/m-p/503364#M81554</guid>
      <dc:creator>saurabh206</dc:creator>
      <dc:date>2016-05-06T05:43:05Z</dc:date>
    </item>
    <item>
      <title>Re: Customizing Kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Customizing-Kernel/m-p/503365#M81555</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There is nothing special regarding to i.MX. I can provide you some common recomendations.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. Linux kernel.&lt;/P&gt;&lt;P&gt;You can remove all unnessesary options and modules from the kernel.&lt;/P&gt;&lt;P&gt;For example if you do not need ethernet you can compile the kernel without its support.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. OS.&lt;/P&gt;&lt;P&gt;You can remove all unnessesary services from startup.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3. hardware.&lt;/P&gt;&lt;P&gt;You can attach some effective radiator to the processor and set maximum frequencies.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 May 2016 08:50:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Customizing-Kernel/m-p/503365#M81555</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2016-05-06T08:50:24Z</dc:date>
    </item>
    <item>
      <title>Re: Customizing Kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Customizing-Kernel/m-p/503366#M81556</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Victor,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Thanks for your reply.Can you please elaborate the steps where I need to edit (File location) and what to edit(Parameters)?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 May 2016 10:26:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Customizing-Kernel/m-p/503366#M81556</guid>
      <dc:creator>senthilkumar_s1</dc:creator>
      <dc:date>2016-05-06T10:26:40Z</dc:date>
    </item>
  </channel>
</rss>