<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックAPBH_DMA USED FOR GPMI</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/APBH-DMA-USED-FOR-GPMI/m-p/503345#M81544</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I read the ”iMX6_Firmware_Guide.pdf“, and I am curious about the DMA command structure uesd in gpmi driver, can I just use the struct "GENERIC_DESCRIPTOR" to operate the DMA channel without using the register such as next command address register.&lt;/P&gt;&lt;P&gt;where can I find the include files used in the test driver, and is there source code related to the code written in the ”iMX6_Firmware_Guide.pdf“?&lt;/P&gt;&lt;P&gt;I am really looking forward to the reply, thanks a lot!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 25 Mar 2016 05:51:12 GMT</pubDate>
    <dc:creator>michaelsyh</dc:creator>
    <dc:date>2016-03-25T05:51:12Z</dc:date>
    <item>
      <title>APBH_DMA USED FOR GPMI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/APBH-DMA-USED-FOR-GPMI/m-p/503345#M81544</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I read the ”iMX6_Firmware_Guide.pdf“, and I am curious about the DMA command structure uesd in gpmi driver, can I just use the struct "GENERIC_DESCRIPTOR" to operate the DMA channel without using the register such as next command address register.&lt;/P&gt;&lt;P&gt;where can I find the include files used in the test driver, and is there source code related to the code written in the ”iMX6_Firmware_Guide.pdf“?&lt;/P&gt;&lt;P&gt;I am really looking forward to the reply, thanks a lot!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Mar 2016 05:51:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/APBH-DMA-USED-FOR-GPMI/m-p/503345#M81544</guid>
      <dc:creator>michaelsyh</dc:creator>
      <dc:date>2016-03-25T05:51:12Z</dc:date>
    </item>
    <item>
      <title>Re: APBH_DMA USED FOR GPMI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/APBH-DMA-USED-FOR-GPMI/m-p/503346#M81545</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Please create request in order to get the Platform SDK sources.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-329745"&gt;How to submit a new question for NXP Support&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Mar 2016 06:07:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/APBH-DMA-USED-FOR-GPMI/m-p/503346#M81545</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-03-25T06:07:04Z</dc:date>
    </item>
  </channel>
</rss>