<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: ZMK programming in imx6 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/ZMK-programming-in-imx6/m-p/503344#M81543</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Rohini&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;system reset can be performed only with POR assertion.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 24 Dec 2015 01:35:46 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2015-12-24T01:35:46Z</dc:date>
    <item>
      <title>ZMK programming in imx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ZMK-programming-in-imx6/m-p/503343#M81542</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I want to program ZMK using software. But my SNV_HPLR write lock bit is set and it can be cleared only by a system reset. So how can I do this system reset? Any help is appreciated. Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Dec 2015 13:13:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ZMK-programming-in-imx6/m-p/503343#M81542</guid>
      <dc:creator>rohininarasipur</dc:creator>
      <dc:date>2015-12-23T13:13:59Z</dc:date>
    </item>
    <item>
      <title>Re: ZMK programming in imx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ZMK-programming-in-imx6/m-p/503344#M81543</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Rohini&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;system reset can be performed only with POR assertion.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Dec 2015 01:35:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ZMK-programming-in-imx6/m-p/503344#M81543</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-12-24T01:35:46Z</dc:date>
    </item>
  </channel>
</rss>