<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Display Flickering</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Display-Flickering/m-p/183330#M8153</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank u...Problem has been solved&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 24 Aug 2012 06:32:43 GMT</pubDate>
    <dc:creator>Nagesh</dc:creator>
    <dc:date>2012-08-24T06:32:43Z</dc:date>
    <item>
      <title>Display Flickering</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Display-Flickering/m-p/183326#M8149</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;We are using the i.MX233 processor in our design.  As far as the finctionalities are concerned everything seems to be working fine.We have observed a peculiar problem with LCD.When we shake the device OR move the device fast in horizontal direction, the screen updates(as flickering) are visible to bare eyes.We are not able to identify what is causing this problem. The same behaviour also observed on i.MX233 evaluation Kit.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Aug 2012 12:23:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Display-Flickering/m-p/183326#M8149</guid>
      <dc:creator>Nagesh</dc:creator>
      <dc:date>2012-08-21T12:23:25Z</dc:date>
    </item>
    <item>
      <title>Re: Display Flickering</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Display-Flickering/m-p/183327#M8150</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You need use high LCD&amp;nbsp;refresh rate. Try use 85Hz or higher.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Aug 2012 13:24:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Display-Flickering/m-p/183327#M8150</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2012-08-22T13:24:52Z</dc:date>
    </item>
    <item>
      <title>Re: Display Flickering</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Display-Flickering/m-p/183328#M8151</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HW to increase refresh rate to 85Hz??&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Specs of LCD which i am using:&lt;/P&gt;&lt;P&gt;Resolution:320*240&lt;/P&gt;&lt;P&gt;Bus width:16bit&lt;/P&gt;&lt;P&gt;pixel clock:5 to 6.8MHz&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried with increasing pixel clock upto 8MHz then also Flicker problem is still present.The same problem is even present in the i.MX233EVK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Refresh rate= pixel clock/number of clocks per frame&lt;/P&gt;&lt;P&gt;I increased the pixel clock which in turn increases the refresh rate.Then also &amp;nbsp;problem was still there.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any other parameter to increase refresh rate or is it some other parameter which is causing this problem?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Aug 2012 17:27:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Display-Flickering/m-p/183328#M8151</guid>
      <dc:creator>Nagesh</dc:creator>
      <dc:date>2012-08-22T17:27:04Z</dc:date>
    </item>
    <item>
      <title>Re: Display Flickering</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Display-Flickering/m-p/183329#M8152</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Perhaps we have so called stroboscopic effect because of external light flickering.&lt;BR /&gt; In such case display refresh frequency should not be a multiple of the frequency of light (60 hz).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Aug 2012 03:08:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Display-Flickering/m-p/183329#M8152</guid>
      <dc:creator>YuriMuhin_ng</dc:creator>
      <dc:date>2012-08-23T03:08:46Z</dc:date>
    </item>
    <item>
      <title>Re: Display Flickering</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Display-Flickering/m-p/183330#M8153</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank u...Problem has been solved&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Aug 2012 06:32:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Display-Flickering/m-p/183330#M8153</guid>
      <dc:creator>Nagesh</dc:creator>
      <dc:date>2012-08-24T06:32:43Z</dc:date>
    </item>
    <item>
      <title>Re: Display Flickering</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Display-Flickering/m-p/183331#M8154</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Nagesh,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; We are using imx233 processor and LCD display with the spec:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Resolution:320*240&lt;/P&gt;&lt;P&gt;Bus width:16bit&lt;/P&gt;&lt;P&gt;pixel clock:5 to 6.8MHz&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; LCD Display will start to flicker when control is transferred&amp;nbsp; from bootloader to O.S , where frame buffer starting address will be changed. Please tell me what solution you are followed&amp;nbsp; to overcome your problem , which may help&amp;nbsp; to solve our problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Kishore P&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Oct 2015 06:33:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Display-Flickering/m-p/183331#M8154</guid>
      <dc:creator>kishorepoojari</dc:creator>
      <dc:date>2015-10-16T06:33:40Z</dc:date>
    </item>
    <item>
      <title>Re: Display Flickering</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Display-Flickering/m-p/183332#M8155</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;As per my experience you must try the high LCD refresh rate. It must be 85Hz or greater.&lt;/P&gt;&lt;P&gt;Use this one Refresh rate= pixel clock/number of clocks per frame.&lt;/P&gt;&lt;P&gt;It is also called stroboscopic effect because of external light flickering.&lt;/P&gt;&lt;P&gt;For this the display refresh frequency should not be a multiple of the frequency of light.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Oct 2015 07:08:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Display-Flickering/m-p/183332#M8155</guid>
      <dc:creator>ervingattis</dc:creator>
      <dc:date>2015-10-16T07:08:49Z</dc:date>
    </item>
    <item>
      <title>Re: Display Flickering</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Display-Flickering/m-p/183333#M8156</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Ervin ,&lt;/P&gt;&lt;P&gt;&amp;nbsp; We are facing flickering problem only when control is transferred&amp;nbsp; from bootloader to O.S , where frame buffer starting address will be switched (From BL to OS).&lt;/P&gt;&lt;P&gt;Once KIOSK application is up their is no flickering is observed . Is their any solution to avoid the flickering while switching the frame buffer starting address.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Kishore P&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Oct 2015 12:33:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Display-Flickering/m-p/183333#M8156</guid>
      <dc:creator>kishorepoojari</dc:creator>
      <dc:date>2015-10-16T12:33:26Z</dc:date>
    </item>
  </channel>
</rss>