<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IMX6.Q  VPU  encode double video  in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-Q-VPU-encode-double-video/m-p/503202#M81517</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Richard&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;reason may be that dual (1280*1080 25 FPS &amp;amp; 1280*960 25FPS)&lt;/P&gt;&lt;P&gt;encode is close to VPU performance max. limit 1080p@30fps, this&lt;/P&gt;&lt;P&gt;is described on p.6 presentation&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;A href="https://community.nxp.com/docs/DOC-95595"&gt;Q&amp;amp;amp;A: MX6 VPU H.264 Dual Stream Encode Limits&lt;/A&gt;&lt;/P&gt;&lt;P&gt;so one can test this case with unit tests mxc_vpu_test&lt;/P&gt;&lt;P&gt;&lt;A href="http://repository.timesys.com/buildsources/i/imx-test/imx-test-3.10.17-1.0.0/" title="http://repository.timesys.com/buildsources/i/imx-test/imx-test-3.10.17-1.0.0/"&gt;Index of /buildsources/i/imx-test/imx-test-3.10.17-1.0.0&lt;/A&gt;&lt;/P&gt;&lt;P&gt;if perfomance is insufficient, decrease fps.&lt;/P&gt;&lt;P&gt;For bitrate seting refer to sect.3.2.2.11 EncOpenParam&lt;/P&gt;&lt;P&gt;attached VPU Programming Manual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 20 Jan 2016 11:22:05 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2016-01-20T11:22:05Z</dc:date>
    <item>
      <title>IMX6.Q  VPU  encode double video</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-Q-VPU-encode-double-video/m-p/503201#M81516</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,ALL&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I'm working on&amp;nbsp; IMX6Q kernel:3.10.17&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I have double camera ,there are&amp;nbsp; DVP and&amp;nbsp; MIPI port, output ：1280*1080 25 FPS&amp;nbsp; and&amp;nbsp; 1280*960 25FPS&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &lt;SPAN style="color: #e23d39;"&gt; the&amp;nbsp; problem&lt;/SPAN&gt; is : the vpu encode is not smooth enough,&amp;nbsp; some time ,encode a frame need more then 40ms, how can i fixed this problem?&lt;/P&gt;&lt;P&gt; how about change the vpu input clk?&amp;nbsp; or&amp;nbsp; change the encode &lt;SPAN style="color: #e23d39;"&gt;bitrate_level &lt;SPAN style="color: #303030;"&gt;? but, I didn't get the interface to change the bitrate_level。。&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #303030;"&gt; anyone can help me?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #303030;"&gt;thank you very much!&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Jan 2016 10:37:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-Q-VPU-encode-double-video/m-p/503201#M81516</guid>
      <dc:creator>richarddestiny</dc:creator>
      <dc:date>2016-01-20T10:37:57Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6.Q  VPU  encode double video</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-Q-VPU-encode-double-video/m-p/503202#M81517</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Richard&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;reason may be that dual (1280*1080 25 FPS &amp;amp; 1280*960 25FPS)&lt;/P&gt;&lt;P&gt;encode is close to VPU performance max. limit 1080p@30fps, this&lt;/P&gt;&lt;P&gt;is described on p.6 presentation&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;A href="https://community.nxp.com/docs/DOC-95595"&gt;Q&amp;amp;amp;A: MX6 VPU H.264 Dual Stream Encode Limits&lt;/A&gt;&lt;/P&gt;&lt;P&gt;so one can test this case with unit tests mxc_vpu_test&lt;/P&gt;&lt;P&gt;&lt;A href="http://repository.timesys.com/buildsources/i/imx-test/imx-test-3.10.17-1.0.0/" title="http://repository.timesys.com/buildsources/i/imx-test/imx-test-3.10.17-1.0.0/"&gt;Index of /buildsources/i/imx-test/imx-test-3.10.17-1.0.0&lt;/A&gt;&lt;/P&gt;&lt;P&gt;if perfomance is insufficient, decrease fps.&lt;/P&gt;&lt;P&gt;For bitrate seting refer to sect.3.2.2.11 EncOpenParam&lt;/P&gt;&lt;P&gt;attached VPU Programming Manual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Jan 2016 11:22:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-Q-VPU-encode-double-video/m-p/503202#M81517</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-01-20T11:22:05Z</dc:date>
    </item>
  </channel>
</rss>