<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: How to Add packages to rootfs on gui?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-Add-packages-to-rootfs-on-gui/m-p/503010#M81460</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Eren,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You may still use HOB. It is deprecated but still working and will no longer be available in Poky 2.1 in favor of Toaster, which does not still have the same functionalities of HOB.&amp;nbsp; If you are using the Community BSP you should have no problem using HOB. Some problems were detected in Daisy for the BSP Release, with some posts in these communities showing some workarounds. I would recommend trying using it as this is the only GUI available for recipe customization as of today.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 30 Mar 2016 14:36:07 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2016-03-30T14:36:07Z</dc:date>
    <item>
      <title>How to Add packages to rootfs on gui?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-Add-packages-to-rootfs-on-gui/m-p/503008#M81458</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I couldn't find that how can I add package to rootfs on a GUI. I have no problem with addign package to local.conf but I need a GUI like buildroot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As I see, yocto doesn't support HOB on the latest version. Do you have any suggestion?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Eren&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Mar 2016 08:26:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-Add-packages-to-rootfs-on-gui/m-p/503008#M81458</guid>
      <dc:creator>erenbasturk</dc:creator>
      <dc:date>2016-03-25T08:26:35Z</dc:date>
    </item>
    <item>
      <title>Re: How to Add packages to rootfs on gui?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-Add-packages-to-rootfs-on-gui/m-p/503009#M81459</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Any suggestion?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 26 Mar 2016 15:11:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-Add-packages-to-rootfs-on-gui/m-p/503009#M81459</guid>
      <dc:creator>erenbasturk</dc:creator>
      <dc:date>2016-03-26T15:11:15Z</dc:date>
    </item>
    <item>
      <title>Re: How to Add packages to rootfs on gui?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-Add-packages-to-rootfs-on-gui/m-p/503010#M81460</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Eren,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You may still use HOB. It is deprecated but still working and will no longer be available in Poky 2.1 in favor of Toaster, which does not still have the same functionalities of HOB.&amp;nbsp; If you are using the Community BSP you should have no problem using HOB. Some problems were detected in Daisy for the BSP Release, with some posts in these communities showing some workarounds. I would recommend trying using it as this is the only GUI available for recipe customization as of today.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Mar 2016 14:36:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-Add-packages-to-rootfs-on-gui/m-p/503010#M81460</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2016-03-30T14:36:07Z</dc:date>
    </item>
  </channel>
</rss>