<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LCD_DATA vs RGB components in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/LCD-DATA-vs-RGB-components/m-p/502810#M81397</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; basically - yes ; but schematic should meet this configuration, and &lt;/P&gt;&lt;P&gt;it is needed to program this mapping.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 03 Mar 2016 08:07:16 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2016-03-03T08:07:16Z</dc:date>
    <item>
      <title>LCD_DATA vs RGB components</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LCD-DATA-vs-RGB-components/m-p/502807#M81394</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In my customer board which is iMX6UL based，DOTCLK mode with 18-bit is required. But I can not find the description of mapping of LCD_D[0..17] to RGB components in RM. Help is need, thanks in advance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cheng Shi&lt;/P&gt;&lt;P&gt;Emtronix&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Mar 2016 02:11:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LCD-DATA-vs-RGB-components/m-p/502807#M81394</guid>
      <dc:creator>x10</dc:creator>
      <dc:date>2016-03-03T02:11:14Z</dc:date>
    </item>
    <item>
      <title>Re: LCD_DATA vs RGB components</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LCD-DATA-vs-RGB-components/m-p/502808#M81395</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; the i.MX6 UL&amp;nbsp; eLCDIF provides flexible options for color_bits-to-pins mapping.&lt;/P&gt;&lt;P&gt;Please take a look at section 33.4.2 (Write Data Path) of the i.MX6 UL Reference&lt;/P&gt;&lt;P&gt;Manual for details regarding pixel data from frame buffer to LCD path. Data of &lt;/P&gt;&lt;P&gt;the frame buffer will be mapped to external LCD bus pins. In particularly, &lt;/P&gt;&lt;P&gt;"WORD_LENGTH=3 indicates that the input frame-buffer is RGB 24 bits per pixel &lt;/P&gt;&lt;P&gt;(RGB 888). If BYTE_PACKING_FORMAT [3:0] is 0x7, it indicates that there is only &lt;/P&gt;&lt;P&gt;one pixel per 32-bit word".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Mar 2016 04:03:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LCD-DATA-vs-RGB-components/m-p/502808#M81395</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-03-03T04:03:42Z</dc:date>
    </item>
    <item>
      <title>Re: LCD_DATA vs RGB components</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LCD-DATA-vs-RGB-components/m-p/502809#M81396</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Yuri&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;As my understanding, there are LCD_DATA[0..7] =&amp;gt; R[0..7], LCD_DATA[8..15] =&amp;gt; G[0..7], and LCD_DATA[16..23] =&amp;gt; B[0..7] in 24-bit DOTCLK mode. Is that right?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Cheng Shi&lt;/P&gt;&lt;P&gt;Emtronix&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Mar 2016 08:03:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LCD-DATA-vs-RGB-components/m-p/502809#M81396</guid>
      <dc:creator>x10</dc:creator>
      <dc:date>2016-03-03T08:03:30Z</dc:date>
    </item>
    <item>
      <title>Re: LCD_DATA vs RGB components</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LCD-DATA-vs-RGB-components/m-p/502810#M81397</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; basically - yes ; but schematic should meet this configuration, and &lt;/P&gt;&lt;P&gt;it is needed to program this mapping.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Mar 2016 08:07:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LCD-DATA-vs-RGB-components/m-p/502810#M81397</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-03-03T08:07:16Z</dc:date>
    </item>
    <item>
      <title>Re: LCD_DATA vs RGB components</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LCD-DATA-vs-RGB-components/m-p/502811#M81398</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Yuri&lt;/P&gt;&lt;P&gt;Are there any recommended mapping for 24-bit DOTCLK mode?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Cheng Shi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Mar 2016 08:13:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LCD-DATA-vs-RGB-components/m-p/502811#M81398</guid>
      <dc:creator>x10</dc:creator>
      <dc:date>2016-03-03T08:13:46Z</dc:date>
    </item>
    <item>
      <title>Re: LCD_DATA vs RGB components</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LCD-DATA-vs-RGB-components/m-p/502812#M81399</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to the i.MX6 UL EVK scheme :&lt;/P&gt;&lt;P&gt;LCD_DATA [0-7]&amp;nbsp; - B [0-7]&lt;/P&gt;&lt;P&gt;LCD_DATA [8-15]&amp;nbsp; - G [0-7]&lt;/P&gt;&lt;P&gt;LCD_DATA [16-23]&amp;nbsp; - R [0-7]&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Mar 2016 07:51:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LCD-DATA-vs-RGB-components/m-p/502812#M81399</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-03-15T07:51:35Z</dc:date>
    </item>
    <item>
      <title>Re: LCD_DATA vs RGB components</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LCD-DATA-vs-RGB-components/m-p/502813#M81400</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can confirm Yuri's answer. The data setup is :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;LCD_DATA [0-7]&amp;nbsp; - B [0-7]&lt;/P&gt;&lt;P&gt;LCD_DATA [8-15]&amp;nbsp; - G [0-7]&lt;/P&gt;&lt;P&gt;LCD_DATA [16-23]&amp;nbsp; - R [0-7]&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I've just connect my display to a 3'th party development board at this way.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards János&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Sep 2016 12:52:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LCD-DATA-vs-RGB-components/m-p/502813#M81400</guid>
      <dc:creator>julbert</dc:creator>
      <dc:date>2016-09-02T12:52:57Z</dc:date>
    </item>
  </channel>
</rss>