<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックIMX6Dual boot up issue</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Dual-boot-up-issue/m-p/502540#M81354</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We have a design that is using the MCIMX6U5DVM10AC device with PMIC MMPF0100F0AEP. We build 3 times pilot runs, however there is a serious problem right now. In some machines it get 1/350 chance to shut down on U-boot , and some machines seem to boot up always very well. so we trace the code to see which instruction is the shut down point. the shut down point is "read" a clock for IPU usage. it even not a "write "instruction but "read"&amp;nbsp; and shut down in the same one point everytime.&lt;/P&gt;&lt;P&gt;Is anyone who also meet this issue, or someone who can tell us what direction we can go for debugging. Many thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 23 Dec 2015 09:02:10 GMT</pubDate>
    <dc:creator>raehsu</dc:creator>
    <dc:date>2015-12-23T09:02:10Z</dc:date>
    <item>
      <title>IMX6Dual boot up issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Dual-boot-up-issue/m-p/502540#M81354</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We have a design that is using the MCIMX6U5DVM10AC device with PMIC MMPF0100F0AEP. We build 3 times pilot runs, however there is a serious problem right now. In some machines it get 1/350 chance to shut down on U-boot , and some machines seem to boot up always very well. so we trace the code to see which instruction is the shut down point. the shut down point is "read" a clock for IPU usage. it even not a "write "instruction but "read"&amp;nbsp; and shut down in the same one point everytime.&lt;/P&gt;&lt;P&gt;Is anyone who also meet this issue, or someone who can tell us what direction we can go for debugging. Many thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Dec 2015 09:02:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Dual-boot-up-issue/m-p/502540#M81354</guid>
      <dc:creator>raehsu</dc:creator>
      <dc:date>2015-12-23T09:02:10Z</dc:date>
    </item>
  </channel>
</rss>