<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 soc_camera on imx53</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/soc-camera-on-imx53/m-p/183264#M8132</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello I was hoping to get some help launching a soc_camera driver in linux.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The camera is an ov7725, using the ov772x driver under the soc_camera drivers in the kernel menu config.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've insmoded the driver onto the ubuntu start board rootfs. The problem is the platform data needed to launch the camera successfully.&lt;/P&gt;&lt;P&gt;Has anyone had luck using a soc camera driver with the imx53 using i2c and the csi interface.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If so what platform data did you give the driver in the board file?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;static void camera_pwdn(int pwdn)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;gpio_request(DISP0_RESET, "csi0-pwdn"); gpio_set_value(DISP0_RESET, pwdn); gpio_free(DISP0_RESET);&lt;/P&gt;&lt;P&gt;}&lt;BR /&gt;static struct mxc_camera_platform_data camera_data =&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;.analog_regulator = "DA9052_LDO7",&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;.core_regulator = "DA9052_LDO7",&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;.mclk = 24000000, .csi = 0,&lt;/P&gt;&lt;P&gt;.pwdn = camera_pwdn,&lt;/P&gt;&lt;P&gt;};&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;static struct i2c_board_info mxc_i2c1_board_info[] __initdata =&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;{ .type = "sgtl5000-i2c", .addr = 0x0a, },&lt;/P&gt;&lt;P&gt;{ .type = "sii9022", .addr = 0x39, .irq = IOMUX_TO_IRQ_V3(DISP0_DET_INT), .platform_data = &amp;amp;sii9022_hdmi_data, },&lt;/P&gt;&lt;P&gt;{ .type = "ov772x", .addr = 0x21, .platform_data = (void *)&amp;amp;camera_data, },&lt;/P&gt;&lt;P&gt;};&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 03 Nov 2011 16:57:34 GMT</pubDate>
    <dc:creator>JoshuaParrish</dc:creator>
    <dc:date>2011-11-03T16:57:34Z</dc:date>
    <item>
      <title>soc_camera on imx53</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/soc-camera-on-imx53/m-p/183264#M8132</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello I was hoping to get some help launching a soc_camera driver in linux.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The camera is an ov7725, using the ov772x driver under the soc_camera drivers in the kernel menu config.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've insmoded the driver onto the ubuntu start board rootfs. The problem is the platform data needed to launch the camera successfully.&lt;/P&gt;&lt;P&gt;Has anyone had luck using a soc camera driver with the imx53 using i2c and the csi interface.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If so what platform data did you give the driver in the board file?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;static void camera_pwdn(int pwdn)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;gpio_request(DISP0_RESET, "csi0-pwdn"); gpio_set_value(DISP0_RESET, pwdn); gpio_free(DISP0_RESET);&lt;/P&gt;&lt;P&gt;}&lt;BR /&gt;static struct mxc_camera_platform_data camera_data =&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;.analog_regulator = "DA9052_LDO7",&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;.core_regulator = "DA9052_LDO7",&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;.mclk = 24000000, .csi = 0,&lt;/P&gt;&lt;P&gt;.pwdn = camera_pwdn,&lt;/P&gt;&lt;P&gt;};&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;static struct i2c_board_info mxc_i2c1_board_info[] __initdata =&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;{ .type = "sgtl5000-i2c", .addr = 0x0a, },&lt;/P&gt;&lt;P&gt;{ .type = "sii9022", .addr = 0x39, .irq = IOMUX_TO_IRQ_V3(DISP0_DET_INT), .platform_data = &amp;amp;sii9022_hdmi_data, },&lt;/P&gt;&lt;P&gt;{ .type = "ov772x", .addr = 0x21, .platform_data = (void *)&amp;amp;camera_data, },&lt;/P&gt;&lt;P&gt;};&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Nov 2011 16:57:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/soc-camera-on-imx53/m-p/183264#M8132</guid>
      <dc:creator>JoshuaParrish</dc:creator>
      <dc:date>2011-11-03T16:57:34Z</dc:date>
    </item>
    <item>
      <title>Re: soc_camera on imx53</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/soc-camera-on-imx53/m-p/183265#M8133</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;soc camera framework was not used in FSL default BSP. If you want to use new camera sensor, you can refer to drivers/media/video/mxc/capture/ov5642.c for quick enablement.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Nov 2011 06:07:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/soc-camera-on-imx53/m-p/183265#M8133</guid>
      <dc:creator>LilyZhang</dc:creator>
      <dc:date>2011-11-04T06:07:11Z</dc:date>
    </item>
    <item>
      <title>Re: soc_camera on imx53</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/soc-camera-on-imx53/m-p/183266#M8134</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Are these drivers in the QSB install or are they in a download from FSL?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Mar 2012 18:00:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/soc-camera-on-imx53/m-p/183266#M8134</guid>
      <dc:creator>AaronLinsdau</dc:creator>
      <dc:date>2012-03-21T18:00:59Z</dc:date>
    </item>
    <item>
      <title>Re: soc_camera on imx53</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/soc-camera-on-imx53/m-p/183267#M8135</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The drivers can be found in the in the downloads from FSL. I liked building in the ubuntu vm. The build tools were already configured so it made everything easier.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Mar 2012 17:15:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/soc-camera-on-imx53/m-p/183267#M8135</guid>
      <dc:creator>JoshuaParrish</dc:creator>
      <dc:date>2012-03-28T17:15:53Z</dc:date>
    </item>
  </channel>
</rss>