<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic bitbake Error with i.MX6UL-EVK dtb in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/bitbake-Error-with-i-MX6UL-EVK-dtb/m-p/501983#M81289</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I ran bitbake last night for the i.MX6UL-EVK platform. The command was: bitbake core-image-base&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The repository has been synched before the build.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am following the steps in the document called: Freescale_Yocto_Project_User's_Guide.pdf&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have the following error:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;| NOTE: make -j 8 imx6ul-14x14-evk.dtb&lt;/P&gt;&lt;P&gt;| make[3]: *** &lt;STRONG&gt;No rule to make target `arch/arm/boot/dts/imx6ul-14x14-evk.dtb'&lt;/STRONG&gt;.&amp;nbsp; Stop.&lt;/P&gt;&lt;P&gt;| make[2]: *** [imx6ul-14x14-evk.dtb] Error 2&lt;/P&gt;&lt;P&gt;| make[1]: *** [sub-make] Error 2&lt;/P&gt;&lt;P&gt;| make: *** [all] Error 2&lt;/P&gt;&lt;P&gt;| ERROR: oe_runmake failed&lt;/P&gt;&lt;P&gt;| WARNING: exit code 1 from a shell command.&lt;/P&gt;&lt;P&gt;| ERROR: Function failed: do_install (log file is located at /home/mtoumi/yocto_base/fsl-release-bsp/build/tmp/work/imx6ulevk-poky-linux-gnueabi/linux-imx/&lt;STRONG&gt;3.14.28-r0&lt;/STRONG&gt;/temp/log.do_install.29429)&lt;/P&gt;&lt;P&gt;ERROR: Task 71 (/home/xxxxx/yocto_base/fsl-release-bsp/sources/meta-fsl-arm/recipes-kernel/linux/linux-imx_3.14.28.bb, do_install) failed with exit code '1'&lt;/P&gt;&lt;P&gt;NOTE: Tasks Summary: Attempted 1428 tasks of which 1382 didn't need to be rerun and 1 failed.&lt;/P&gt;&lt;P&gt;Waiting for 0 running tasks to finish:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Summary: 1 task failed:&lt;/P&gt;&lt;P&gt;&amp;nbsp; /home/xxxxx/yocto_base/fsl-release-bsp/sources/meta-fsl-arm/recipes-kernel/linux/linux-imx_3.14.28.bb, do_install&lt;/P&gt;&lt;P&gt;Summary: There was 1 ERROR message shown, returning a non-zero exit code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What's missing?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 13 Apr 2016 14:04:43 GMT</pubDate>
    <dc:creator>mickaeltoumi</dc:creator>
    <dc:date>2016-04-13T14:04:43Z</dc:date>
    <item>
      <title>bitbake Error with i.MX6UL-EVK dtb</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/bitbake-Error-with-i-MX6UL-EVK-dtb/m-p/501983#M81289</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I ran bitbake last night for the i.MX6UL-EVK platform. The command was: bitbake core-image-base&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The repository has been synched before the build.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am following the steps in the document called: Freescale_Yocto_Project_User's_Guide.pdf&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have the following error:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;| NOTE: make -j 8 imx6ul-14x14-evk.dtb&lt;/P&gt;&lt;P&gt;| make[3]: *** &lt;STRONG&gt;No rule to make target `arch/arm/boot/dts/imx6ul-14x14-evk.dtb'&lt;/STRONG&gt;.&amp;nbsp; Stop.&lt;/P&gt;&lt;P&gt;| make[2]: *** [imx6ul-14x14-evk.dtb] Error 2&lt;/P&gt;&lt;P&gt;| make[1]: *** [sub-make] Error 2&lt;/P&gt;&lt;P&gt;| make: *** [all] Error 2&lt;/P&gt;&lt;P&gt;| ERROR: oe_runmake failed&lt;/P&gt;&lt;P&gt;| WARNING: exit code 1 from a shell command.&lt;/P&gt;&lt;P&gt;| ERROR: Function failed: do_install (log file is located at /home/mtoumi/yocto_base/fsl-release-bsp/build/tmp/work/imx6ulevk-poky-linux-gnueabi/linux-imx/&lt;STRONG&gt;3.14.28-r0&lt;/STRONG&gt;/temp/log.do_install.29429)&lt;/P&gt;&lt;P&gt;ERROR: Task 71 (/home/xxxxx/yocto_base/fsl-release-bsp/sources/meta-fsl-arm/recipes-kernel/linux/linux-imx_3.14.28.bb, do_install) failed with exit code '1'&lt;/P&gt;&lt;P&gt;NOTE: Tasks Summary: Attempted 1428 tasks of which 1382 didn't need to be rerun and 1 failed.&lt;/P&gt;&lt;P&gt;Waiting for 0 running tasks to finish:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Summary: 1 task failed:&lt;/P&gt;&lt;P&gt;&amp;nbsp; /home/xxxxx/yocto_base/fsl-release-bsp/sources/meta-fsl-arm/recipes-kernel/linux/linux-imx_3.14.28.bb, do_install&lt;/P&gt;&lt;P&gt;Summary: There was 1 ERROR message shown, returning a non-zero exit code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What's missing?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Apr 2016 14:04:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/bitbake-Error-with-i-MX6UL-EVK-dtb/m-p/501983#M81289</guid>
      <dc:creator>mickaeltoumi</dc:creator>
      <dc:date>2016-04-13T14:04:43Z</dc:date>
    </item>
    <item>
      <title>Re: bitbake Error with i.MX6UL-EVK dtb</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/bitbake-Error-with-i-MX6UL-EVK-dtb/m-p/501984#M81290</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Mickael T,&lt;/P&gt;&lt;P&gt;The 3.14.28 BSP Release does not support the i.MX6UL EVK. You can see the supported machine options on the Release Notes or section 5.2 of the Yocto User's Guide. I would recommend switching to BSP 3.14.52 release, which does support the i.MX6UL EVK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Apr 2016 20:57:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/bitbake-Error-with-i-MX6UL-EVK-dtb/m-p/501984#M81290</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2016-04-13T20:57:00Z</dc:date>
    </item>
    <item>
      <title>Re: bitbake Error with i.MX6UL-EVK dtb</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/bitbake-Error-with-i-MX6UL-EVK-dtb/m-p/501985#M81291</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok thanks for the answer. I will move to 3.14.52. I believe I missed a key last night, my initial intention was to get 3.14.&lt;STRONG&gt;3&lt;/STRONG&gt;8.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Apr 2016 21:59:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/bitbake-Error-with-i-MX6UL-EVK-dtb/m-p/501985#M81291</guid>
      <dc:creator>mickaeltoumi</dc:creator>
      <dc:date>2016-04-13T21:59:15Z</dc:date>
    </item>
  </channel>
</rss>