<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MIPI CSI-2 frame dump in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-CSI-2-frame-dump/m-p/501794#M81233</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Shajin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am not aware of ways of dumping mipi captured frame, probably&lt;/P&gt;&lt;P&gt;one can write own application using sect.20.3.3 Programming Interface&lt;/P&gt;&lt;P&gt;mipi driver attached Linux Manual. Problem is that mipi has not accessible&lt;/P&gt;&lt;P&gt;data frame buffer, as it uses MIPI CSI to IPU Gasket (CSI2IPU), data is passed&lt;/P&gt;&lt;P&gt;directly to IPU. IPU data is processed with DMA (IDMAC). So for dumping&lt;/P&gt;&lt;P&gt;captured frame both MIPI and IPU should be programmed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 20 Jan 2016 01:44:54 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2016-01-20T01:44:54Z</dc:date>
    <item>
      <title>MIPI CSI-2 frame dump</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-CSI-2-frame-dump/m-p/501793#M81232</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm exploring MIPI CSI-2 interface in SABRE SD Platform which uses Omnivision ov5640 camera. My understanding on MIPI is very minimum. I wonder, Is there any way in kernel space the captured frame can be dumped/print ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your time..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Shajin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Jan 2016 18:15:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIPI-CSI-2-frame-dump/m-p/501793#M81232</guid>
      <dc:creator>shajinas</dc:creator>
      <dc:date>2016-01-19T18:15:54Z</dc:date>
    </item>
    <item>
      <title>Re: MIPI CSI-2 frame dump</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-CSI-2-frame-dump/m-p/501794#M81233</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Shajin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am not aware of ways of dumping mipi captured frame, probably&lt;/P&gt;&lt;P&gt;one can write own application using sect.20.3.3 Programming Interface&lt;/P&gt;&lt;P&gt;mipi driver attached Linux Manual. Problem is that mipi has not accessible&lt;/P&gt;&lt;P&gt;data frame buffer, as it uses MIPI CSI to IPU Gasket (CSI2IPU), data is passed&lt;/P&gt;&lt;P&gt;directly to IPU. IPU data is processed with DMA (IDMAC). So for dumping&lt;/P&gt;&lt;P&gt;captured frame both MIPI and IPU should be programmed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Jan 2016 01:44:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIPI-CSI-2-frame-dump/m-p/501794#M81233</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-01-20T01:44:54Z</dc:date>
    </item>
  </channel>
</rss>