<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Powering iMX.23 through VDDIO pin?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Powering-iMX-23-through-VDDIO-pin/m-p/149685#M810</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mike,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;No, we weren't able to get it work and punted on it since we needed to get the board spun and move on.&amp;nbsp; We pulled all 3.3V peripherals off the processor (including direct drive LEDs) so the only thing the processor is powering now is itself and memory through VDD5V.&amp;nbsp; It doesn't run very hot in this configuration.&lt;/P&gt;&lt;P&gt;Another option we considered was supplying power via VDD4P2V or BATT.&amp;nbsp; We would have had to add the components to enable the DCDC converter and incur more design time and component cost.&amp;nbsp; But you might want to look at that for your imx28x.&amp;nbsp; 3.3V is the minimum for VDD4P2V/BATT, so I would look to increase that a little more for a comfortable margin, but of course that's yet another external regulator.&lt;/P&gt;&lt;P&gt;It's too bad they didn't spec the DCDC converter to operate with 5V to address non-portable applications.&lt;/P&gt;&lt;P&gt;We found the OnSemi NCP1529 to be a nice fixed/adj. high frequency regulator with a low parts count if you want to explore some external regulator options.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 26 Apr 2011 14:10:06 GMT</pubDate>
    <dc:creator>markl</dc:creator>
    <dc:date>2011-04-26T14:10:06Z</dc:date>
    <item>
      <title>Powering iMX.23 through VDDIO pin?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Powering-iMX-23-through-VDDIO-pin/m-p/149682#M807</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;A question on power source...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Our board has a number of 3.3V peripherals on it, and combined they draw more than the i.MX can supply.&amp;nbsp; So, we had to add a separate 3.3V switching regulator.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Our board is externally powered from 5V, and we are currently using the VDD5V input on the i.MX to give it power.&amp;nbsp; However, this results in some power being dissipated constantly through i.MX linear regulators, no matter what mode the i.MX power supply is in.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;And plus another downside of using the VDD5V input is that the i.MX doesn't have a lot of tolerance (5% @ &amp;gt;100mA) for voltage droop on it (table 2-3).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So, since we have a stable 3.3V supply available, is it possible to power the i.MX23 directly through the VDDIO pin?&amp;nbsp; This would allow more tolerance for 5V fluctuations since it would now be a function of the external 3.3V regulator, and it could possibly reduce the heat dissipation in the i.MX a little bit.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There is no battery in our application, so VDD4P2V doesn't matter, and we would just use the linear regulators to supply VDDA and ﻿VDDD and disable the DCDC converter (which we're already not using anyway).&amp;nbsp; Looking at the diagram of the power supply (figure 32-1) in the manual, it appears that power coming in through the VDDIO pin should be possible since the final stage of the linear regulators are all pass MOSFETs.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It's a little unconventional, I admit, but I can't think of any reason why it can't (or shouldn't) be done.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for any thoughts,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 06 Mar 2011 20:33:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Powering-iMX-23-through-VDDIO-pin/m-p/149682#M807</guid>
      <dc:creator>markl</dc:creator>
      <dc:date>2011-03-06T20:33:03Z</dc:date>
    </item>
    <item>
      <title>Re: Powering iMX.23 through VDDIO pin?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Powering-iMX-23-through-VDDIO-pin/m-p/149683#M808</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok, so I tried this and I'll save everyone time replying.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In short, I couldn't get this to work.&amp;nbsp; It doesn't draw any current worth mentioning on VDDIO and obviously doesn't boot.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm guessing that something is looking for voltage coming into VDD4P2V or VDD5V before anything interesting starts happening.&amp;nbsp; Oh well.&amp;nbsp; board_parts_count++ ...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Mar 2011 19:12:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Powering-iMX-23-through-VDDIO-pin/m-p/149683#M808</guid>
      <dc:creator>markl</dc:creator>
      <dc:date>2011-03-08T19:12:56Z</dc:date>
    </item>
    <item>
      <title>Re: Powering iMX.23 through VDDIO pin?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Powering-iMX-23-through-VDDIO-pin/m-p/149684#M809</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mark;&lt;/P&gt;&lt;BLOCKQUOTE cite="http://imxcommunity.org/forum/topics/powering-imx23-through-vddio?groupUrl=imx23&amp;amp;#4103961Comment6808"&gt;&lt;DIV&gt;&lt;P&gt;did you get to any results on this power supply case.&lt;/P&gt;&lt;P&gt;I am trying to come up with similar solutions to reduce the IC's power consumption; specially in Imx28x which seems to have a much bigger power consumption than imx233!&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/DIV&gt;&lt;/BLOCKQUOTE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Apr 2011 04:18:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Powering-iMX-23-through-VDDIO-pin/m-p/149684#M809</guid>
      <dc:creator>mikeasa</dc:creator>
      <dc:date>2011-04-26T04:18:01Z</dc:date>
    </item>
    <item>
      <title>Re: Powering iMX.23 through VDDIO pin?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Powering-iMX-23-through-VDDIO-pin/m-p/149685#M810</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mike,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;No, we weren't able to get it work and punted on it since we needed to get the board spun and move on.&amp;nbsp; We pulled all 3.3V peripherals off the processor (including direct drive LEDs) so the only thing the processor is powering now is itself and memory through VDD5V.&amp;nbsp; It doesn't run very hot in this configuration.&lt;/P&gt;&lt;P&gt;Another option we considered was supplying power via VDD4P2V or BATT.&amp;nbsp; We would have had to add the components to enable the DCDC converter and incur more design time and component cost.&amp;nbsp; But you might want to look at that for your imx28x.&amp;nbsp; 3.3V is the minimum for VDD4P2V/BATT, so I would look to increase that a little more for a comfortable margin, but of course that's yet another external regulator.&lt;/P&gt;&lt;P&gt;It's too bad they didn't spec the DCDC converter to operate with 5V to address non-portable applications.&lt;/P&gt;&lt;P&gt;We found the OnSemi NCP1529 to be a nice fixed/adj. high frequency regulator with a low parts count if you want to explore some external regulator options.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Apr 2011 14:10:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Powering-iMX-23-through-VDDIO-pin/m-p/149685#M810</guid>
      <dc:creator>markl</dc:creator>
      <dc:date>2011-04-26T14:10:06Z</dc:date>
    </item>
    <item>
      <title>Re: Powering iMX.23 through VDDIO pin?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Powering-iMX-23-through-VDDIO-pin/m-p/149686#M811</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;thanks mark.&lt;/P&gt;&lt;P&gt;for imx28; the power calculator from freescale; shows the power usage is about twice the imx233.(part of it is due to DDR2 chip).&lt;/P&gt;&lt;P&gt;with that; the chip's power supply efficiency is about 75%!!!(and they call this efficient too!).&lt;/P&gt;&lt;P&gt;It has the convenience to regulators on the cpu; but at highly low efficiency.&lt;/P&gt;&lt;P&gt;So now I am thinking of how to disable all the cpu's regulators and use all, from outside which increases board space and cost. but 75% eff. is just out of question and I must use DDR2 memory!&lt;/P&gt;&lt;P&gt;thanks again.&lt;/P&gt;&lt;P&gt;.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Apr 2011 19:22:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Powering-iMX-23-through-VDDIO-pin/m-p/149686#M811</guid>
      <dc:creator>mikeasa</dc:creator>
      <dc:date>2011-04-26T19:22:43Z</dc:date>
    </item>
    <item>
      <title>Re: Powering iMX.23 through VDDIO pin?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Powering-iMX-23-through-VDDIO-pin/m-p/149687#M812</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;CITE&gt;Mark Litwack said:&lt;/CITE&gt;&lt;BLOCKQUOTE cite="http://imxcommunity.org/forum/topics/powering-imx23-through-vddio?groupUrl=imx23#4103961Comment6808"&gt;&lt;DIV&gt;&lt;P&gt;Ok, so I tried this and I'll save everyone time replying.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In short, I couldn't get this to work.&amp;nbsp; It doesn't draw any current worth mentioning on VDDIO and obviously doesn't boot.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm guessing that something is looking for voltage coming into VDD4P2V or VDD5V before anything interesting starts happening.&amp;nbsp; Oh well.&amp;nbsp; board_parts_count++ ...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Mark, I've been designing a feature phone using i.MX233 and one thing I want to say is, it's one of the lowest power ARM SoCs out there! But you have to keep the following in mind to appreciate its low power capabilities&lt;/P&gt;&lt;P&gt;1. The linear regulators regulators should never be used if your board draws significant current, say &amp;gt; 1/2 the rating. as they have poor efficiency, thus will heat up the die. I use the linear regulators only when I'm charging the battery through USB-5V.&lt;/P&gt;&lt;P&gt;2. If your current demand is more than the DC-DC can supply, then using additional external DC-DC converter is the best option. let the integrated DC-DC power up the SoC and some light loads on board and the rest separately supplied from external DC-DC. I have GSM/GPRS, GPS,SDIO wifi and bluetooth chips on my tiny PCB and all are powered from an external DC-DC which can supply up to 3A @3V3, from a 3.6V, 1200mAh Li-ion battery which usually lasts up to 5days once fully charged!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I know this is so a late reply, but i posted anyway 'case it might help&lt;/P&gt;&lt;P&gt;--cheers!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; ---Dan&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/DIV&gt;&lt;/BLOCKQUOTE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 May 2011 14:41:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Powering-iMX-23-through-VDDIO-pin/m-p/149687#M812</guid>
      <dc:creator>danix</dc:creator>
      <dc:date>2011-05-05T14:41:14Z</dc:date>
    </item>
  </channel>
</rss>