<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: NAND Flash with i.MX6Q in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/NAND-Flash-with-i-MX6Q/m-p/500684#M80967</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Q. What are the recomended width and voltage of the NAND Flash.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A. i.MX6Q can support both 3.3V and 1.8V NAND Flash parts, so, there is no difference here. Typically, 8-bit wide NAND Flash parts are used, since 16-bit wide ones are not widespread on the market, and they are not supported by i.MX6Q.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Q. Is there an upper limit for the size of the flash regarding the comemrcially available chips.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A. There is no memory size limitation from the i.MX6Q GPMI NAND Flash controller point of view.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 20 Jan 2016 11:45:26 GMT</pubDate>
    <dc:creator>art</dc:creator>
    <dc:date>2016-01-20T11:45:26Z</dc:date>
    <item>
      <title>NAND Flash with i.MX6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/NAND-Flash-with-i-MX6Q/m-p/500683#M80966</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Greetings,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On a custom hardware we are planning to add a NAND Flash on the PCB. When choosing the NAND Flash to work with i.MX6, what are&lt;/P&gt;&lt;P&gt;the recomended width and voltage of the NAND Flash. I am looking at Micron products. Is there an upper limit for the size of the flash regarding the&lt;/P&gt;&lt;P&gt;comemrcially available chips.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mete&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Jan 2016 13:30:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/NAND-Flash-with-i-MX6Q/m-p/500683#M80966</guid>
      <dc:creator>atillametetured</dc:creator>
      <dc:date>2016-01-19T13:30:56Z</dc:date>
    </item>
    <item>
      <title>Re: NAND Flash with i.MX6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/NAND-Flash-with-i-MX6Q/m-p/500684#M80967</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Q. What are the recomended width and voltage of the NAND Flash.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A. i.MX6Q can support both 3.3V and 1.8V NAND Flash parts, so, there is no difference here. Typically, 8-bit wide NAND Flash parts are used, since 16-bit wide ones are not widespread on the market, and they are not supported by i.MX6Q.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Q. Is there an upper limit for the size of the flash regarding the comemrcially available chips.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A. There is no memory size limitation from the i.MX6Q GPMI NAND Flash controller point of view.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Jan 2016 11:45:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/NAND-Flash-with-i-MX6Q/m-p/500684#M80967</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2016-01-20T11:45:26Z</dc:date>
    </item>
    <item>
      <title>Re: NAND Flash with i.MX6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/NAND-Flash-with-i-MX6Q/m-p/500685#M80968</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Artur,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much for the detailed information.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind Regards,&lt;/P&gt;&lt;P&gt;Mete&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Jan 2016 14:25:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/NAND-Flash-with-i-MX6Q/m-p/500685#M80968</guid>
      <dc:creator>atillametetured</dc:creator>
      <dc:date>2016-01-20T14:25:34Z</dc:date>
    </item>
  </channel>
</rss>