<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.mx6q 32KHz Internal Oscillator &amp; HDMI CEC in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6q-32KHz-Internal-Oscillator-HDMI-CEC/m-p/500256#M80857</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are working on a custom board solution and are investigating non-working CEC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The root cause appears to be incorrect timing of bit transmission - confirmed by both an HDMI analyzer and scope - basically bits are transitioning "too fast" and very similar to issue reported &lt;A _jive_internal="true" href="https://community.nxp.com/message/362859#comment-362859"&gt;here&lt;/A&gt;.&amp;nbsp; Start and bit transitions are approximately 60% of nominal (e.g., +/-2.4ms actual versus +/-3.6ms nominal)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Our board does not populate the external 32KHz source and is therefore using the internal oscillator.&lt;/P&gt;&lt;P&gt;Enabling RTC and examining counter values we can see that the internal oscillator is "running fast" with the same variance as CEC bit timings.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have some parts on order to see if external 32KHz oscillator cleans things up but was wondering:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Has anyone else observed CEC issues with internal oscillator?&lt;/LI&gt;&lt;LI&gt;Is there any mechanism (I can find no reference) to trim the internal oscillator for a quick test?&lt;/LI&gt;&lt;LI&gt;Could anything else be causing this timing issue?&lt;UL&gt;&lt;LI&gt;The HDMI core is driving the line and no external controls.&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance - will post our findings back to this thread.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kevin Cormier&lt;BR /&gt;Fidus Systems&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 23 Mar 2016 15:03:11 GMT</pubDate>
    <dc:creator>kevincormier</dc:creator>
    <dc:date>2016-03-23T15:03:11Z</dc:date>
    <item>
      <title>i.mx6q 32KHz Internal Oscillator &amp; HDMI CEC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6q-32KHz-Internal-Oscillator-HDMI-CEC/m-p/500256#M80857</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are working on a custom board solution and are investigating non-working CEC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The root cause appears to be incorrect timing of bit transmission - confirmed by both an HDMI analyzer and scope - basically bits are transitioning "too fast" and very similar to issue reported &lt;A _jive_internal="true" href="https://community.nxp.com/message/362859#comment-362859"&gt;here&lt;/A&gt;.&amp;nbsp; Start and bit transitions are approximately 60% of nominal (e.g., +/-2.4ms actual versus +/-3.6ms nominal)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Our board does not populate the external 32KHz source and is therefore using the internal oscillator.&lt;/P&gt;&lt;P&gt;Enabling RTC and examining counter values we can see that the internal oscillator is "running fast" with the same variance as CEC bit timings.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have some parts on order to see if external 32KHz oscillator cleans things up but was wondering:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Has anyone else observed CEC issues with internal oscillator?&lt;/LI&gt;&lt;LI&gt;Is there any mechanism (I can find no reference) to trim the internal oscillator for a quick test?&lt;/LI&gt;&lt;LI&gt;Could anything else be causing this timing issue?&lt;UL&gt;&lt;LI&gt;The HDMI core is driving the line and no external controls.&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance - will post our findings back to this thread.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kevin Cormier&lt;BR /&gt;Fidus Systems&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Mar 2016 15:03:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx6q-32KHz-Internal-Oscillator-HDMI-CEC/m-p/500256#M80857</guid>
      <dc:creator>kevincormier</dc:creator>
      <dc:date>2016-03-23T15:03:11Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx6q 32KHz Internal Oscillator &amp; HDMI CEC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6q-32KHz-Internal-Oscillator-HDMI-CEC/m-p/500257#M80858</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Addition of an external 32KHz oscillator corrected the bit timings and enabled CEC operation. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Mar 2016 19:05:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx6q-32KHz-Internal-Oscillator-HDMI-CEC/m-p/500257#M80858</guid>
      <dc:creator>kevincormier</dc:creator>
      <dc:date>2016-03-23T19:05:05Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx6q 32KHz Internal Oscillator &amp; HDMI CEC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6q-32KHz-Internal-Oscillator-HDMI-CEC/m-p/500258#M80859</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kevin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;internal oscillator inaccuracy is caused by erratum :&lt;/P&gt;&lt;P&gt;ERR007926 ROM: 32 kHz internal oscillator timing inaccuracy&lt;/P&gt;&lt;P&gt;i.MX6DQ Errata &lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.freescale.com/external-link.jspa?url=http%3A%2F%2Fcache.freescale.com%2Ffiles%2F32bit%2Fdoc%2Ferrata%2FIMX6DQCE.pdf" rel="nofollow" target="_blank"&gt;http://cache.freescale.com/files/32bit/doc/errata/IMX6DQCE.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Unfortunately there is no way to trim the internal oscillator.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Mar 2016 00:41:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx6q-32KHz-Internal-Oscillator-HDMI-CEC/m-p/500258#M80859</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-03-24T00:41:11Z</dc:date>
    </item>
  </channel>
</rss>