<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic lvds is white when waked up in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/lvds-is-white-when-waked-up/m-p/499758#M80705</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using imx6dl board ,android 4.4.2, and sometimes when I wake up the lvds , the screen is white&lt;/P&gt;&lt;P&gt;I tried to delay the led_enable to 250ms, but it did not work ,what should I do ? thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 23 Mar 2016 07:07:02 GMT</pubDate>
    <dc:creator>zhao_feng</dc:creator>
    <dc:date>2016-03-23T07:07:02Z</dc:date>
    <item>
      <title>lvds is white when waked up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/lvds-is-white-when-waked-up/m-p/499758#M80705</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using imx6dl board ,android 4.4.2, and sometimes when I wake up the lvds , the screen is white&lt;/P&gt;&lt;P&gt;I tried to delay the led_enable to 250ms, but it did not work ,what should I do ? thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Mar 2016 07:07:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/lvds-is-white-when-waked-up/m-p/499758#M80705</guid>
      <dc:creator>zhao_feng</dc:creator>
      <dc:date>2016-03-23T07:07:02Z</dc:date>
    </item>
    <item>
      <title>Re: lvds is white when waked up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/lvds-is-white-when-waked-up/m-p/499759#M80706</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi feng,&lt;/P&gt;&lt;P&gt;Is the board you designed it yourself? And you porting the LVDS screen to your board? If yes, here the lvds do not work maybe caused by the improper parameter setting， you should according to the screen datasheet&lt;SPAN class="contentTitle"&gt;&lt;/SPAN&gt;. Here you can refer to the thread in our community &lt;A href="https://community.nxp.com/docs/DOC-172312"&gt;Porting LVDS LCD With Low Resolution to i.MX6&lt;/A&gt; . The step is almost the same. Hope it can help you.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Dan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Mark Correct&amp;nbsp; button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Mar 2016 08:28:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/lvds-is-white-when-waked-up/m-p/499759#M80706</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2016-03-23T08:28:40Z</dc:date>
    </item>
  </channel>
</rss>