<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: MIPI DSI mipi clock</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-DSI-mipi-clock/m-p/499714#M80704</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;MIPI DSI interface of i.MX6S processor supports from 80 Mbps up to 1 Gbps speed per data lane.&lt;/P&gt;&lt;P&gt;DSI receiver cores can mange one clock lane and up to 4 data lanes through the lane management,&lt;/P&gt;&lt;P&gt;however two data lanes are implemented in the transmitter D-PHY, therefore the maximum throughput of display port is 2Gbps.&lt;/P&gt;&lt;P&gt;Please refer to 9.10.2 and 9.10.3 chapters of i.MX 6Solo/6DualLite Applications Processor Reference Manual for more details.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 18 Apr 2016 06:24:59 GMT</pubDate>
    <dc:creator>b36401</dc:creator>
    <dc:date>2016-04-18T06:24:59Z</dc:date>
    <item>
      <title>MIPI DSI mipi clock</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-DSI-mipi-clock/m-p/499713#M80703</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I'm using&amp;nbsp; a Agilent DSO9084A Oscilloscope to analyze a two lane MIPI DSI bus.&lt;/P&gt;&lt;P&gt;The MIPI analyzation software don't use the external MIPI clk&amp;nbsp; from the imx6 cpu, but instead needs the data rate specified.&lt;/P&gt;&lt;P&gt;I need to know the exact mipi clk used when configuring my display.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For example, when i configure my display to use a max_phy_clk=300, in mipi_lcd_config,&amp;nbsp; what is the exact mipi clk generated from this.&lt;/P&gt;&lt;P&gt;I'm using kernel driver from branch imx_3.14.38_6qp_ga&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Felix&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Mar 2016 16:16:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIPI-DSI-mipi-clock/m-p/499713#M80703</guid>
      <dc:creator>felixh</dc:creator>
      <dc:date>2016-03-23T16:16:47Z</dc:date>
    </item>
    <item>
      <title>Re: MIPI DSI mipi clock</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-DSI-mipi-clock/m-p/499714#M80704</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;MIPI DSI interface of i.MX6S processor supports from 80 Mbps up to 1 Gbps speed per data lane.&lt;/P&gt;&lt;P&gt;DSI receiver cores can mange one clock lane and up to 4 data lanes through the lane management,&lt;/P&gt;&lt;P&gt;however two data lanes are implemented in the transmitter D-PHY, therefore the maximum throughput of display port is 2Gbps.&lt;/P&gt;&lt;P&gt;Please refer to 9.10.2 and 9.10.3 chapters of i.MX 6Solo/6DualLite Applications Processor Reference Manual for more details.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Apr 2016 06:24:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIPI-DSI-mipi-clock/m-p/499714#M80704</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2016-04-18T06:24:59Z</dc:date>
    </item>
  </channel>
</rss>