<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Trouble using USB OTG on SABRE for MFG Tool in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Trouble-using-USB-OTG-on-SABRE-for-MFG-Tool/m-p/182865#M8065</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to copy my uBoot and Android distribution into the eMMC of a imx53 SABRE tablet, with the MFG Tool.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- I've changed my SW26 (0x00) and SW28 (0x30) dip switches to the according value for USB Serial Download Mode for the MFG Tool.&lt;/P&gt;&lt;P&gt;- I've connected with the OTG port (J34) micro-USB connector on the tablet side, following the Freescale BSP user guide.&lt;/P&gt;&lt;P&gt;- On the PC side, I have a Windows XP SP2.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The issue is that the tablet is not correctly recognized by the PC. A peripheral is enumerated, but no VID and PID declared. So I'm unable to match it with the iMX_BulkIO_Driver.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- I'm not sure about the use of the USB OTG port use. Is this the right one ?&lt;/P&gt;&lt;P&gt;- Did I miss a step ?&lt;/P&gt;&lt;P&gt;- Which other way do I have to update a bootloader, kernel, ramdisk and partitions on the eMMC ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your feedback and help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Colin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 22 Aug 2012 13:27:33 GMT</pubDate>
    <dc:creator>ColinChaballier</dc:creator>
    <dc:date>2012-08-22T13:27:33Z</dc:date>
    <item>
      <title>Trouble using USB OTG on SABRE for MFG Tool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Trouble-using-USB-OTG-on-SABRE-for-MFG-Tool/m-p/182865#M8065</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to copy my uBoot and Android distribution into the eMMC of a imx53 SABRE tablet, with the MFG Tool.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- I've changed my SW26 (0x00) and SW28 (0x30) dip switches to the according value for USB Serial Download Mode for the MFG Tool.&lt;/P&gt;&lt;P&gt;- I've connected with the OTG port (J34) micro-USB connector on the tablet side, following the Freescale BSP user guide.&lt;/P&gt;&lt;P&gt;- On the PC side, I have a Windows XP SP2.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The issue is that the tablet is not correctly recognized by the PC. A peripheral is enumerated, but no VID and PID declared. So I'm unable to match it with the iMX_BulkIO_Driver.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- I'm not sure about the use of the USB OTG port use. Is this the right one ?&lt;/P&gt;&lt;P&gt;- Did I miss a step ?&lt;/P&gt;&lt;P&gt;- Which other way do I have to update a bootloader, kernel, ramdisk and partitions on the eMMC ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your feedback and help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Colin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Aug 2012 13:27:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Trouble-using-USB-OTG-on-SABRE-for-MFG-Tool/m-p/182865#M8065</guid>
      <dc:creator>ColinChaballier</dc:creator>
      <dc:date>2012-08-22T13:27:33Z</dc:date>
    </item>
    <item>
      <title>Re: Trouble using USB OTG on SABRE for MFG Tool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Trouble-using-USB-OTG-on-SABRE-for-MFG-Tool/m-p/182866#M8066</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've double check all the points, measured voltage at DIP switches in/out, changed my micro-B USB cable.... And nothing new. In fact there is no USB enumeration.&amp;nbsp;&lt;/P&gt;&lt;P&gt;My guess is that the USB OTG controller looks like deactivated. Is this possible ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Colin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Aug 2012 14:56:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Trouble-using-USB-OTG-on-SABRE-for-MFG-Tool/m-p/182866#M8066</guid>
      <dc:creator>ColinChaballier</dc:creator>
      <dc:date>2012-08-27T14:56:40Z</dc:date>
    </item>
  </channel>
</rss>