<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Pulseaudio + Yocto + Systemd</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Pulseaudio-Yocto-Systemd/m-p/498979#M80474</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Caio&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;dbus systemd is not supported in nxp/fsl linux bsps, as for pulseaudio&lt;/P&gt;&lt;P&gt;configuration with linux one can look at attached linux guide&lt;/P&gt;&lt;P&gt;sect.7.4 Pulseaudio input/output settings.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 31 Dec 2015 01:23:59 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2015-12-31T01:23:59Z</dc:date>
    <item>
      <title>Pulseaudio + Yocto + Systemd</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Pulseaudio-Yocto-Systemd/m-p/498977#M80472</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm trying to add the pulseadio into my Image&lt;/P&gt;&lt;P&gt;So I added these lines in my local.conf&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;DISTRO_FEATURES_append = " pulseaudio opengl wifi ethernet loopback udev dbus systemd"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;IMAGE_INSTALL_append = " qtbase qtbase-fonts qtbase-plugins qtmultimedia qtmultimedia-plugins qtmultimedia-qmlplugins qtbase-examples cinematicexperience tslib tslib-calibrate tslib-conf tslib-tests sisc imx-vpu&amp;nbsp; gpu-viv-bin-mx6q sqlite3&amp;nbsp; packagegroup-fslc-gstreamer1.0 dbus pulseaudio pulseaudio-server pulseaudio-misc pulseaudio-module-dbus-protocol alsa-utils i2c-tools"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PACKAGECONFIG_append_pn-pulseaudio = " systemd"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But when the Linux boot the pulseaudio doesn't start, there's no pulseadio.service.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I try to run the pulseaudio with --system or -nC ,I get some error in the console. Which is the best way to starts pulseaudio with dbus and systemd?&lt;/P&gt;&lt;P&gt;Someone could help me?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yocto 1.7.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Caio Pereira&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Dec 2015 19:08:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Pulseaudio-Yocto-Systemd/m-p/498977#M80472</guid>
      <dc:creator>caiopereira</dc:creator>
      <dc:date>2015-12-21T19:08:10Z</dc:date>
    </item>
    <item>
      <title>Re: Pulseaudio + Yocto + Systemd</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Pulseaudio-Yocto-Systemd/m-p/498978#M80473</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;After add the root into pulse group I could use the pulseaudio&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;gpasswd -a root audio&lt;/P&gt;&lt;P&gt;pulseaudio --system&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I test the pulse audio using the gstreamer.&lt;/P&gt;&lt;P&gt;gst-launch-0.10 filesrc location=/usr/share/sounds/alsa/Front_Right.wav ! wavparse ! pulsesink&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But the audio it's crackling, it's horrible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tryed with pulseaudio --system --realtime, but I couldn't resolve the latency problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Someone could give an advice to configure the pulseaudio?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Dec 2015 18:32:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Pulseaudio-Yocto-Systemd/m-p/498978#M80473</guid>
      <dc:creator>caiopereira</dc:creator>
      <dc:date>2015-12-22T18:32:21Z</dc:date>
    </item>
    <item>
      <title>Re: Pulseaudio + Yocto + Systemd</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Pulseaudio-Yocto-Systemd/m-p/498979#M80474</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Caio&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;dbus systemd is not supported in nxp/fsl linux bsps, as for pulseaudio&lt;/P&gt;&lt;P&gt;configuration with linux one can look at attached linux guide&lt;/P&gt;&lt;P&gt;sect.7.4 Pulseaudio input/output settings.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Dec 2015 01:23:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Pulseaudio-Yocto-Systemd/m-p/498979#M80474</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-12-31T01:23:59Z</dc:date>
    </item>
  </channel>
</rss>