<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Is the ipu-lib able to work on iMX6Q? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Is-the-ipu-lib-able-to-work-on-iMX6Q/m-p/182790#M8047</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using the iMX6Q now. I want to add 3 screen layer in one display. I think the iMX6Q default code implement 2 screen layer fb0,fb1(overlay) in one display. How can I add the third screen layer?&lt;/P&gt;&lt;P&gt;I found iMX53 has ipu-lib and screenlayer library to meet this requirement. But in iMX6Q default code, the&amp;nbsp;ipu-lib is useless.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 21 Aug 2012 07:48:17 GMT</pubDate>
    <dc:creator>SamTan</dc:creator>
    <dc:date>2012-08-21T07:48:17Z</dc:date>
    <item>
      <title>Is the ipu-lib able to work on iMX6Q?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-the-ipu-lib-able-to-work-on-iMX6Q/m-p/182790#M8047</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using the iMX6Q now. I want to add 3 screen layer in one display. I think the iMX6Q default code implement 2 screen layer fb0,fb1(overlay) in one display. How can I add the third screen layer?&lt;/P&gt;&lt;P&gt;I found iMX53 has ipu-lib and screenlayer library to meet this requirement. But in iMX6Q default code, the&amp;nbsp;ipu-lib is useless.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Aug 2012 07:48:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-the-ipu-lib-able-to-work-on-iMX6Q/m-p/182790#M8047</guid>
      <dc:creator>SamTan</dc:creator>
      <dc:date>2012-08-21T07:48:17Z</dc:date>
    </item>
    <item>
      <title>Re: Is the ipu-lib able to work on iMX6Q?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-the-ipu-lib-able-to-work-on-iMX6Q/m-p/182791#M8048</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;ipu-lib is not runnable on imx6, but you can directly use ioctl to get similar functions.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Sep 2012 03:16:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-the-ipu-lib-able-to-work-on-iMX6Q/m-p/182791#M8048</guid>
      <dc:creator>fengwei</dc:creator>
      <dc:date>2012-09-18T03:16:55Z</dc:date>
    </item>
    <item>
      <title>Re: Is the ipu-lib able to work on iMX6Q?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-the-ipu-lib-able-to-work-on-iMX6Q/m-p/182792#M8049</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ipu-lib is not used on i.mx6. Using GPU to do the third screen layer combination is better than IPU. The above mentioned ioctls are defined in include/linux/ipu.h. The unit test name is mxc_ipudev_test.out and also has a script named autorun-ipu.sh under the target rootfs.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Nov 2012 03:21:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-the-ipu-lib-able-to-work-on-iMX6Q/m-p/182792#M8049</guid>
      <dc:creator>wayne1z</dc:creator>
      <dc:date>2012-11-13T03:21:21Z</dc:date>
    </item>
  </channel>
</rss>