<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic IMX6Q Sabrelite board Linux 3.10.17_1.0.0_ga PCIe issue in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-Sabrelite-board-Linux-3-10-17-1-0-0-ga-PCIe-issue/m-p/498279#M80351</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Linux 3.10.17_1.0.0_ga bootup on IMX6sabrelite board with PCIe adaptor from boundary device. I connect Broadcom WiFi Bluetooth PCIe chipset. I boot the device, PCIe device is detected once, but then PCIe device are never listed again with lspci command. I tried with other PCie device and other IMX6Q board, reset multiple times, lspci never list my device. &lt;/P&gt;&lt;P&gt;Its the first time I work with PCIe, not much knowledge about it. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do any one face this type of issue. Pls suggest any solution&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 23 Mar 2016 06:02:36 GMT</pubDate>
    <dc:creator>paullalthuamsan</dc:creator>
    <dc:date>2016-03-23T06:02:36Z</dc:date>
    <item>
      <title>IMX6Q Sabrelite board Linux 3.10.17_1.0.0_ga PCIe issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-Sabrelite-board-Linux-3-10-17-1-0-0-ga-PCIe-issue/m-p/498279#M80351</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Linux 3.10.17_1.0.0_ga bootup on IMX6sabrelite board with PCIe adaptor from boundary device. I connect Broadcom WiFi Bluetooth PCIe chipset. I boot the device, PCIe device is detected once, but then PCIe device are never listed again with lspci command. I tried with other PCie device and other IMX6Q board, reset multiple times, lspci never list my device. &lt;/P&gt;&lt;P&gt;Its the first time I work with PCIe, not much knowledge about it. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do any one face this type of issue. Pls suggest any solution&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Mar 2016 06:02:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-Sabrelite-board-Linux-3-10-17-1-0-0-ga-PCIe-issue/m-p/498279#M80351</guid>
      <dc:creator>paullalthuamsan</dc:creator>
      <dc:date>2016-03-23T06:02:36Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6Q Sabrelite board Linux 3.10.17_1.0.0_ga PCIe issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-Sabrelite-board-Linux-3-10-17-1-0-0-ga-PCIe-issue/m-p/498280#M80352</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Paul&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can try attached patch and check below link&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/384792"&gt;PCIe link doesn't come up with XIO2001 PCI bridge on iMX6Q custom board &lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Mar 2016 08:53:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-Sabrelite-board-Linux-3-10-17-1-0-0-ga-PCIe-issue/m-p/498280#M80352</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-03-23T08:53:14Z</dc:date>
    </item>
  </channel>
</rss>