<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Uboot too fast and USB host read timeouts in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Uboot-too-fast-and-USB-host-read-timeouts/m-p/498250#M80349</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We made a small production serie of 10 PCBA's with a i.MX6D based on a custom design.&lt;/P&gt;&lt;P&gt;This board has a dedicated USB host (i.MX6 host port) and USB device (i.MX6 OTG port) connection.&lt;/P&gt;&lt;P&gt;9 boards are working fine, but on one board we see 3 problems:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;uBoot seems to run faster than on the other boards, about 3 times faster.&lt;/LI&gt;&lt;LI&gt;After a cold start the USB stick at the USB host port of the i.MX6 is not always recognised.&lt;/LI&gt;&lt;LI&gt;When the USB stick do get recognised, we get read timeouts when we try to access the data.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Problems 1 and 2 seems to be dependant on the board temperature. When the temperature rises, uBoot seems to slow down a bit, but still faster than on the other boards. The USB stick now gets recognised all the time. But still read timeouts.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Things I have checked:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;24MHz crystal is stable and at the right frequency, at cold startup and after couple hours.&lt;/LI&gt;&lt;LI&gt;Power supplies are all in the right range and ripple is less than 5%.&lt;/LI&gt;&lt;LI&gt;I saw that the LDO_2P5 had a saw tooth voltage ripple which was near 5%. Followed the EB814 document on minimum ESR requirements, placed a 100mOhm resistor is series with the bulk capacitor of de LDO_2P5 regulator. The saw tooth voltage ripple disappeared. But no change in the behaviour of the board.&lt;/LI&gt;&lt;LI&gt;No USB problems detected on the i.MX6 OTG port in device mode&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am out of ideas now, so if any of you have suggestions, please let me know.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 01 Mar 2016 09:27:32 GMT</pubDate>
    <dc:creator>thomaslantinga</dc:creator>
    <dc:date>2016-03-01T09:27:32Z</dc:date>
    <item>
      <title>Uboot too fast and USB host read timeouts</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Uboot-too-fast-and-USB-host-read-timeouts/m-p/498250#M80349</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We made a small production serie of 10 PCBA's with a i.MX6D based on a custom design.&lt;/P&gt;&lt;P&gt;This board has a dedicated USB host (i.MX6 host port) and USB device (i.MX6 OTG port) connection.&lt;/P&gt;&lt;P&gt;9 boards are working fine, but on one board we see 3 problems:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;uBoot seems to run faster than on the other boards, about 3 times faster.&lt;/LI&gt;&lt;LI&gt;After a cold start the USB stick at the USB host port of the i.MX6 is not always recognised.&lt;/LI&gt;&lt;LI&gt;When the USB stick do get recognised, we get read timeouts when we try to access the data.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Problems 1 and 2 seems to be dependant on the board temperature. When the temperature rises, uBoot seems to slow down a bit, but still faster than on the other boards. The USB stick now gets recognised all the time. But still read timeouts.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Things I have checked:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;24MHz crystal is stable and at the right frequency, at cold startup and after couple hours.&lt;/LI&gt;&lt;LI&gt;Power supplies are all in the right range and ripple is less than 5%.&lt;/LI&gt;&lt;LI&gt;I saw that the LDO_2P5 had a saw tooth voltage ripple which was near 5%. Followed the EB814 document on minimum ESR requirements, placed a 100mOhm resistor is series with the bulk capacitor of de LDO_2P5 regulator. The saw tooth voltage ripple disappeared. But no change in the behaviour of the board.&lt;/LI&gt;&lt;LI&gt;No USB problems detected on the i.MX6 OTG port in device mode&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am out of ideas now, so if any of you have suggestions, please let me know.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Mar 2016 09:27:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Uboot-too-fast-and-USB-host-read-timeouts/m-p/498250#M80349</guid>
      <dc:creator>thomaslantinga</dc:creator>
      <dc:date>2016-03-01T09:27:32Z</dc:date>
    </item>
    <item>
      <title>Re: Uboot too fast and USB host read timeouts</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Uboot-too-fast-and-USB-host-read-timeouts/m-p/498251#M80350</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Thomas&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can attach jtag debugger or using uboot commands and output&lt;/P&gt;&lt;P&gt;arm clock on CCM_CLKO1,2. Program CCM_CCOSR register &lt;/P&gt;&lt;P&gt;and measure frequency arm_clk_root, osc_clk. In general chip&lt;/P&gt;&lt;P&gt;can be damaged due to ESD or overheating.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Mar 2016 01:40:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Uboot-too-fast-and-USB-host-read-timeouts/m-p/498251#M80350</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-03-02T01:40:54Z</dc:date>
    </item>
  </channel>
</rss>