<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: IMX6 AUDMUX</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-AUDMUX/m-p/498111#M80294</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi hong&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;description of AUDMUX can be found in sect.16.5.1.1.2 Internal Network Mode&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf" title="http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf"&gt;http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;also may be useful to look at attached document Chapter 5&lt;/P&gt;&lt;P&gt;Configuring the AUDMUX Driver and&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/doc/app_note/AN2628.pdf" title="http://cache.freescale.com/files/32bit/doc/app_note/AN2628.pdf"&gt;http://cache.freescale.com/files/32bit/doc/app_note/AN2628.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 30 Dec 2015 10:44:00 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2015-12-30T10:44:00Z</dc:date>
    <item>
      <title>IMX6 AUDMUX</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-AUDMUX/m-p/498110#M80293</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;TABLE cellpadding="0" cellspacing="0" style="color: #444444; font-family: Tahoma, 'Microsoft Yahei', Simsun; font-size: 12px;"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD class="t_f" style="font-size: 14px;"&gt;我们在用IMX6S调试声卡，SSI1用的是AUDMUX的internal port2，AUDMUX的external port3上挂了一路声卡。SSI是slave模式，外部声卡是master模式。&lt;BR /&gt;现在的需求是SSI在放音的时候，同时驱动AUDMUX的external port3和port4，port3用来放音，port4用来采集放音数据作参考。&lt;BR /&gt;1。根据现在的需求，SSI1的AUDMUX的internal port2运行在internal network模式，因为时钟信号是从port3来的，那么port2和port4的PTCR寄存器的时钟信号来源选择port3吗？还是port2运行在internal network模式，port3和port4的时钟信号来源就要选择port2呢？&lt;BR /&gt;2。SSI在录音的时候，只想从port3输入，port4对录音会有影响吗？PDCR的INMMASK把port4屏蔽掉，只留port3，跟SSI port2与port3点对点的效果一样吗？&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Dec 2015 07:57:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-AUDMUX/m-p/498110#M80293</guid>
      <dc:creator>zhouenlai2002-1</dc:creator>
      <dc:date>2015-12-21T07:57:13Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 AUDMUX</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-AUDMUX/m-p/498111#M80294</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi hong&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;description of AUDMUX can be found in sect.16.5.1.1.2 Internal Network Mode&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf" title="http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf"&gt;http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;also may be useful to look at attached document Chapter 5&lt;/P&gt;&lt;P&gt;Configuring the AUDMUX Driver and&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/doc/app_note/AN2628.pdf" title="http://cache.freescale.com/files/32bit/doc/app_note/AN2628.pdf"&gt;http://cache.freescale.com/files/32bit/doc/app_note/AN2628.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Dec 2015 10:44:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-AUDMUX/m-p/498111#M80294</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-12-30T10:44:00Z</dc:date>
    </item>
  </channel>
</rss>