<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Andriod 5.1.1.2 kernel hangs in IMX 6 SL EVK  platform in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Andriod-5-1-1-2-kernel-hangs-in-IMX-6-SL-EVK-platform/m-p/497902#M80255</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Lyf,&lt;/P&gt;&lt;P&gt;Sorry for late reply. When the android system boot up, and then go to sleep mode, when you insert other device such as USB flash disk， mouse or keyboard by USB OTG&amp;nbsp; the system will awake. So here you can go to the setting options on your android system, to set the display time. It will be OK.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Dan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Mark Correct&amp;nbsp; button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 29 Apr 2016 08:38:27 GMT</pubDate>
    <dc:creator>Rita_Wang</dc:creator>
    <dc:date>2016-04-29T08:38:27Z</dc:date>
    <item>
      <title>Andriod 5.1.1.2 kernel hangs in IMX 6 SL EVK  platform</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Andriod-5-1-1-2-kernel-hangs-in-IMX-6-SL-EVK-platform/m-p/497898#M80251</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp; Experts,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The IMX 6 SL EVK Android 5.1.1.2 build freezes after bootup. Then the kernel hangs after some times.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kindly find the logs below,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PM: suspend entry 1970-01-01 00:01:19.686132634 UTC&lt;/P&gt;&lt;P&gt;PM: Syncing filesystems ... done.&lt;/P&gt;&lt;P&gt;Freezing user space processes ...&lt;/P&gt;&lt;P&gt;PM: Wakeup pending, aborting suspend&lt;/P&gt;&lt;P&gt;last active wakeup source: eventpoll&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Freezing of tasks aborted after 0.007 seconds (36 tasks refusing to freeze, wq_busy=0):&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Restarting tasks ... done.&lt;/P&gt;&lt;P&gt;PM: suspend exit 1970-01-01 00:01:19.742020884 UTC&lt;/P&gt;&lt;P&gt;PM: suspend entry 1970-01-01 00:01:20.075762301 UTC&lt;/P&gt;&lt;P&gt;PM: Syncing filesystems ... done.&lt;/P&gt;&lt;P&gt;Freezing user space processes ... (elapsed 0.001 seconds) done.&lt;/P&gt;&lt;P&gt;Freezing remaining freezable tasks ... (elapsed 0.001 seconds) done.&lt;/P&gt;&lt;P&gt;Suspending console(s) (use no_console_suspend to debug&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Apr 2016 07:02:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Andriod-5-1-1-2-kernel-hangs-in-IMX-6-SL-EVK-platform/m-p/497898#M80251</guid>
      <dc:creator>lyfsci</dc:creator>
      <dc:date>2016-04-12T07:02:29Z</dc:date>
    </item>
    <item>
      <title>Re: Andriod 5.1.1.2 kernel hangs in IMX 6 SL EVK  platform</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Andriod-5-1-1-2-kernel-hangs-in-IMX-6-SL-EVK-platform/m-p/497899#M80252</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Any answers !!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Apr 2016 13:17:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Andriod-5-1-1-2-kernel-hangs-in-IMX-6-SL-EVK-platform/m-p/497899#M80252</guid>
      <dc:creator>lyfsci</dc:creator>
      <dc:date>2016-04-13T13:17:56Z</dc:date>
    </item>
    <item>
      <title>Re: Andriod 5.1.1.2 kernel hangs in IMX 6 SL EVK  platform</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Andriod-5-1-1-2-kernel-hangs-in-IMX-6-SL-EVK-platform/m-p/497900#M80253</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi lyf sci,&lt;/P&gt;&lt;P&gt;When you use the Demo images running on your board, does it boot up success? Here how do you build the BSP, is any error occur during building?&lt;/P&gt;&lt;P&gt;Have a nice day&lt;/P&gt;&lt;P&gt;Dan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Apr 2016 07:09:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Andriod-5-1-1-2-kernel-hangs-in-IMX-6-SL-EVK-platform/m-p/497900#M80253</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2016-04-15T07:09:18Z</dc:date>
    </item>
    <item>
      <title>Re: Andriod 5.1.1.2 kernel hangs in IMX 6 SL EVK  platform</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Andriod-5-1-1-2-kernel-hangs-in-IMX-6-SL-EVK-platform/m-p/497901#M80254</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Dan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is no error observed during the compilation process. But when the USB OTG cable remains plugged in then the above issues doesn't comes. Here how to disable the Suspend/resume in the Freescale AOSP ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Lyf&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Apr 2016 11:42:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Andriod-5-1-1-2-kernel-hangs-in-IMX-6-SL-EVK-platform/m-p/497901#M80254</guid>
      <dc:creator>lyfsci</dc:creator>
      <dc:date>2016-04-18T11:42:27Z</dc:date>
    </item>
    <item>
      <title>Re: Andriod 5.1.1.2 kernel hangs in IMX 6 SL EVK  platform</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Andriod-5-1-1-2-kernel-hangs-in-IMX-6-SL-EVK-platform/m-p/497902#M80255</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Lyf,&lt;/P&gt;&lt;P&gt;Sorry for late reply. When the android system boot up, and then go to sleep mode, when you insert other device such as USB flash disk， mouse or keyboard by USB OTG&amp;nbsp; the system will awake. So here you can go to the setting options on your android system, to set the display time. It will be OK.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Dan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Mark Correct&amp;nbsp; button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Apr 2016 08:38:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Andriod-5-1-1-2-kernel-hangs-in-IMX-6-SL-EVK-platform/m-p/497902#M80255</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2016-04-29T08:38:27Z</dc:date>
    </item>
  </channel>
</rss>