<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic DDR2 Calibration and Stress Test for i.MX28 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/DDR2-Calibration-and-Stress-Test-for-i-MX28/m-p/496227#M79880</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to run OBDS on a i.MX28 custom board with new DDR2 SDRAM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please share link or file for:&lt;/P&gt;&lt;P&gt;1. Correct version of DDR2 Register Programming Aid (xlsx file) for i.MX28&lt;/P&gt;&lt;P&gt;2. Correct version of DDR2 Calibration Test for i.MX28&lt;/P&gt;&lt;P&gt;3. Correct version of DDR2 Stress Test for i.MX28&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Arun&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 09 Feb 2016 12:41:27 GMT</pubDate>
    <dc:creator>arunachalamrama</dc:creator>
    <dc:date>2016-02-09T12:41:27Z</dc:date>
    <item>
      <title>DDR2 Calibration and Stress Test for i.MX28</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR2-Calibration-and-Stress-Test-for-i-MX28/m-p/496227#M79880</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to run OBDS on a i.MX28 custom board with new DDR2 SDRAM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please share link or file for:&lt;/P&gt;&lt;P&gt;1. Correct version of DDR2 Register Programming Aid (xlsx file) for i.MX28&lt;/P&gt;&lt;P&gt;2. Correct version of DDR2 Calibration Test for i.MX28&lt;/P&gt;&lt;P&gt;3. Correct version of DDR2 Stress Test for i.MX28&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Arun&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Feb 2016 12:41:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR2-Calibration-and-Stress-Test-for-i-MX28/m-p/496227#M79880</guid>
      <dc:creator>arunachalamrama</dc:creator>
      <dc:date>2016-02-09T12:41:27Z</dc:date>
    </item>
    <item>
      <title>Re: DDR2 Calibration and Stress Test for i.MX28</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR2-Calibration-and-Stress-Test-for-i-MX28/m-p/496228#M79881</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: Verdana; font-size: 12,0000pt;"&gt;Please look at my comments below.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: Verdana; font-size: 12,0000pt;"&gt;1.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: Verdana; font-size: 12,0000pt;"&gt;&amp;nbsp; Please refer to the following :&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;A href="https://community.nxp.com/docs/DOC-1455"&gt;Board Bring-up and DDR Initialization Tools&lt;/A&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: Verdana; font-size: 12,0000pt;"&gt;2.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: Verdana; font-size: 12,0000pt;"&gt;&amp;nbsp; There are the echo gating output and feedback signals (EMI_DDR_OPEN and &lt;/SPAN&gt;&lt;SPAN style="font-family: Verdana; font-size: 12,0000pt;"&gt;&lt;SPAN style="font-family: Verdana; font-size: 12,0000pt;"&gt;EMI_DDR_OPEN_FB), &lt;BR /&gt;used by the DRAM PHY to put a window around the DQS transition. &lt;/SPAN&gt;&lt;SPAN style="font-family: Verdana; font-size: 12,0000pt;"&gt;&lt;SPAN style="font-family: Verdana; font-size: 12,0000pt;"&gt;They should be routed so that &lt;BR /&gt;length of trace from DDR_Open to DDR_Open_FB is&amp;nbsp; &lt;/SPAN&gt;&lt;SPAN style="font-size: 12,0000pt; font-family: Verdana;"&gt;mean ( EMI_CLK+EMI_CLKn , DQS0+DQS0n, DQS1+DQS1n ).&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: Verdana; font-size: 12,0000pt;"&gt;Some calibration procedure could help in case of EMI_DDR_OPEN and EMI_DDR_OPEN_FB &lt;/SPAN&gt;&lt;SPAN style="font-size: 12,0000pt; font-family: Verdana;"&gt;signals violation, &lt;BR /&gt;but we do not have such code for calibration.&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: Verdana; font-size: 12,0000pt;"&gt;&lt;SPAN style="font-family: Verdana; font-size: 12,0000pt;"&gt; &lt;/SPAN&gt;&lt;SPAN style="font-size: 12,0000pt; font-family: Verdana;"&gt;3.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12,0000pt; font-family: Verdana;"&gt;&amp;nbsp; We do not have the Stress Test for I.MX28, but the following thread contains "mem_test",&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: Verdana; font-size: 12,0000pt;"&gt;which is based on FSL / NXP codes, used for DDR stress tester of i.MX6.&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: Verdana; font-size: 12,0000pt;"&gt;&lt;A href="https://community.nxp.com/message/375263"&gt;Re: i.MX28 DDR stress test&lt;/A&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: Verdana; font-size: 12,0000pt;"&gt;The Code Sourcery (Mentor) toolchain (host – Windows, executable (.elf)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: Verdana; font-size: 12,0000pt;"&gt;image&amp;nbsp; – for bare metal) was used to build it. As I know, such release is not&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: Verdana; font-size: 12,0000pt;"&gt;available now on Mentor web. You may try other GNU compiler.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: Verdana; font-size: 12,0000pt;"&gt;&amp;nbsp; One can try to load the test via a JTAG debugger (test.elf file should be used&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: Verdana; font-size: 12,0000pt;"&gt;here) or it is possible to load and run the test (test.sb) via USB in i.MX28 recovery&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: Verdana; font-size: 12,0000pt;"&gt;mode. Please use usb_load.bat for it. Note the sources contain memory initialization&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: Verdana; font-size: 12,0000pt;"&gt;for i.MX28 EVK. Perhaps it is needed to modify initialization for specific board. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Feb 2016 01:32:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR2-Calibration-and-Stress-Test-for-i-MX28/m-p/496228#M79881</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-02-10T01:32:35Z</dc:date>
    </item>
  </channel>
</rss>