<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: i.MX6SDL IDMAC setting for de-interlacing.</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6SDL-IDMAC-setting-for-de-interlacing/m-p/495888#M79776</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Pls refer to the Table 38-30. IPU's Processing flows:&lt;/P&gt;&lt;P&gt;Interlaced input coming from the memory via 3 channels 8, 9 and 10. &lt;/P&gt;&lt;P&gt;so channel 8 is useful. for more detailed information, you can refer to this table ,and you can refer to the source code in the unit test, name includs "tvin".&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 25 Dec 2015 08:04:29 GMT</pubDate>
    <dc:creator>joanxie</dc:creator>
    <dc:date>2015-12-25T08:04:29Z</dc:date>
    <item>
      <title>i.MX6SDL IDMAC setting for de-interlacing.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6SDL-IDMAC-setting-for-de-interlacing/m-p/495887#M79775</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Our partner have a question about i.MX6S IPU IDMAC.&lt;/P&gt;&lt;P&gt;They want to use VDIC de-interlacing processing, but it has not worked well.&lt;/P&gt;&lt;P&gt;Then, we are checking IDMAC setting.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[Q1]&lt;/P&gt;&lt;P&gt;Please see Table 38-29 in IMX6SDLRM Rev.2.&lt;/P&gt;&lt;P&gt;For de-interlacing, IDMAC_CH_5, 9, 10, and 13 should be enabled.&lt;/P&gt;&lt;P&gt;Next, please see Table 38-9, ch 8 seems to be also needed not only ch 5, 9, 10, and 13.&lt;/P&gt;&lt;P&gt;Should we enabled ch 8 also?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[Q2]&lt;/P&gt;&lt;P&gt;Actually, ch 0 in Table 38-9 is enabled now.&lt;/P&gt;&lt;P&gt;To use VDIC de-interlacing, should we disable ch 0 to prevent collision?&lt;/P&gt;&lt;P&gt;Or we can ignore it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Satoshi Shimoda&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Dec 2015 07:04:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6SDL-IDMAC-setting-for-de-interlacing/m-p/495887#M79775</guid>
      <dc:creator>satoshishimoda</dc:creator>
      <dc:date>2015-12-18T07:04:32Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6SDL IDMAC setting for de-interlacing.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6SDL-IDMAC-setting-for-de-interlacing/m-p/495888#M79776</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Pls refer to the Table 38-30. IPU's Processing flows:&lt;/P&gt;&lt;P&gt;Interlaced input coming from the memory via 3 channels 8, 9 and 10. &lt;/P&gt;&lt;P&gt;so channel 8 is useful. for more detailed information, you can refer to this table ,and you can refer to the source code in the unit test, name includs "tvin".&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Dec 2015 08:04:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6SDL-IDMAC-setting-for-de-interlacing/m-p/495888#M79776</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2015-12-25T08:04:29Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6SDL IDMAC setting for de-interlacing.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6SDL-IDMAC-setting-for-de-interlacing/m-p/495889#M79777</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI Guanqiong Xie,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your reply, and sorry my information for your was not sufficient.&lt;/P&gt;&lt;P&gt;Our partner is using CSI -&amp;gt; VDIC -&amp;gt; Mem path with the setting written in the following post.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/317265"&gt;i.MX6 CSI -&amp;amp;gt; VDIC path&lt;/A&gt; &lt;/P&gt;&lt;P&gt;According to your reply, channel 8 is useful for Mem -&amp;gt; VDIC -&amp;gt; Mem path.&lt;/P&gt;&lt;P&gt;But it is not useful for CSI -&amp;gt; VDIC -&amp;gt; Mem path since Table 38-29 does not mention channel 8, right?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Satoshi Shimoda&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Dec 2015 06:00:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6SDL-IDMAC-setting-for-de-interlacing/m-p/495889#M79777</guid>
      <dc:creator>satoshishimoda</dc:creator>
      <dc:date>2015-12-28T06:00:52Z</dc:date>
    </item>
  </channel>
</rss>