<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: How to confirm initialize i2c data about ov5640 camera.</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-confirm-initialize-i2c-data-about-ov5640-camera/m-p/495530#M79720</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;one more suggestion for you:&lt;/P&gt;&lt;P&gt;You can check the ov5640.c driver source code. It is located in linux/drivers/media/video/mxc/capture/.&lt;/P&gt;&lt;P&gt;There are two functions ov5640_write_reg() and ov5640_read_reg() using i2c for read and write the ov5640's registers.&lt;/P&gt;&lt;P&gt;And when run the ov5640_probe(), It will using ov5640_read_reg() to read the chip_id higher and lower bytes first. After checked the camera is ov5640, then it will initialize the camera by sending a set of data in ov5640_global_init_setting[],&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 22 Mar 2016 03:37:40 GMT</pubDate>
    <dc:creator>jimmychan</dc:creator>
    <dc:date>2016-03-22T03:37:40Z</dc:date>
    <item>
      <title>How to confirm initialize i2c data about ov5640 camera.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-confirm-initialize-i2c-data-about-ov5640-camera/m-p/495528#M79718</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;my configure set below&lt;/P&gt;&lt;P&gt;UBUNTU 12.04&lt;/P&gt;&lt;P&gt;kernel 3.0.35&lt;/P&gt;&lt;P&gt;LTIB&lt;/P&gt;&lt;P&gt;i.mx6q sabresd board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hello.&lt;/P&gt;&lt;P&gt;I want to confirm i2c data of ov5640 camera when boot i.mx6 board.&lt;/P&gt;&lt;P&gt;So.. I was check clk for i2c (R181 &amp;amp; R182) of CSI0(ov5640 camera).&lt;/P&gt;&lt;P&gt;But I don't know that is correct data.&lt;/P&gt;&lt;P&gt;when i check i2c data, &lt;/P&gt;&lt;P&gt;it is 0x38 ack 0x0D ack 0x39 ack 0x15..... i think .. it's wrong&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you have ov5640 camera initialize i2c data, share for me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ps. &lt;/P&gt;&lt;P&gt;Where can i search i2c data for changing data ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Mar 2016 01:57:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-confirm-initialize-i2c-data-about-ov5640-camera/m-p/495528#M79718</guid>
      <dc:creator>hanseunglee</dc:creator>
      <dc:date>2016-03-22T01:57:56Z</dc:date>
    </item>
    <item>
      <title>Re: How to confirm initialize i2c data about ov5640 camera.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-confirm-initialize-i2c-data-about-ov5640-camera/m-p/495529#M79719</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Hanseung&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can look at attached baremetal ov5640 camera codes from sdk.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Mar 2016 02:22:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-confirm-initialize-i2c-data-about-ov5640-camera/m-p/495529#M79719</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-03-22T02:22:25Z</dc:date>
    </item>
    <item>
      <title>Re: How to confirm initialize i2c data about ov5640 camera.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-confirm-initialize-i2c-data-about-ov5640-camera/m-p/495530#M79720</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;one more suggestion for you:&lt;/P&gt;&lt;P&gt;You can check the ov5640.c driver source code. It is located in linux/drivers/media/video/mxc/capture/.&lt;/P&gt;&lt;P&gt;There are two functions ov5640_write_reg() and ov5640_read_reg() using i2c for read and write the ov5640's registers.&lt;/P&gt;&lt;P&gt;And when run the ov5640_probe(), It will using ov5640_read_reg() to read the chip_id higher and lower bytes first. After checked the camera is ov5640, then it will initialize the camera by sending a set of data in ov5640_global_init_setting[],&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Mar 2016 03:37:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-confirm-initialize-i2c-data-about-ov5640-camera/m-p/495530#M79720</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2016-03-22T03:37:40Z</dc:date>
    </item>
  </channel>
</rss>