<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Problems using dual NIC with Linux images</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Problems-using-dual-NIC-with-Linux-images/m-p/182394#M7970</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;No it isn't an hardware issue, there is a bug in the network driver..&lt;BR /&gt;I've the same issue.&lt;BR /&gt;Look at this post:&lt;BR /&gt;&lt;A href="http://forums.freescale.com/t5/i-MX-Microprocessors/iMX28-Network-MDIO-timeout-recovery-and-lost-IRQs/td-p/73309" target="_blank"&gt;http://forums.freescale.com/t5/i-MX-Microprocessors/iMX28-Network-MDIO-timeout-recovery-and-lost-IRQs/td-p/73309&lt;/A&gt;&lt;/P&gt;&lt;P&gt;I've tried to apply the patch in the kernel 2.6.35 but it fails. &lt;BR /&gt;I've applied the patch by hand, but the problem isn't resolved.&lt;BR /&gt;Then I've commented the line writel(1, fep-&amp;gt;hwp + FEC_ECNTRL); in function fec_stop(). &lt;BR /&gt;In my opinion this is the best solution, most of the time the ethernet works fine, but sometimes the problem returns.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 12 Jun 2012 20:19:52 GMT</pubDate>
    <dc:creator>katte</dc:creator>
    <dc:date>2012-06-12T20:19:52Z</dc:date>
    <item>
      <title>Problems using dual NIC with Linux images</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problems-using-dual-NIC-with-Linux-images/m-p/182388#M7964</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello all-&lt;/P&gt;&lt;P&gt;I'm using the i.MX28EVK, and I'm having a hard time bringing up the second NIC consistently. I initially ran into this was the ltib build I made, but then I grabbed the included Linux SD card, and it results in the same behavior. The frustrating thing is that every 4-5 boots or so it works (using the reference image), but the rest of the time it doesn't. When it doesn't work, I get the following in the serial session (from the reference image marked "MX28EVK Linux 110-77224 Rev c"):&lt;/P&gt;&lt;P&gt;/***********************/&lt;/P&gt;&lt;P&gt;eth1: Freescale FEC PHY driver [Generic PHY] (mii_bus:phy_addr=0:01, irq=-1)&lt;BR /&gt;PHY: 0:01 - Link is Up - 100/Full&lt;BR /&gt;PHY: 0:01 - Link is Down&lt;BR /&gt;PHY: 0:01 - Link is Up - 100/Full&lt;BR /&gt;PHY: 0:01 - Link is Down&lt;BR /&gt;PHY: 0:01 - Link is Up - 100/Full&lt;/P&gt;&lt;P&gt;/***********************/&lt;/P&gt;&lt;P&gt;I thought for a while that it might be a hardware issue, but the the Windows CE reference build works every time I boot it.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Nov 2011 16:37:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problems-using-dual-NIC-with-Linux-images/m-p/182388#M7964</guid>
      <dc:creator>CH1z</dc:creator>
      <dc:date>2011-11-01T16:37:47Z</dc:date>
    </item>
    <item>
      <title>Re: Problems using dual NIC with Linux images</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problems-using-dual-NIC-with-Linux-images/m-p/182389#M7965</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Are you running a native Linux host or Linux host under VMWare?&amp;nbsp; My EVK setup initially worked fine with Ubuntu host running&amp;nbsp;under VMWare on a Win7 PC with a single NIC, but when I added a second dedicated NIC for the EVK ethernet link, It would no longer work.&amp;nbsp; I finally had Wireshark runnong on both the Windows side and the Ubuntu side of the (supposedly) same VMWare interface for the dedicated fixed IP link and could see packet traffic&amp;nbsp;stalling on both sides.&amp;nbsp; I converted the Win7 machine to a true dual-interface Ubuntu setup and all problems disappeared.&lt;/P&gt;&lt;P&gt;Good Luck,&lt;/P&gt;&lt;P&gt;Darrell&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Nov 2011 01:04:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problems-using-dual-NIC-with-Linux-images/m-p/182389#M7965</guid>
      <dc:creator>dingram1z</dc:creator>
      <dc:date>2011-11-11T01:04:50Z</dc:date>
    </item>
    <item>
      <title>Re: Problems using dual NIC with Linux images</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problems-using-dual-NIC-with-Linux-images/m-p/182390#M7966</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;P&gt;Thanks for the reply. I'm actually talking about the dual interface on the reference board, rather than in the dev VM machine.&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Nov 2011 02:30:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problems-using-dual-NIC-with-Linux-images/m-p/182390#M7966</guid>
      <dc:creator>CH1z</dc:creator>
      <dc:date>2011-11-11T02:30:59Z</dc:date>
    </item>
    <item>
      <title>Re: Problems using dual NIC with Linux images</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problems-using-dual-NIC-with-Linux-images/m-p/182391#M7967</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, I'm having the same issue.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 10 Jun 2012 04:14:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problems-using-dual-NIC-with-Linux-images/m-p/182391#M7967</guid>
      <dc:creator>tcmichals</dc:creator>
      <dc:date>2012-06-10T04:14:33Z</dc:date>
    </item>
    <item>
      <title>Re: Problems using dual NIC with Linux images</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problems-using-dual-NIC-with-Linux-images/m-p/182392#M7968</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;FWIW, eventually we were shipped a new EVK, which solved the issue. Our first board said "Rev. C" , but the new one that worked was marked "Rev D".&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Jun 2012 02:54:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problems-using-dual-NIC-with-Linux-images/m-p/182392#M7968</guid>
      <dc:creator>CH1z</dc:creator>
      <dc:date>2012-06-11T02:54:28Z</dc:date>
    </item>
    <item>
      <title>Re: Problems using dual NIC with Linux images</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problems-using-dual-NIC-with-Linux-images/m-p/182393#M7969</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Checked the rev, it is D.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Jun 2012 12:54:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problems-using-dual-NIC-with-Linux-images/m-p/182393#M7969</guid>
      <dc:creator>tcmichals</dc:creator>
      <dc:date>2012-06-11T12:54:24Z</dc:date>
    </item>
    <item>
      <title>Re: Problems using dual NIC with Linux images</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problems-using-dual-NIC-with-Linux-images/m-p/182394#M7970</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;No it isn't an hardware issue, there is a bug in the network driver..&lt;BR /&gt;I've the same issue.&lt;BR /&gt;Look at this post:&lt;BR /&gt;&lt;A href="http://forums.freescale.com/t5/i-MX-Microprocessors/iMX28-Network-MDIO-timeout-recovery-and-lost-IRQs/td-p/73309" target="_blank"&gt;http://forums.freescale.com/t5/i-MX-Microprocessors/iMX28-Network-MDIO-timeout-recovery-and-lost-IRQs/td-p/73309&lt;/A&gt;&lt;/P&gt;&lt;P&gt;I've tried to apply the patch in the kernel 2.6.35 but it fails. &lt;BR /&gt;I've applied the patch by hand, but the problem isn't resolved.&lt;BR /&gt;Then I've commented the line writel(1, fep-&amp;gt;hwp + FEC_ECNTRL); in function fec_stop(). &lt;BR /&gt;In my opinion this is the best solution, most of the time the ethernet works fine, but sometimes the problem returns.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Jun 2012 20:19:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problems-using-dual-NIC-with-Linux-images/m-p/182394#M7970</guid>
      <dc:creator>katte</dc:creator>
      <dc:date>2012-06-12T20:19:52Z</dc:date>
    </item>
    <item>
      <title>Re: Problems using dual NIC with Linux images</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problems-using-dual-NIC-with-Linux-images/m-p/182395#M7971</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Another useful post:&lt;/P&gt;&lt;P&gt;&lt;A href="http://imxcommunity.org/forum/topics/help-about-fec-problem"&gt;http://imxcommunity.org/forum/topics/help-about-fec-problem&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Jun 2012 20:36:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problems-using-dual-NIC-with-Linux-images/m-p/182395#M7971</guid>
      <dc:creator>katte</dc:creator>
      <dc:date>2012-06-12T20:36:50Z</dc:date>
    </item>
    <item>
      <title>Re: Problems using dual NIC with Linux images</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problems-using-dual-NIC-with-Linux-images/m-p/182396#M7972</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I got a fairly stable configuration.&lt;BR /&gt;I've deleted the line writel(1, fep-&amp;gt;hwp + FEC_ECNTRL);&lt;BR /&gt;In the file drivers/net/fec.c, function fec_stop().&lt;/P&gt;&lt;P&gt;I've also modified the file /etc/rc.d/init.d/network, adding &lt;BR /&gt;ifconfig eth0 down&lt;BR /&gt;ifconfig eth0 up&lt;BR /&gt;ifconfig eth0 down&lt;BR /&gt;ifconfig eth0 up&lt;BR /&gt;(2 times)&lt;/P&gt;&lt;P&gt;at the end of the configuration of eth0..&lt;BR /&gt;Now it seems that the ethernet is configured and working everytime.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Jun 2012 08:31:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problems-using-dual-NIC-with-Linux-images/m-p/182396#M7972</guid>
      <dc:creator>katte</dc:creator>
      <dc:date>2012-06-13T08:31:29Z</dc:date>
    </item>
  </channel>
</rss>