<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: i2c access in linux</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i2c-access-in-linux/m-p/182338#M7954</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Done, It is powered correctly.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've also noticed this morning that sound is no longer working. Could packages installed cause sound to no longer work? Sound is also on i2c, but it's on i2c1.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 02 Nov 2011 15:58:38 GMT</pubDate>
    <dc:creator>JoshuaParrish</dc:creator>
    <dc:date>2011-11-02T15:58:38Z</dc:date>
    <item>
      <title>i2c access in linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i2c-access-in-linux/m-p/182336#M7952</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everyone,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm having issues accessing and using i2c in linux.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What I am trying to do is set up a camera, the ov7725 using the ov772x driver in linux.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm using i2c-2 on the imx53 loco board (QSB board).&lt;/P&gt;&lt;P&gt;I'm also using CSI0.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Now to the problem, simply stated I can't see any i2c signals on i2c-2.&lt;/P&gt;&lt;P&gt;-I've changed my board file to include&amp;nbsp;&lt;/P&gt;&lt;P&gt;static struct mxc_camera_platform_data camera_data = {.analog_regulator = "VSD",.mclk = 24000000,.csi = 0,.pwdn = CSI0_PWDN,};&lt;BR /&gt;static struct i2c_board_info mxc_i2c2_board_info[] __initdata = { { .type = "ov772x", .addr = 0x21, .platform_data = (void *)&amp;amp;camera_data, },};&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Now the issues that I'm having with the camera are the .pwdn var in the&amp;nbsp;struct mxc_camera_platform_data camera_data; also&amp;nbsp;.platform_data = (void *)&amp;amp;camera_data,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;but that's with the camera.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The i2c is set up such that&amp;nbsp;&lt;/P&gt;&lt;P&gt;MX53_PAD_KEY_COL3__I2C2_SCL, MX53_PAD_KEY_ROW3__I2C2_SDA,&lt;/P&gt;&lt;P&gt;are in my pads function and&amp;nbsp;&lt;/P&gt;&lt;P&gt;i2c_register_board_info(2, mxc_i2c2_board_info,ARRAY_SIZE(mxc_i2c2_board_info));&lt;/P&gt;&lt;P&gt;is in my init function&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I've made a new kernel file and I have loaded it into my microsd I've found errors loading the ov772x module, however if I use a program called i2c-tools I can't even see i2c signals generated from the board.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;That being said, if I flip those ports to GPIO instead of i2c I see my signals changing (based off of echo 1 &amp;gt; /sys/class/gpio109/value)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So I know that those ports are still good ( I haven't damaged them.)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've dumped my board info file to show the whole code I'm using to setup i2c-2 for use.&lt;/P&gt;&lt;P&gt;Could anyone verify that setting it up this way should work?&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;/*&amp;nbsp;* Copyright (C) 2010-2011 Freescale Semiconductor, Inc. All Rights Reserved.&amp;nbsp;*/&lt;BR /&gt;/*&amp;nbsp;* This program is free software; you can redistribute it and/or modify&amp;nbsp;* it under the terms of the GNU General Public License as published by&amp;nbsp;* the Free Software Foundation; either version 2 of the License, or&amp;nbsp;* (at your option) any later version.&lt;BR /&gt;&amp;nbsp;* This program is distributed in the hope that it will be useful,&amp;nbsp;* but WITHOUT ANY WARRANTY; without even the implied warranty of&amp;nbsp;* MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. &amp;nbsp;See the&amp;nbsp;* GNU General Public License for more details.&lt;BR /&gt;&amp;nbsp;* You should have received a copy of the GNU General Public License along&amp;nbsp;* with this program; if not, write to the Free Software Foundation, Inc.,&amp;nbsp;* 51 Franklin Street, Fifth Floor, Boston, MA 02110-1301 USA.&amp;nbsp;*/&lt;BR /&gt;#include &amp;lt;linux/types.h&amp;gt;#include &amp;lt;linux/sched.h&amp;gt;#include &amp;lt;linux/delay.h&amp;gt;#include &amp;lt;linux/pm.h&amp;gt;#include &amp;lt;linux/interrupt.h&amp;gt;#include &amp;lt;linux/irq.h&amp;gt;#include &amp;lt;linux/init.h&amp;gt;#include &amp;lt;linux/input.h&amp;gt;#include &amp;lt;linux/nodemask.h&amp;gt;#include &amp;lt;linux/clk.h&amp;gt;#include &amp;lt;linux/platform_device.h&amp;gt;#include &amp;lt;linux/fsl_devices.h&amp;gt;#include &amp;lt;linux/spi/spi.h&amp;gt;#include &amp;lt;linux/i2c.h&amp;gt;#include &amp;lt;linux/ata.h&amp;gt;#include &amp;lt;linux/mtd/mtd.h&amp;gt;#include &amp;lt;linux/mtd/map.h&amp;gt;#include &amp;lt;linux/mtd/partitions.h&amp;gt;#include &amp;lt;linux/regulator/consumer.h&amp;gt;#include &amp;lt;linux/pmic_external.h&amp;gt;#include &amp;lt;linux/pmic_status.h&amp;gt;#include &amp;lt;linux/ipu.h&amp;gt;#include &amp;lt;linux/mxcfb.h&amp;gt;#include &amp;lt;linux/pwm_backlight.h&amp;gt;#include &amp;lt;linux/fec.h&amp;gt;#include &amp;lt;linux/ahci_platform.h&amp;gt;#include &amp;lt;linux/gpio_keys.h&amp;gt;#include &amp;lt;mach/common.h&amp;gt;#include &amp;lt;mach/hardware.h&amp;gt;#include &amp;lt;asm/irq.h&amp;gt;#include &amp;lt;asm/setup.h&amp;gt;#include &amp;lt;asm/mach-types.h&amp;gt;#include &amp;lt;asm/mach/arch.h&amp;gt;#include &amp;lt;asm/mach/time.h&amp;gt;#include &amp;lt;asm/mach/keypad.h&amp;gt;#include &amp;lt;asm/mach/flash.h&amp;gt;#include &amp;lt;mach/memory.h&amp;gt;#include &amp;lt;mach/gpio.h&amp;gt;#include &amp;lt;mach/mmc.h&amp;gt;#include &amp;lt;mach/mxc_dvfs.h&amp;gt;#include &amp;lt;mach/iomux-mx53.h&amp;gt;#include &amp;lt;mach/i2c.h&amp;gt;#include &amp;lt;mach/mxc_iim.h&amp;gt;&lt;BR /&gt;#include "crm_regs.h"#include "devices.h"#include "usb.h"&lt;BR /&gt;/*!&amp;nbsp;* @file mach-mx5/mx53_loco.c&amp;nbsp;*&amp;nbsp;* @brief This file contains MX53 loco board specific initialization routines.&amp;nbsp;*&amp;nbsp;* @ingroup MSL_MX53&amp;nbsp;*/&lt;BR /&gt;/* MX53 LOCO GPIO PIN configurations */#define NVDD_FAULT (0*32 + 5) /* GPIO1_5 */&lt;BR /&gt;#define FEC_INT (1*32 + 4) /* GPIO_2_4 */#define HEADPHONE_DEC_B (1*32 + 5) /* GPIO_2_5 */#define MIC_DEC_B (1*32 + 6) /* GPIO_2_6 */#define USER_UI1 (1*32 + 14) /* GPIO_2_14 */#define USER_UI2 (1*32 + 15) /* GPIO_2_15 */#define MX53_nONKEY (0*32 + 8) /* GPIO_1_8 */&lt;BR /&gt;#define SD3_CD (2*32 + 11) /* GPIO_3_11 */#define SD3_WP (2*32 + 12) /* GPIO_3_12 */#define DISP0_POWER_EN (2*32 + 24) /* GPIO_3_24 */#define DISP0_DET_INT (2*32 + 31) /* GPIO_3_31 */&lt;BR /&gt;#define DISP0_RESET (4*32 + 0) /* GPIO_5_0 */&lt;BR /&gt;#define CSI0_RTSB (5*32 + 9) /* GPIO_6_9 */#define CSI0_PWDN (5*32 + 10) /* GPIO_6_10 */#define ACCL_EN (5*32 + 14) /* GPIO_6_14 */#define ACCL_INT1_IN (5*32 + 15) /* GPIO_6_15 */#define ACCL_INT2_IN (5*32 + 16) /* GPIO_6_16 */&lt;BR /&gt;#define LCD_BLT_EN (6*32 + 2) /* GPIO_7_2 */#define FEC_RST (6*32 + 6) /* GPIO_7_6 */#define USER_LED_EN (6*32 + 7) /* GPIO_7_7 */#define USB_PWREN (6*32 + 8) /* GPIO_7_8 */#define NIRQ (6*32 + 11) /* GPIO7_11 */// Added by JP#define IR_CTRL (6*32 + 12) /* GPIO7_12 */&lt;BR /&gt;extern int __init mx53_loco_init_da9052(void);&lt;BR /&gt;static struct pad_desc mx53_loco_pads[] = { /* FEC */ MX53_PAD_FEC_MDC__FEC_MDC, MX53_PAD_FEC_MDIO__FEC_MDIO, MX53_PAD_FEC_REF_CLK__FEC_REF_CLK, MX53_PAD_FEC_RX_ER__FEC_RX_ER, MX53_PAD_FEC_CRS_DV__FEC_CRS_DV, MX53_PAD_FEC_RXD1__FEC_RXD1, MX53_PAD_FEC_RXD0__FEC_RXD0, MX53_PAD_FEC_TX_EN__FEC_TX_EN, MX53_PAD_FEC_TXD1__FEC_TXD1, MX53_PAD_FEC_TXD0__FEC_TXD0, /* FEC_nRST */ MX53_PAD_ATA_DA_0__GPIO_7_6, /* FEC_nINT */ MX53_PAD_ATA_DATA4__GPIO_2_4, /* AUDMUX5 */ MX53_PAD_KEY_COL0__AUD5_TXC, MX53_PAD_KEY_ROW0__AUD5_TXD, MX53_PAD_KEY_COL1__AUD5_TXFS, MX53_PAD_KEY_ROW1__AUD5_RXD, /* I2C2 */ //MX53_PAD_KEY_COL3__GPIO_4_12, //Make GPIO //MX53_PAD_KEY_ROW3__GPIO_4_13, //Make GPIO MX53_PAD_KEY_COL3__I2C2_SCL, MX53_PAD_KEY_ROW3__I2C2_SDA, /* SD1 */ MX53_PAD_SD1_CMD__SD1_CMD, MX53_PAD_SD1_CLK__SD1_CLK, MX53_PAD_SD1_DATA0__SD1_DATA0, MX53_PAD_SD1_DATA1__SD1_DATA1, MX53_PAD_SD1_DATA2__SD1_DATA2, MX53_PAD_SD1_DATA3__SD1_DATA3, /* SD3 */ MX53_PAD_ATA_DATA8__SD3_DAT0, MX53_PAD_ATA_DATA9__SD3_DAT1, MX53_PAD_ATA_DATA10__SD3_DAT2, MX53_PAD_ATA_DATA11__SD3_DAT3, MX53_PAD_ATA_DATA0__SD3_DAT4, MX53_PAD_ATA_DATA1__SD3_DAT5, MX53_PAD_ATA_DATA2__SD3_DAT6, MX53_PAD_ATA_DATA3__SD3_DAT7, MX53_PAD_ATA_IORDY__SD3_CLK, MX53_PAD_ATA_RESET_B__SD3_CMD, /* SD3_CD */ MX53_PAD_EIM_DA11__GPIO_3_11, /* SD3_WP */ MX53_PAD_EIM_DA12__GPIO_3_12, /* VGA */ MX53_PAD_EIM_OE__DI1_PIN7, MX53_PAD_EIM_RW__DI1_PIN8, /* DISPLB */ MX53_PAD_EIM_D20__SER_DISP0_CS, MX53_PAD_EIM_D21__DISPB0_SER_CLK, MX53_PAD_EIM_D22__DISPB0_SER_DIN, MX53_PAD_EIM_D23__DI0_D0_CS, /* DISP0_POWER_EN */ MX53_PAD_EIM_D24__GPIO_3_24, /* DISP0 DET INT */ MX53_PAD_EIM_D31__GPIO_3_31,&lt;BR /&gt; /* LVDS */ MX53_PAD_LVDS0_TX3_P__LVDS0_TX3, MX53_PAD_LVDS0_CLK_P__LVDS0_CLK, MX53_PAD_LVDS0_TX2_P__LVDS0_TX2, MX53_PAD_LVDS0_TX1_P__LVDS0_TX1, MX53_PAD_LVDS0_TX0_P__LVDS0_TX0, MX53_PAD_LVDS1_TX3_P__LVDS1_TX3, MX53_PAD_LVDS1_TX2_P__LVDS1_TX2, MX53_PAD_LVDS1_CLK_P__LVDS1_CLK, MX53_PAD_LVDS1_TX1_P__LVDS1_TX1, MX53_PAD_LVDS1_TX0_P__LVDS1_TX0, /* I2C1 */ MX53_PAD_CSI0_D8__I2C1_SDA, MX53_PAD_CSI0_D9__I2C1_SCL, /* UART1 */ MX53_PAD_CSI0_D10__UART1_TXD, MX53_PAD_CSI0_D11__UART1_RXD, /* CSI0 */ MX53_PAD_CSI0_D12__CSI0_D12, MX53_PAD_CSI0_D13__CSI0_D13, MX53_PAD_CSI0_D14__CSI0_D14, MX53_PAD_CSI0_D15__CSI0_D15, MX53_PAD_CSI0_D16__CSI0_D16, MX53_PAD_CSI0_D17__CSI0_D17, MX53_PAD_CSI0_D18__CSI0_D18, MX53_PAD_CSI0_D19__CSI0_D19, MX53_PAD_CSI0_VSYNC__CSI0_VSYNC, MX53_PAD_CSI0_MCLK__CSI0_HSYNC, MX53_PAD_CSI0_PIXCLK__CSI0_PIXCLK, /* DISPLAY */ MX53_PAD_DI0_DISP_CLK__DI0_DISP_CLK, MX53_PAD_DI0_PIN15__DI0_PIN15, MX53_PAD_DI0_PIN2__DI0_PIN2, MX53_PAD_DI0_PIN3__DI0_PIN3, MX53_PAD_DISP0_DAT0__DISP0_DAT0, MX53_PAD_DISP0_DAT1__DISP0_DAT1, MX53_PAD_DISP0_DAT2__DISP0_DAT2, MX53_PAD_DISP0_DAT3__DISP0_DAT3, MX53_PAD_DISP0_DAT4__DISP0_DAT4, MX53_PAD_DISP0_DAT5__DISP0_DAT5, MX53_PAD_DISP0_DAT6__DISP0_DAT6, MX53_PAD_DISP0_DAT7__DISP0_DAT7, MX53_PAD_DISP0_DAT8__DISP0_DAT8, MX53_PAD_DISP0_DAT9__DISP0_DAT9, MX53_PAD_DISP0_DAT10__DISP0_DAT10, MX53_PAD_DISP0_DAT11__DISP0_DAT11, MX53_PAD_DISP0_DAT12__DISP0_DAT12, MX53_PAD_DISP0_DAT13__DISP0_DAT13, MX53_PAD_DISP0_DAT14__DISP0_DAT14, MX53_PAD_DISP0_DAT15__DISP0_DAT15, MX53_PAD_DISP0_DAT16__DISP0_DAT16, MX53_PAD_DISP0_DAT17__DISP0_DAT17, MX53_PAD_DISP0_DAT18__DISP0_DAT18, MX53_PAD_DISP0_DAT19__DISP0_DAT19, MX53_PAD_DISP0_DAT20__DISP0_DAT20, MX53_PAD_DISP0_DAT21__DISP0_DAT21, MX53_PAD_DISP0_DAT22__DISP0_DAT22, MX53_PAD_DISP0_DAT23__DISP0_DAT23, /* Audio CLK*/ MX53_PAD_GPIO_0__SSI_EXT1_CLK, /* PWM */ MX53_PAD_GPIO_1__PWMO, /* SPDIF */ MX53_PAD_GPIO_7__PLOCK, //MX53_PAD_GPIO_17__SPDIF_OUT1, /* GPIO */ MX53_PAD_ATA_DA_1__GPIO_7_7, MX53_PAD_ATA_DA_2__GPIO_7_8, MX53_PAD_ATA_DATA5__GPIO_2_5, MX53_PAD_ATA_DATA6__GPIO_2_6, MX53_PAD_ATA_DATA14__GPIO_2_14, MX53_PAD_ATA_DATA15__GPIO_2_15, MX53_PAD_ATA_INTRQ__GPIO_7_2, MX53_PAD_EIM_WAIT__GPIO_5_0, MX53_PAD_NANDF_WP_B__GPIO_6_9, MX53_PAD_NANDF_RB0__GPIO_6_10, MX53_PAD_NANDF_CS1__GPIO_6_14, MX53_PAD_NANDF_CS2__GPIO_6_15, MX53_PAD_NANDF_CS3__GPIO_6_16, MX53_PAD_GPIO_5__GPIO_1_5, MX53_PAD_GPIO_16__GPIO_7_11, MX53_PAD_GPIO_8__GPIO_1_8, /*IR_CTRL*/ MX53_PAD_GPIO_17__GPIO_7_12,};&lt;BR /&gt;static struct fb_videomode video_modes[] = { { /* NTSC TV output */ "TV-NTSC", 60, 720, 480, 74074, 122, 15, 18, 26, 1, 1, FB_SYNC_HOR_HIGH_ACT | FB_SYNC_VERT_HIGH_ACT, FB_VMODE_INTERLACED, 0,}, { /* PAL TV output */ "TV-PAL", 50, 720, 576, 74074, 132, 11, 22, 26, 1, 1, FB_SYNC_HOR_HIGH_ACT | FB_SYNC_VERT_HIGH_ACT, FB_VMODE_INTERLACED | FB_VMODE_ODD_FLD_FIRST, 0,}, { /* 1080i50 TV output */ "1080I50", 50, 1920, 1080, 13468, 192, 527, 20, 24, 1, 1, FB_SYNC_HOR_HIGH_ACT | FB_SYNC_VERT_HIGH_ACT, FB_VMODE_INTERLACED | FB_VMODE_ODD_FLD_FIRST, 0,}, { /* 1080i60 TV output */ "1080I60", 60, 1920, 1080, 13468, 192, 87, 20, 24, 1, 1, FB_SYNC_HOR_HIGH_ACT | FB_SYNC_VERT_HIGH_ACT, FB_VMODE_INTERLACED | FB_VMODE_ODD_FLD_FIRST, 0,}, { /* 800x480 @ 57 Hz , pixel clk @ 27MHz */ "CLAA-WVGA", 57, 800, 480, 37037, 40, 60, 10, 10, 20, 10, FB_SYNC_CLK_LAT_FALL, FB_VMODE_NONINTERLACED, 0,}, { /* 800x480 @ 60 Hz , pixel clk @ 32MHz */ "SEIKO-WVGA", 60, 800, 480, 29850, 89, 164, 23, 10, 10, 10, FB_SYNC_CLK_LAT_FALL, FB_VMODE_NONINTERLACED, 0,}, { "XGA", 60, 1024, 768, 15385, 220, 40, 21, 7, 60, 10, 0, FB_VMODE_NONINTERLACED, 0,}, { /* 720p30 TV output */ "720P30", 30, 1280, 720, 13468, 260, 1759, 25, 4, 1, 1, FB_SYNC_HOR_HIGH_ACT | FB_SYNC_VERT_HIGH_ACT, FB_VMODE_NONINTERLACED, 0,}, { "720P60", 60, 1280, 720, 13468, 260, 109, 25, 4, 1, 1, FB_SYNC_HOR_HIGH_ACT | FB_SYNC_VERT_HIGH_ACT, FB_VMODE_NONINTERLACED, 0,}, { /* VGA 1280x1024 108M pixel clk output */ "SXGA", 60, 1280, 1024, 9259, 48, 248, 1, 38, 112, 3, 0, FB_VMODE_NONINTERLACED, 0,}, { /* 1600x1200 @ 60 Hz 162M pixel clk*/ "UXGA", 60, 1600, 1200, 6172, 304, 64, 1, 46, 192, 3, FB_SYNC_HOR_HIGH_ACT|FB_SYNC_VERT_HIGH_ACT, FB_VMODE_NONINTERLACED, 0,}, { /* 1080p24 TV output */ "1080P24", 24, 1920, 1080, 13468, 192, 637, 38, 6, 1, 1, FB_SYNC_HOR_HIGH_ACT | FB_SYNC_VERT_HIGH_ACT, FB_VMODE_NONINTERLACED, 0,}, { /* 1080p25 TV output */ "1080P25", 25, 1920, 1080, 13468, 192, 527, 38, 6, 1, 1, FB_SYNC_HOR_HIGH_ACT | FB_SYNC_VERT_HIGH_ACT, FB_VMODE_NONINTERLACED, 0,}, { /* 1080p30 TV output */ "1080P30", 30, 1920, 1080, 13468, 192, 87, 38, 6, 1, 1, FB_SYNC_HOR_HIGH_ACT | FB_SYNC_VERT_HIGH_ACT, FB_VMODE_NONINTERLACED, 0,}, { "1080P60", 60, 1920, 1080, 7692, 100, 40, 30, 3, 10, 2, 0, FB_VMODE_NONINTERLACED, 0,},};&lt;BR /&gt;static struct platform_pwm_backlight_data mxc_pwm_backlight_data = { .pwm_id = 1, .max_brightness = 255, .dft_brightness = 128, .pwm_period_ns = 50000,};&lt;BR /&gt;extern void mx5_ipu_reset(void);static struct mxc_ipu_config mxc_ipu_data = { .rev = 3, .reset = mx5_ipu_reset,};&lt;BR /&gt;extern void mx5_vpu_reset(void);static struct mxc_vpu_platform_data mxc_vpu_data = { .reset = mx5_vpu_reset,};&lt;BR /&gt;static struct fec_platform_data fec_data = { .phy = PHY_INTERFACE_MODE_RMII,};&lt;BR /&gt;static struct mxc_dvfs_platform_data dvfs_core_data = { .reg_id = "DA9052_BUCK_CORE", .clk1_id = "cpu_clk", .clk2_id = "gpc_dvfs_clk", .gpc_cntr_offset = MXC_GPC_CNTR_OFFSET, .gpc_vcr_offset = MXC_GPC_VCR_OFFSET, .ccm_cdcr_offset = MXC_CCM_CDCR_OFFSET, .ccm_cacrr_offset = MXC_CCM_CACRR_OFFSET, .ccm_cdhipr_offset = MXC_CCM_CDHIPR_OFFSET, .prediv_mask = 0x1F800, .prediv_offset = 11, .prediv_val = 3, .div3ck_mask = 0xE0000000, .div3ck_offset = 29, .div3ck_val = 2, .emac_val = 0x08, .upthr_val = 25, .dnthr_val = 9, .pncthr_val = 33, .upcnt_val = 10, .dncnt_val = 10, .delay_time = 30,};&lt;BR /&gt;static struct mxc_bus_freq_platform_data bus_freq_data = { .gp_reg_id = "DA9052_BUCK_CORE", .lp_reg_id = "DA9052_BUCK_PRO",};&lt;BR /&gt;static struct tve_platform_data tve_data = { .dac_reg = "DA9052_LDO7",};&lt;BR /&gt;static struct ldb_platform_data ldb_data = { .ext_ref = 1,};&lt;BR /&gt;static void mxc_iim_enable_fuse(void){ u32 reg;&lt;BR /&gt; if (!ccm_base) return;&lt;BR /&gt; /* enable fuse blown */ reg = readl(ccm_base + 0x64); reg |= 0x10; writel(reg, ccm_base + 0x64);}&lt;BR /&gt;static void mxc_iim_disable_fuse(void){ u32 reg;&lt;BR /&gt; if (!ccm_base) return; /* enable fuse blown */ reg = readl(ccm_base + 0x64); reg &amp;amp;= ~0x10; writel(reg, ccm_base + 0x64);}&lt;BR /&gt;static struct mxc_iim_data iim_data = { .bank_start = MXC_IIM_MX53_BANK_START_ADDR, .bank_end &amp;nbsp; = MXC_IIM_MX53_BANK_END_ADDR, .enable_fuse = mxc_iim_enable_fuse, .disable_fuse = mxc_iim_disable_fuse,};&lt;BR /&gt;static struct resource mxcfb_resources[] = { [0] = { &amp;nbsp; &amp;nbsp; &amp;nbsp; .flags = IORESOURCE_MEM, &amp;nbsp; &amp;nbsp; &amp;nbsp; },};&lt;BR /&gt;static struct mxc_fb_platform_data fb_data[] = { { .interface_pix_fmt = IPU_PIX_FMT_RGB565, .mode_str = "CLAA-WVGA", .mode = video_modes, .num_modes = ARRAY_SIZE(video_modes), }, { .interface_pix_fmt = IPU_PIX_FMT_BGR24, .mode_str = "XGA", .mode = video_modes, .num_modes = ARRAY_SIZE(video_modes), },};&lt;BR /&gt;extern int primary_di;static int __init mxc_init_fb(void){ if (!machine_is_mx53_loco()) return 0;&lt;BR /&gt; if (primary_di) { printk(KERN_INFO "DI1 is primary\n"); /* DI1 -&amp;gt; DP-BG channel: */ mxc_fb_devices[1].num_resources = ARRAY_SIZE(mxcfb_resources); mxc_fb_devices[1].resource = mxcfb_resources; mxc_register_device(&amp;amp;mxc_fb_devices[1], &amp;amp;fb_data[1]);&lt;BR /&gt; /* DI0 -&amp;gt; DC channel: */ mxc_register_device(&amp;amp;mxc_fb_devices[0], &amp;amp;fb_data[0]); } else { printk(KERN_INFO "DI0 is primary\n");&lt;BR /&gt; /* DI0 -&amp;gt; DP-BG channel: */ mxc_fb_devices[0].num_resources = ARRAY_SIZE(mxcfb_resources); mxc_fb_devices[0].resource = mxcfb_resources; mxc_register_device(&amp;amp;mxc_fb_devices[0], &amp;amp;fb_data[0]);&lt;BR /&gt; /* DI1 -&amp;gt; DC channel: */ mxc_register_device(&amp;amp;mxc_fb_devices[1], &amp;amp;fb_data[1]); }&lt;BR /&gt; /* * DI0/1 DP-FG channel: */ mxc_register_device(&amp;amp;mxc_fb_devices[2], NULL);&lt;BR /&gt; return 0;}device_initcall(mxc_init_fb);&lt;BR /&gt;static void sii9022_hdmi_reset(void){ gpio_set_value(DISP0_RESET, 0); msleep(10); gpio_set_value(DISP0_RESET, 1); msleep(10);}&lt;BR /&gt;static struct mxc_lcd_platform_data sii9022_hdmi_data = {&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;.reset = sii9022_hdmi_reset,};&lt;BR /&gt;static struct imxi2c_platform_data mxci2c_data = {&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;.bitrate = 100000,};&lt;BR /&gt;static struct i2c_board_info mxc_i2c0_board_info[] __initdata = { { .type = "mma8450", .addr = 0x1C, },};&lt;BR /&gt;static struct i2c_board_info mxc_i2c1_board_info[] __initdata = { { .type = "sgtl5000-i2c", .addr = 0x0a, }, { .type = "sii9022", .addr = 0x39, .irq = IOMUX_TO_IRQ_V3(DISP0_DET_INT), .platform_data = &amp;amp;sii9022_hdmi_data, },};// ADDED by Joshua Parrish Project ISHKA for camera OV7725&lt;BR /&gt;static struct mxc_camera_platform_data camera_data = {.analog_regulator = "VSD",.mclk = 24000000,.csi = 0,.pwdn = CSI0_PWDN,};&lt;BR /&gt;static struct i2c_board_info mxc_i2c2_board_info[] __initdata = { { .type = "ov772x", .addr = 0x21, .platform_data = (void *)&amp;amp;camera_data, },};// ----- Completed&lt;BR /&gt;static int sdhc_write_protect(struct device *dev){ int ret = 0;&lt;BR /&gt; if (to_platform_device(dev)-&amp;gt;id == 2) ret = gpio_get_value(SD3_WP);&lt;BR /&gt; return ret;}&lt;BR /&gt;static unsigned int sdhc_get_card_det_status(struct device *dev){ int ret = 0;&lt;BR /&gt; if (to_platform_device(dev)-&amp;gt;id == 2) ret = gpio_get_value(SD3_CD);&lt;BR /&gt; return ret;}&lt;BR /&gt;static struct mxc_mmc_platform_data mmc1_data = { .ocr_mask = MMC_VDD_27_28 | MMC_VDD_28_29 | MMC_VDD_29_30 | MMC_VDD_31_32, .caps = MMC_CAP_4_BIT_DATA, .min_clk = 400000, .max_clk = 50000000, .card_inserted_state = 1, .clock_mmc = "esdhc_clk", .power_mmc = NULL,};&lt;BR /&gt;static struct mxc_mmc_platform_data mmc3_data = { .ocr_mask = MMC_VDD_27_28 | MMC_VDD_28_29 | MMC_VDD_29_30 | MMC_VDD_31_32, .caps = MMC_CAP_4_BIT_DATA | MMC_CAP_8_BIT_DATA | MMC_CAP_DATA_DDR, .min_clk = 400000, .max_clk = 50000000, .card_inserted_state = 0, .status = sdhc_get_card_det_status, .wp_status = sdhc_write_protect, .clock_mmc = "esdhc_clk",};&lt;BR /&gt;static int headphone_det_status(void){ return (gpio_get_value(HEADPHONE_DEC_B) == 0);}&lt;BR /&gt;static int mxc_sgtl5000_init(void);&lt;BR /&gt;static struct mxc_audio_platform_data sgtl5000_data = { .ssi_num = 1, .src_port = 2, .ext_port = 5, .hp_irq = IOMUX_TO_IRQ_V3(HEADPHONE_DEC_B), .hp_status = headphone_det_status, .init = mxc_sgtl5000_init,};&lt;BR /&gt;static int mxc_sgtl5000_init(void){ struct clk *ssi_ext1; int rate;&lt;BR /&gt; ssi_ext1 = clk_get(NULL, "ssi_ext1_clk"); if (IS_ERR(ssi_ext1)) return -1;&lt;BR /&gt; rate = clk_round_rate(ssi_ext1, 24000000); if (rate &amp;lt; 8000000 || rate &amp;gt; 27000000) { printk(KERN_ERR "Error: SGTL5000 mclk freq %d out of range!\n", &amp;nbsp; rate); clk_put(ssi_ext1); return -1; }&lt;BR /&gt; clk_set_rate(ssi_ext1, rate); clk_enable(ssi_ext1); sgtl5000_data.sysclk = rate;&lt;BR /&gt; return 0;}&lt;BR /&gt;static struct platform_device mxc_sgtl5000_device = { .name = "imx-3stack-sgtl5000",};&lt;BR /&gt;static struct mxc_asrc_platform_data mxc_asrc_data = { .channel_bits = 4, .clk_map_ver = 2,};&lt;BR /&gt;static struct mxc_spdif_platform_data mxc_spdif_data = { .spdif_tx = 1, .spdif_rx = 0, .spdif_clk_44100 = -1, /* Souce from CKIH1 for 44.1K */ /* Source from CCM spdif_clk (24M) for 48k and 32k * It's not accurate */ .spdif_clk_48000 = 1, .spdif_clkid = 0, .spdif_clk = NULL, /* spdif bus clk */};&lt;BR /&gt;static void mx53_loco_usbh1_vbus(bool on){ if (on) gpio_set_value(USB_PWREN, 1); else gpio_set_value(USB_PWREN, 0);}&lt;BR /&gt;#if defined(CONFIG_KEYBOARD_GPIO) || defined(CONFIG_KEYBOARD_GPIO_MODULE)#define GPIO_BUTTON(gpio_num, ev_code, act_low, descr, wake) \{ \ .gpio = gpio_num, \ .type = EV_KEY, \ .code = ev_code, \ .active_low = act_low, \ .desc = "btn " descr, \ .wakeup = wake, \}&lt;BR /&gt;static struct gpio_keys_button loco_buttons[] = { GPIO_BUTTON(MX53_nONKEY, KEY_POWER, 1, "power", 0), GPIO_BUTTON(USER_UI1, KEY_VOLUMEUP, 1, "volume-up", 0), GPIO_BUTTON(USER_UI2, KEY_VOLUMEDOWN, 1, "volume-down", 0),};&lt;BR /&gt;static struct gpio_keys_platform_data loco_button_data = { .buttons = loco_buttons, .nbuttons = ARRAY_SIZE(loco_buttons),};&lt;BR /&gt;static struct platform_device loco_button_device = { .name = "gpio-keys", .id = -1, .num_resources &amp;nbsp;= 0, .dev = { .platform_data = &amp;amp;loco_button_data, }};&lt;BR /&gt;static void __init loco_add_device_buttons(void){ platform_device_register(&amp;amp;loco_button_device);}#elsestatic void __init loco_add_device_buttons(void) {}#endif&lt;BR /&gt;&lt;BR /&gt;/*!&amp;nbsp;* Board specific fixup function. It is called by \b setup_arch() in&amp;nbsp;* setup.c file very early on during kernel starts. It allows the user to&amp;nbsp;* statically fill in the proper values for the passed-in parameters. None of&amp;nbsp;* the parameters is used currently.&amp;nbsp;*&amp;nbsp;* @param &amp;nbsp;desc &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; pointer to \b struct \b machine_desc&amp;nbsp;* @param &amp;nbsp;tags &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; pointer to \b struct \b tag&amp;nbsp;* @param &amp;nbsp;cmdline &amp;nbsp; &amp;nbsp; &amp;nbsp;pointer to the command line&amp;nbsp;* @param &amp;nbsp;mi &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; pointer to \b struct \b meminfo&amp;nbsp;*/static void __init fixup_mxc_board(struct machine_desc *desc, struct tag *tags, &amp;nbsp; char **cmdline, struct meminfo *mi){ struct tag *t; struct tag *mem_tag = 0; int total_mem = SZ_1G; int left_mem = 0; int gpu_mem = SZ_128M; int fb_mem = SZ_32M; char *str;&lt;BR /&gt; mxc_set_cpu_type(MXC_CPU_MX53);&lt;BR /&gt; for_each_tag(mem_tag, tags) { if (mem_tag-&amp;gt;hdr.tag == ATAG_MEM) { total_mem = mem_tag-&amp;gt;u.mem.size; left_mem = total_mem - gpu_mem - fb_mem; break; } }&lt;BR /&gt; for_each_tag(t, tags) { if (t-&amp;gt;hdr.tag == ATAG_CMDLINE) { str = t-&amp;gt;u.cmdline.cmdline; str = strstr(str, "mem="); if (str != NULL) { str += 4; left_mem = memparse(str, &amp;amp;str); if (left_mem == 0 || left_mem &amp;gt; total_mem) left_mem = total_mem - gpu_mem - fb_mem; }&lt;BR /&gt; str = t-&amp;gt;u.cmdline.cmdline; str = strstr(str, "gpu_memory="); if (str != NULL) { str += 11; gpu_mem = memparse(str, &amp;amp;str); }&lt;BR /&gt; break; } }&lt;BR /&gt; if (mem_tag) { fb_mem = total_mem - left_mem - gpu_mem; if (fb_mem &amp;lt; 0) { gpu_mem = total_mem - left_mem; fb_mem = 0; } mem_tag-&amp;gt;u.mem.size = left_mem;&lt;BR /&gt; /*reserve memory for gpu*/ gpu_device.resource[5].start = mem_tag-&amp;gt;u.mem.start + left_mem; gpu_device.resource[5].end = gpu_device.resource[5].start + gpu_mem - 1;#if defined(CONFIG_FB_MXC_SYNC_PANEL) || \ defined(CONFIG_FB_MXC_SYNC_PANEL_MODULE) if (fb_mem) { mxcfb_resources[0].start = gpu_device.resource[5].end + 1; mxcfb_resources[0].end = mxcfb_resources[0].start + fb_mem - 1; } else { mxcfb_resources[0].start = 0; mxcfb_resources[0].end = 0; }#endif }}&lt;BR /&gt;static void __init mx53_loco_io_init(void){ mxc_iomux_v3_setup_multiple_pads(mx53_loco_pads, ARRAY_SIZE(mx53_loco_pads));&lt;BR /&gt; /* SD3 */ gpio_request(SD3_CD, "sd3-cd"); gpio_direction_input(SD3_CD); gpio_request(SD3_WP, "sd3-wp"); gpio_direction_input(SD3_WP);&lt;BR /&gt; /* reset FEC PHY */ gpio_request(FEC_RST, "fec-rst"); gpio_direction_output(FEC_RST, 0); gpio_set_value(FEC_RST, 0); msleep(1); gpio_set_value(FEC_RST, 1);&lt;BR /&gt; /* headphone_det_b */ gpio_request(HEADPHONE_DEC_B, "headphone-dec"); gpio_direction_input(HEADPHONE_DEC_B);&lt;BR /&gt; /* USB PWR enable */ gpio_request(USB_PWREN, "usb-pwr"); gpio_direction_output(USB_PWREN, 0);&lt;BR /&gt; /* Sii9022 HDMI controller */ gpio_request(DISP0_RESET, "disp0-reset"); gpio_direction_output(DISP0_RESET, 0); gpio_request(DISP0_DET_INT, "disp0-detect"); gpio_direction_input(DISP0_DET_INT);&lt;BR /&gt; /* LCD panel power enable */ gpio_request(DISP0_POWER_EN, "disp0-power-en"); gpio_direction_output(DISP0_POWER_EN, 1);&lt;BR /&gt; // Section added by JP to turn off IR to start /* IR_CTRL */ /* gpio_request(IR_CTRL, "IR_CTRL"); gpio_direction_output(IR_CTRL, 0); gpio_set_value(IR_CTRL, 0); */}&lt;BR /&gt;/*!&amp;nbsp;* Board specific initialization.&amp;nbsp;*/static void __init mxc_board_init(void){ mxc_ipu_data.di_clk[0] = clk_get(NULL, "ipu_di0_clk"); mxc_ipu_data.di_clk[1] = clk_get(NULL, "ipu_di1_clk"); mxc_ipu_data.csi_clk[0] = clk_get(NULL, "ssi_ext1_clk"); mxc_spdif_data.spdif_core_clk = clk_get(NULL, "spdif_xtal_clk"); clk_put(mxc_spdif_data.spdif_core_clk);&lt;BR /&gt; mxcsdhc3_device.resource[2].start = IOMUX_TO_IRQ_V3(SD3_CD); mxcsdhc3_device.resource[2].end = IOMUX_TO_IRQ_V3(SD3_CD);&lt;BR /&gt; mxc_cpu_common_init(); mx53_loco_io_init();&lt;BR /&gt; mxc_register_device(&amp;amp;mxc_dma_device, NULL); mxc_register_device(&amp;amp;mxc_wdt_device, NULL); mxc_register_device(&amp;amp;mxci2c_devices[0], &amp;amp;mxci2c_data); mxc_register_device(&amp;amp;mxci2c_devices[1], &amp;amp;mxci2c_data); mxc_register_device(&amp;amp;mxci2c_devices[2], &amp;amp;mxci2c_data); //Added by JP&amp;nbsp;&lt;BR /&gt; mx53_loco_init_da9052();&lt;BR /&gt; mxc_register_device(&amp;amp;mxc_rtc_device, NULL); mxc_register_device(&amp;amp;mxc_ipu_device, &amp;amp;mxc_ipu_data); mxc_register_device(&amp;amp;mxc_ldb_device, &amp;amp;ldb_data); mxc_register_device(&amp;amp;mxc_tve_device, &amp;amp;tve_data); mxc_register_device(&amp;amp;mxcvpu_device, &amp;amp;mxc_vpu_data); mxc_register_device(&amp;amp;gpu_device, &amp;amp;z160_revision); mxc_register_device(&amp;amp;mxcscc_device, NULL); mxc_register_device(&amp;amp;mxc_dvfs_core_device, &amp;amp;dvfs_core_data); mxc_register_device(&amp;amp;busfreq_device, &amp;amp;bus_freq_data); mxc_register_device(&amp;amp;mxc_iim_device, &amp;amp;iim_data); mxc_register_device(&amp;amp;mxc_pwm2_device, NULL); mxc_register_device(&amp;amp;mxc_pwm1_backlight_device, &amp;amp;mxc_pwm_backlight_data); mxc_register_device(&amp;amp;mxcsdhc1_device, &amp;amp;mmc1_data); mxc_register_device(&amp;amp;mxcsdhc3_device, &amp;amp;mmc3_data); mxc_register_device(&amp;amp;mxc_ssi1_device, NULL); mxc_register_device(&amp;amp;mxc_ssi2_device, NULL); mxc_register_device(&amp;amp;mxc_alsa_spdif_device, &amp;amp;mxc_spdif_data); mxc_register_device(&amp;amp;ahci_fsl_device, &amp;amp;sata_data); mxc_register_device(&amp;amp;mxc_fec_device, &amp;amp;fec_data); /* ASRC is only available for MX53 TO2.0 */ if (cpu_is_mx53_rev(CHIP_REV_2_0) &amp;gt;= 1) { mxc_asrc_data.asrc_core_clk = clk_get(NULL, "asrc_clk"); clk_put(mxc_asrc_data.asrc_core_clk); mxc_asrc_data.asrc_audio_clk = clk_get(NULL, "asrc_serial_clk"); clk_put(mxc_asrc_data.asrc_audio_clk); mxc_register_device(&amp;amp;mxc_asrc_device, &amp;amp;mxc_asrc_data); }&lt;BR /&gt; i2c_register_board_info(0, mxc_i2c0_board_info, ARRAY_SIZE(mxc_i2c0_board_info)); i2c_register_board_info(1, mxc_i2c1_board_info, ARRAY_SIZE(mxc_i2c1_board_info)); i2c_register_board_info(2, mxc_i2c2_board_info, ARRAY_SIZE(mxc_i2c2_board_info));&lt;BR /&gt; mxc_register_device(&amp;amp;mxc_sgtl5000_device, &amp;amp;sgtl5000_data); mx5_usb_dr_init(); mx5_set_host1_vbus_func(mx53_loco_usbh1_vbus); mx5_usbh1_init(); mxc_register_device(&amp;amp;mxc_v4l2_device, NULL); mxc_register_device(&amp;amp;mxc_v4l2out_device, NULL); loco_add_device_buttons();}&lt;BR /&gt;static void __init mx53_loco_timer_init(void){ struct clk *uart_clk;&lt;BR /&gt; mx53_clocks_init(32768, 24000000, 0, 0);&lt;BR /&gt; uart_clk = clk_get_sys("mxcintuart.0", NULL); early_console_setup(MX53_BASE_ADDR(UART1_BASE_ADDR), uart_clk);}&lt;BR /&gt;static struct sys_timer mxc_timer = { .init = mx53_loco_timer_init,};&lt;BR /&gt;/*&amp;nbsp;* The following uses standard kernel macros define in arch.h in order to&amp;nbsp;* initialize __mach_desc_MX53_LOCO data structure.&amp;nbsp;*/MACHINE_START(MX53_LOCO, "Freescale MX53 LOCO Board") /* Maintainer: Freescale Semiconductor, Inc. */ .fixup = fixup_mxc_board, .map_io = mx5_map_io, .init_irq = mx5_init_irq, .init_machine = mxc_board_init, .timer = &amp;amp;mxc_timer,MACHINE_END&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Nov 2011 17:12:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i2c-access-in-linux/m-p/182336#M7952</guid>
      <dc:creator>JoshuaParrish</dc:creator>
      <dc:date>2011-11-01T17:12:52Z</dc:date>
    </item>
    <item>
      <title>Re: i2c access in linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i2c-access-in-linux/m-p/182337#M7953</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Because I2C2 was tested on QS board, suggest you check whether your OV camera sensor is powered up well.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Nov 2011 02:00:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i2c-access-in-linux/m-p/182337#M7953</guid>
      <dc:creator>LilyZhang</dc:creator>
      <dc:date>2011-11-02T02:00:27Z</dc:date>
    </item>
    <item>
      <title>Re: i2c access in linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i2c-access-in-linux/m-p/182338#M7954</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Done, It is powered correctly.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've also noticed this morning that sound is no longer working. Could packages installed cause sound to no longer work? Sound is also on i2c, but it's on i2c1.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Nov 2011 15:58:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i2c-access-in-linux/m-p/182338#M7954</guid>
      <dc:creator>JoshuaParrish</dc:creator>
      <dc:date>2011-11-02T15:58:38Z</dc:date>
    </item>
    <item>
      <title>Re: i2c access in linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i2c-access-in-linux/m-p/182339#M7955</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Solved,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Even though the pins in the board file are called i2c2 they are really located at i2c-1 in linux. and insantiated in i2c-1 in the board file.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Nov 2011 16:39:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i2c-access-in-linux/m-p/182339#M7955</guid>
      <dc:creator>JoshuaParrish</dc:creator>
      <dc:date>2011-11-03T16:39:18Z</dc:date>
    </item>
  </channel>
</rss>