<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: iMX6 SSI with absolute value encoder in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-SSI-with-absolute-value-encoder/m-p/493723#M79335</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Got output:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;AUDMUX4 TXD is connected to the RS422 transmitter, internal use of AUDMUX1 and therefor SSI1.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;// TXD, RXD and RXC to ALT 3&lt;/P&gt;&lt;P&gt;m_muxAud4TXD.SetAddr( 0x020E0050);&lt;/P&gt;&lt;P&gt;m_muxAud4TXD.SetValue( 3);&amp;nbsp;&amp;nbsp;&amp;nbsp; // ALT3&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;// GPIO1_IO15, SW_PAD_CTL_PAD_SD2_DATA0, ALT 3&lt;/P&gt;&lt;P&gt;m_muxAud4RXD.SetAddr( 0x020E0054);&lt;/P&gt;&lt;P&gt;m_muxAud4RXD.SetValue(3);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;// GPIO1_IO11, IOMUXC_SW_MUX_CTL_PAD_SD2_CMD, ALT3&lt;/P&gt;&lt;P&gt;m_muxAud4RXC.SetAddr( 0x020E0358);&lt;/P&gt;&lt;P&gt;m_muxAud4RXC.SetValue(3);&lt;/P&gt;&lt;P&gt;// configure AUDMUX1&lt;/P&gt;&lt;P&gt;m_audm1_ptcr.SetAddr( 0x021D8000);&lt;/P&gt;&lt;P&gt;m_audm1_pdcr.SetAddr( 0x021D8004);&lt;/P&gt;&lt;P&gt;// AUDMUX1 to AUDMUX4, TCLKDIR out, port 4&lt;/P&gt;&lt;P&gt;m_audm1_ptcr.SetValue( (1&amp;lt;&amp;lt;26) + (3&amp;lt;&amp;lt;22) );&lt;/P&gt;&lt;P&gt;m_audm1_pdcr.SetValue( (3&amp;lt;&amp;lt;13) );&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;// configure AUDMUX4&lt;/P&gt;&lt;P&gt;m_audm4_ptcr.SetAddr( 0x021D8018);&lt;/P&gt;&lt;P&gt;m_audm4_pdcr.SetAddr( 0x021D801C);&lt;/P&gt;&lt;P&gt;// recv clock as output, dest is 0&lt;/P&gt;&lt;P&gt;m_audm4_ptcr.SetValue( (1&amp;lt;&amp;lt;16) + (8&amp;lt;&amp;lt;12));//0000800);&lt;/P&gt;&lt;P&gt;m_audm4_pdcr.SetValue( 0 );&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // port 1 is 000 as mask&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;// Configure SSI1&lt;/P&gt;&lt;P&gt;m_ssi1cr.SetAddr( 0x02028010);&lt;/P&gt;&lt;P&gt;// rec enabled, trans enabled, SSI enable&lt;/P&gt;&lt;P&gt;m_ssi1cr.SetValue(&amp;nbsp;&amp;nbsp; (1&amp;lt;&amp;lt;2) + (1&amp;lt;&amp;lt;1) + (1&amp;lt;&amp;lt;0) );&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;m_ssi1stx0.SetAddr( 0x02028000);&lt;/P&gt;&lt;P&gt;m_ssi1srx0.SetAddr( 0x02028008);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;m_ssi1stcr.SetAddr( 0x0202801C);&lt;/P&gt;&lt;P&gt;// internal clock, clock divided by 256&lt;/P&gt;&lt;P&gt;m_ssi1stcr.SetValue( (1&amp;lt;&amp;lt;7) + (1&amp;lt;&amp;lt;5) + 0xFF );&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;m_ssi1stccr.SetAddr( 0x02028024);&lt;/P&gt;&lt;P&gt;// not more then 24bit, divider and prescaler&lt;/P&gt;&lt;P&gt;m_ssi1stccr.SetValue( (1&amp;lt;&amp;lt;18) + (1&amp;lt;&amp;lt;17) + (11&amp;lt;&amp;lt;13) );&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;// receive&lt;/P&gt;&lt;P&gt;m_ssi1srcr.SetAddr( 0x02028020);&lt;/P&gt;&lt;P&gt;m_ssi1srccr.SetAddr( 0x02028028);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;m_ssi1srcr.SetValue( (1&amp;lt;&amp;lt;7) );&lt;/P&gt;&lt;P&gt;m_ssi1srccr.SetValue( (7&amp;lt;&amp;lt;13) );&lt;/P&gt;&lt;P&gt;// FIFO control&lt;/P&gt;&lt;P&gt;m_ssi1sfcsr.SetAddr( 0x0202802C);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Writing a bit mask to m_ssi1stx0 is sent out to the PIN.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 02 Jun 2016 14:37:28 GMT</pubDate>
    <dc:creator>dirkschäfer</dc:creator>
    <dc:date>2016-06-02T14:37:28Z</dc:date>
    <item>
      <title>iMX6 SSI with absolute value encoder</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-SSI-with-absolute-value-encoder/m-p/493718#M79330</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;on an ATMEL G45 I use the SSI interface with an absolute value encoder. TXD is hardwired with RXC. I send 0xAAAAAAAA followed by 0xFFFFFFFF forever. The clock send out by TXD is given over RS422 to the absolute value encoder and TXC. TXD is 32bit, RXD is 16bit. So after sending 32bits 0xAAAAAAAA, there are 16bits in RXD, clocked by RXC. I than read the absolute position of the encoder.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now I want this with the iMX6. But I am lost. The clock is controlled by the CCM. But which register to set the data to send?&lt;/P&gt;&lt;P&gt;And from which register reading the data coming in?&lt;/P&gt;&lt;P&gt;Chapter 16, AUDMUX, just explains timing and data control registers. I wired AUD4_TXD to RS422 and AUD4RXC. And AUD4RXD to a RS422-reciever. The enocder returns gray-code and just needs a clock, generated from TXD.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;No OS used. To start, I would like to know how to set the data to send over TXD.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many thanks for your help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 May 2016 12:02:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-SSI-with-absolute-value-encoder/m-p/493718#M79330</guid>
      <dc:creator>dirkschäfer</dc:creator>
      <dc:date>2016-05-02T12:02:15Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 SSI with absolute value encoder</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-SSI-with-absolute-value-encoder/m-p/493719#M79331</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I overlooked Chapter 61, excuse this please.&lt;/P&gt;&lt;P&gt;How to connect AUD4_TXD to SSI1, for example?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 May 2016 12:25:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-SSI-with-absolute-value-encoder/m-p/493719#M79331</guid>
      <dc:creator>dirkschäfer</dc:creator>
      <dc:date>2016-05-02T12:25:54Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 SSI with absolute value encoder</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-SSI-with-absolute-value-encoder/m-p/493720#M79332</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Dirk&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can look at attached example from sdk, also please&lt;/P&gt;&lt;P&gt;Chapter 5, Chapter 32 Configuring the SSI Driver iMX6_Firmware_Guide.pdf.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 May 2016 00:37:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-SSI-with-absolute-value-encoder/m-p/493720#M79332</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-05-03T00:37:16Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 SSI with absolute value encoder</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-SSI-with-absolute-value-encoder/m-p/493721#M79333</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;// PINs&lt;/P&gt;&lt;P&gt;m_muxAud4TXD.SetAddr( 0x020E0050);&lt;/P&gt;&lt;P&gt;m_muxAud4TXD.SetValue( 3);&amp;nbsp;&amp;nbsp;&amp;nbsp; // ALT3&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;// configure AUDMUX 4&lt;/P&gt;&lt;P&gt;m_portTiming.SetAddr( 0x021D8018);&lt;/P&gt;&lt;P&gt;m_dataCtrl.SetAddr( 0x021D801C);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;// TXC as output, TXC as output, RXC from port&lt;/P&gt;&lt;P&gt;m_portTiming.SetValue( (1&amp;lt;&amp;lt;26) + (1&amp;lt;&amp;lt;16) + (8&amp;lt;&amp;lt;12) );&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;// connected to SSI1&lt;/P&gt;&lt;P&gt;m_dataCtrl.SetValue(0);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;// configure SSI&lt;/P&gt;&lt;P&gt;m_stx0.SetAddr( 0x02028000);&lt;/P&gt;&lt;P&gt;m_srx0.SetAddr( 0x02028008);&lt;/P&gt;&lt;P&gt;m_ctrl.SetAddr( 0x02028010);&lt;/P&gt;&lt;P&gt;m_txconf.SetAddr( 0x0202801C);&lt;/P&gt;&lt;P&gt;m_rxconf.SetAddr( 0x02028020);&lt;/P&gt;&lt;P&gt;m_txclock.SetAddr( 0x02028024);&lt;/P&gt;&lt;P&gt;m_rxclock.SetAddr( 0x02028028);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;// recv enable, tx enable, ssi enable&lt;/P&gt;&lt;P&gt;m_ctrl.SetValue( (1&amp;lt;&amp;lt;2) + (1&amp;lt;&amp;lt;1) + (1&amp;lt;&amp;lt;0) );&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;// lsb_aligned, internal clock&lt;/P&gt;&lt;P&gt;m_txconf.SetValue( (1&amp;lt;&amp;lt;9) + (1&amp;lt;&amp;lt;5) );&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;// lsb_aligned, external clock&lt;/P&gt;&lt;P&gt;m_rxconf.SetValue( (1&amp;lt;&amp;lt;9) );&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;// 32bit&lt;/P&gt;&lt;P&gt;m_txclock.SetValue( (1&amp;lt;&amp;lt;18) + (1&amp;lt;&amp;lt;17) + (15&amp;lt;&amp;lt;13) );&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;// 16bit, no divider or prescaler&lt;/P&gt;&lt;P&gt;m_rxclock.SetValue( (7&amp;lt;&amp;lt;13) );&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Every second writing 0xAAAAAAAA to m_stx0. Clocks for SSI1 are enabled in ccgr5.&lt;/P&gt;&lt;P&gt;No output. SSI1 and AUDMUX4 should be muxed.&lt;/P&gt;&lt;P&gt;Is it right to set AUDMUX4 to port 1, meaning SSI1?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 May 2016 11:51:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-SSI-with-absolute-value-encoder/m-p/493721#M79333</guid>
      <dc:creator>dirkschäfer</dc:creator>
      <dc:date>2016-05-03T11:51:07Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 SSI with absolute value encoder</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-SSI-with-absolute-value-encoder/m-p/493722#M79334</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Tried the following:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I used AUDMUX1, and connect it to port4. And SSI1, because it seems to be connected to AUDMUX1.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;m_portTiming.SetAddr( 0x021D8000);//0x021D8018);&lt;/P&gt;&lt;P&gt;m_dataCtrl.SetAddr( 0x021D8004);//0x021D801C);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;// RC from RXC pin AUD4, 1011&lt;/P&gt;&lt;P&gt;m_portTiming.SetValue( /*(1&amp;lt;&amp;lt;26) + (3&amp;lt;&amp;lt;22) +/*(1&amp;lt;&amp;lt;16) +*/ (11&amp;lt;&amp;lt;12) );&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;// connected to SSI1&lt;/P&gt;&lt;P&gt;// no, to AUD4&lt;/P&gt;&lt;P&gt;m_dataCtrl.SetValue( 3&amp;lt;&amp;lt;13);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;No output on AUDMUX4_TXD. With bitbanging the absolute value encoder works fine.&lt;/P&gt;&lt;P&gt;Where am I wrong?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 May 2016 14:32:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-SSI-with-absolute-value-encoder/m-p/493722#M79334</guid>
      <dc:creator>dirkschäfer</dc:creator>
      <dc:date>2016-05-04T14:32:21Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 SSI with absolute value encoder</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-SSI-with-absolute-value-encoder/m-p/493723#M79335</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Got output:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;AUDMUX4 TXD is connected to the RS422 transmitter, internal use of AUDMUX1 and therefor SSI1.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;// TXD, RXD and RXC to ALT 3&lt;/P&gt;&lt;P&gt;m_muxAud4TXD.SetAddr( 0x020E0050);&lt;/P&gt;&lt;P&gt;m_muxAud4TXD.SetValue( 3);&amp;nbsp;&amp;nbsp;&amp;nbsp; // ALT3&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;// GPIO1_IO15, SW_PAD_CTL_PAD_SD2_DATA0, ALT 3&lt;/P&gt;&lt;P&gt;m_muxAud4RXD.SetAddr( 0x020E0054);&lt;/P&gt;&lt;P&gt;m_muxAud4RXD.SetValue(3);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;// GPIO1_IO11, IOMUXC_SW_MUX_CTL_PAD_SD2_CMD, ALT3&lt;/P&gt;&lt;P&gt;m_muxAud4RXC.SetAddr( 0x020E0358);&lt;/P&gt;&lt;P&gt;m_muxAud4RXC.SetValue(3);&lt;/P&gt;&lt;P&gt;// configure AUDMUX1&lt;/P&gt;&lt;P&gt;m_audm1_ptcr.SetAddr( 0x021D8000);&lt;/P&gt;&lt;P&gt;m_audm1_pdcr.SetAddr( 0x021D8004);&lt;/P&gt;&lt;P&gt;// AUDMUX1 to AUDMUX4, TCLKDIR out, port 4&lt;/P&gt;&lt;P&gt;m_audm1_ptcr.SetValue( (1&amp;lt;&amp;lt;26) + (3&amp;lt;&amp;lt;22) );&lt;/P&gt;&lt;P&gt;m_audm1_pdcr.SetValue( (3&amp;lt;&amp;lt;13) );&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;// configure AUDMUX4&lt;/P&gt;&lt;P&gt;m_audm4_ptcr.SetAddr( 0x021D8018);&lt;/P&gt;&lt;P&gt;m_audm4_pdcr.SetAddr( 0x021D801C);&lt;/P&gt;&lt;P&gt;// recv clock as output, dest is 0&lt;/P&gt;&lt;P&gt;m_audm4_ptcr.SetValue( (1&amp;lt;&amp;lt;16) + (8&amp;lt;&amp;lt;12));//0000800);&lt;/P&gt;&lt;P&gt;m_audm4_pdcr.SetValue( 0 );&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // port 1 is 000 as mask&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;// Configure SSI1&lt;/P&gt;&lt;P&gt;m_ssi1cr.SetAddr( 0x02028010);&lt;/P&gt;&lt;P&gt;// rec enabled, trans enabled, SSI enable&lt;/P&gt;&lt;P&gt;m_ssi1cr.SetValue(&amp;nbsp;&amp;nbsp; (1&amp;lt;&amp;lt;2) + (1&amp;lt;&amp;lt;1) + (1&amp;lt;&amp;lt;0) );&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;m_ssi1stx0.SetAddr( 0x02028000);&lt;/P&gt;&lt;P&gt;m_ssi1srx0.SetAddr( 0x02028008);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;m_ssi1stcr.SetAddr( 0x0202801C);&lt;/P&gt;&lt;P&gt;// internal clock, clock divided by 256&lt;/P&gt;&lt;P&gt;m_ssi1stcr.SetValue( (1&amp;lt;&amp;lt;7) + (1&amp;lt;&amp;lt;5) + 0xFF );&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;m_ssi1stccr.SetAddr( 0x02028024);&lt;/P&gt;&lt;P&gt;// not more then 24bit, divider and prescaler&lt;/P&gt;&lt;P&gt;m_ssi1stccr.SetValue( (1&amp;lt;&amp;lt;18) + (1&amp;lt;&amp;lt;17) + (11&amp;lt;&amp;lt;13) );&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;// receive&lt;/P&gt;&lt;P&gt;m_ssi1srcr.SetAddr( 0x02028020);&lt;/P&gt;&lt;P&gt;m_ssi1srccr.SetAddr( 0x02028028);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;m_ssi1srcr.SetValue( (1&amp;lt;&amp;lt;7) );&lt;/P&gt;&lt;P&gt;m_ssi1srccr.SetValue( (7&amp;lt;&amp;lt;13) );&lt;/P&gt;&lt;P&gt;// FIFO control&lt;/P&gt;&lt;P&gt;m_ssi1sfcsr.SetAddr( 0x0202802C);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Writing a bit mask to m_ssi1stx0 is sent out to the PIN.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Jun 2016 14:37:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-SSI-with-absolute-value-encoder/m-p/493723#M79335</guid>
      <dc:creator>dirkschäfer</dc:creator>
      <dc:date>2016-06-02T14:37:28Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 SSI with absolute value encoder</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-SSI-with-absolute-value-encoder/m-p/493724#M79336</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;No Input:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The TXC is connected to the TXD, so the recieve-clock should be done by the bitmask sent out to TXD.&lt;/P&gt;&lt;P&gt;AUDMUX4 must be aware of TXC.&lt;/P&gt;&lt;P&gt;Is it enough to configure&lt;/P&gt;&lt;P&gt;// recv clock as output, dest is 0&lt;/P&gt;&lt;P&gt;m_audm4_ptcr.SetValue( (1&amp;lt;&amp;lt;16) + (8&amp;lt;&amp;lt;12));&lt;/P&gt;&lt;P&gt;// to port 1&lt;/P&gt;&lt;P&gt;m_audm4_pdcr.SetValue( 0 );&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;AND&lt;/P&gt;&lt;P&gt;// recieve control, FIFO 0 enable, falling edge, external clock (1&amp;lt;&amp;lt;5) ?&lt;/P&gt;&lt;P&gt;m_ssi1srcr.SetValue( (1&amp;lt;&amp;lt;7) );&lt;/P&gt;&lt;P&gt;// no divider, TXD does clocking, 16bit,&lt;/P&gt;&lt;P&gt;m_ssi1srccr.SetValue( (7&amp;lt;&amp;lt;13) );&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;FIFO control never shows data in RECV.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Jun 2016 14:44:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-SSI-with-absolute-value-encoder/m-p/493724#M79336</guid>
      <dc:creator>dirkschäfer</dc:creator>
      <dc:date>2016-06-02T14:44:23Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 SSI with absolute value encoder</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-SSI-with-absolute-value-encoder/m-p/493725#M79337</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I still have a problem to get the RXC over the PIN. If I configure AUDMUX4_RXC as outport, source to port 4, sending data stopps.&lt;/P&gt;&lt;P&gt;Why touching RXC influence sending data?&lt;/P&gt;&lt;P&gt;The TXD is connected to RXD, because I want to generate the clock for the absolute value encoder by the bitmaks transmitted. The falling edges than should be the clock for recieving.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many thanks for your help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Jun 2016 08:22:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-SSI-with-absolute-value-encoder/m-p/493725#M79337</guid>
      <dc:creator>dirkschäfer</dc:creator>
      <dc:date>2016-06-03T08:22:32Z</dc:date>
    </item>
  </channel>
</rss>