<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックIMX6UL UART or USB serial downloader</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6UL-UART-or-USB-serial-downloader/m-p/493116#M79215</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We got a custom board based on a IMX6UL, which is not detected as an HID.&lt;/P&gt;&lt;P&gt;Is there anyway to know if the serial downloader is going through UART or USB?&lt;/P&gt;&lt;P&gt;Maybe any register or something?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and best regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 05 Feb 2016 12:55:09 GMT</pubDate>
    <dc:creator>alubeiro</dc:creator>
    <dc:date>2016-02-05T12:55:09Z</dc:date>
    <item>
      <title>IMX6UL UART or USB serial downloader</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6UL-UART-or-USB-serial-downloader/m-p/493116#M79215</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We got a custom board based on a IMX6UL, which is not detected as an HID.&lt;/P&gt;&lt;P&gt;Is there anyway to know if the serial downloader is going through UART or USB?&lt;/P&gt;&lt;P&gt;Maybe any register or something?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and best regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Feb 2016 12:55:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6UL-UART-or-USB-serial-downloader/m-p/493116#M79215</guid>
      <dc:creator>alubeiro</dc:creator>
      <dc:date>2016-02-05T12:55:09Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6UL UART or USB serial downloader</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6UL-UART-or-USB-serial-downloader/m-p/493117#M79216</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; In serial downloader mode i.MX6UL boot ROM&amp;nbsp; checks activity on USB OTG1 and UART 1/2.&lt;/P&gt;&lt;P&gt;According to section 8.9.2 (UART) of the i.MX6UL RM : "The noise on UART RX data pad may &lt;BR /&gt;cause a “data ready” event reported by UART controller, and further cause ROM entering UART &lt;BR /&gt;serial download mode."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; I am afraid we do not have explicit external indicator to define if boot ROM is in serial downloader&lt;/P&gt;&lt;P&gt;mode, and what channel is used : USB or UART, except having proper activities of USB or UART.&lt;/P&gt;&lt;P&gt;Also JTAG debugging may be used to define what device USB or UART is active now.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; The fact of non-working USB boot mode (when properly configured BOOT_MODE[1:0] ) may mean,&lt;/P&gt;&lt;P&gt;the system does not start. Please check design using "Hardware Development Guide for the&lt;/P&gt;&lt;P&gt;i.MX 6UltraLite Applications Processor".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf" title="http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf"&gt;http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Feb 2016 06:03:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6UL-UART-or-USB-serial-downloader/m-p/493117#M79216</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-02-08T06:03:40Z</dc:date>
    </item>
  </channel>
</rss>