<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 malloc used executable binary unable to run in imx6 linux</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/malloc-used-executable-binary-unable-to-run-in-imx6-linux/m-p/492851#M79182</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;i written a simple &lt;STRONG&gt;malloc&lt;/STRONG&gt; c program and cross compiled into arm, then i run in arm bsp it shows &lt;STRONG&gt;segmentation fault. &lt;/STRONG&gt;Then i compiled that program as statically, then it's successfully run. But this is testing purpose i did.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have an big source file, in that source have &lt;STRONG&gt;malloc, &lt;/STRONG&gt; also i'm not able to compile as statically. So in dynamically linked file how can i use..?&lt;/P&gt;&lt;P&gt;i cross checked with shared libraries(libc.so.6 is there). Everything is there.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you help me to fix this issue.?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Aravinth&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 09 Apr 2016 12:43:58 GMT</pubDate>
    <dc:creator>aravinthkumarja</dc:creator>
    <dc:date>2016-04-09T12:43:58Z</dc:date>
    <item>
      <title>malloc used executable binary unable to run in imx6 linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/malloc-used-executable-binary-unable-to-run-in-imx6-linux/m-p/492851#M79182</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;i written a simple &lt;STRONG&gt;malloc&lt;/STRONG&gt; c program and cross compiled into arm, then i run in arm bsp it shows &lt;STRONG&gt;segmentation fault. &lt;/STRONG&gt;Then i compiled that program as statically, then it's successfully run. But this is testing purpose i did.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have an big source file, in that source have &lt;STRONG&gt;malloc, &lt;/STRONG&gt; also i'm not able to compile as statically. So in dynamically linked file how can i use..?&lt;/P&gt;&lt;P&gt;i cross checked with shared libraries(libc.so.6 is there). Everything is there.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you help me to fix this issue.?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Aravinth&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 09 Apr 2016 12:43:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/malloc-used-executable-binary-unable-to-run-in-imx6-linux/m-p/492851#M79182</guid>
      <dc:creator>aravinthkumarja</dc:creator>
      <dc:date>2016-04-09T12:43:58Z</dc:date>
    </item>
    <item>
      <title>Re: malloc used executable binary unable to run in imx6 linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/malloc-used-executable-binary-unable-to-run-in-imx6-linux/m-p/492852#M79183</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; I hope the following helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://danluu.com/malloc-tutorial/" title="http://danluu.com/malloc-tutorial/"&gt;A quick tutorial on implementing and debugging malloc, free, calloc, and realloc&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://stackoverflow.com/questions/3479330/how-is-malloc-implemented-internally" title="http://stackoverflow.com/questions/3479330/how-is-malloc-implemented-internally"&gt;http://stackoverflow.com/questions/3479330/how-is-malloc-implemented-internally&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Apr 2016 06:04:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/malloc-used-executable-binary-unable-to-run-in-imx6-linux/m-p/492852#M79183</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-04-11T06:04:06Z</dc:date>
    </item>
  </channel>
</rss>