<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックI.mx6 PCIe clock setting</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/I-mx6-PCIe-clock-setting/m-p/492437#M79087</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello..,&lt;/P&gt;&lt;P&gt;I am using I.mx6 processor, In that I need to configure the PCIe&lt;/P&gt;&lt;P&gt;1.Please can anyone give me clear steps and which register I need to use to enable clock for PCIe.&lt;/P&gt;&lt;P&gt;2.PLL6 is used to generate clock for the PCIe. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 02 May 2016 06:38:57 GMT</pubDate>
    <dc:creator>karthikas</dc:creator>
    <dc:date>2016-05-02T06:38:57Z</dc:date>
    <item>
      <title>I.mx6 PCIe clock setting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-mx6-PCIe-clock-setting/m-p/492437#M79087</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello..,&lt;/P&gt;&lt;P&gt;I am using I.mx6 processor, In that I need to configure the PCIe&lt;/P&gt;&lt;P&gt;1.Please can anyone give me clear steps and which register I need to use to enable clock for PCIe.&lt;/P&gt;&lt;P&gt;2.PLL6 is used to generate clock for the PCIe. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 May 2016 06:38:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-mx6-PCIe-clock-setting/m-p/492437#M79087</guid>
      <dc:creator>karthikas</dc:creator>
      <dc:date>2016-05-02T06:38:57Z</dc:date>
    </item>
    <item>
      <title>Re: I.mx6 PCIe clock setting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-mx6-PCIe-clock-setting/m-p/492438#M79088</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi KARTHIK&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;most full explanation of PCIe settings is provided on&amp;nbsp; i.MX6Q PCIe EP/RC Validation System&lt;/P&gt;&lt;P&gt;page :&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-wiki-small" data-containerid="2004" data-containertype="14" data-objectid="95014" data-objecttype="102" href="https://community.freescale.com/docs/DOC-95014"&gt;https://community.freescale.com/docs/DOC-95014&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 May 2016 12:32:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-mx6-PCIe-clock-setting/m-p/492438#M79088</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-05-02T12:32:22Z</dc:date>
    </item>
  </channel>
</rss>