<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 iMX6Q camera gstream error</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-camera-gstream-error/m-p/491975#M78974</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;when i try to use gsteram im getting these errors::&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(camera:236): GStreamer-CRITICAL **: gst_value_list_get_value: assertion 'index &amp;lt; VALUE_LIST_SIZE (value)' failed&lt;/P&gt;&lt;P&gt;(camera:236): GStreamer-CRITICAL **: gst_value_init_and_copy: assertion 'G_IS_VALUE (src)' failed&lt;/P&gt;&lt;P&gt;(camera:236): GStreamer-CRITICAL **: gst_structure_id_take_value: assertion 'G_IS_VALUE (value)' failed &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;they are printed endlessly on the screen and i cant get any images nor with any other application. (like cat..)&lt;/P&gt;&lt;P&gt;any help appreciated, thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 14 Jan 2016 16:06:17 GMT</pubDate>
    <dc:creator>shlomiperlman</dc:creator>
    <dc:date>2016-01-14T16:06:17Z</dc:date>
    <item>
      <title>iMX6Q camera gstream error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-camera-gstream-error/m-p/491975#M78974</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;when i try to use gsteram im getting these errors::&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(camera:236): GStreamer-CRITICAL **: gst_value_list_get_value: assertion 'index &amp;lt; VALUE_LIST_SIZE (value)' failed&lt;/P&gt;&lt;P&gt;(camera:236): GStreamer-CRITICAL **: gst_value_init_and_copy: assertion 'G_IS_VALUE (src)' failed&lt;/P&gt;&lt;P&gt;(camera:236): GStreamer-CRITICAL **: gst_structure_id_take_value: assertion 'G_IS_VALUE (value)' failed &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;they are printed endlessly on the screen and i cant get any images nor with any other application. (like cat..)&lt;/P&gt;&lt;P&gt;any help appreciated, thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Jan 2016 16:06:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-camera-gstream-error/m-p/491975#M78974</guid>
      <dc:creator>shlomiperlman</dc:creator>
      <dc:date>2016-01-14T16:06:17Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6Q camera gstream error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-camera-gstream-error/m-p/491976#M78975</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi shlomi,&lt;/P&gt;&lt;P&gt;I don't suppose anyone can answer your question without providing more detailed information. Mainly:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Camera type&lt;/LI&gt;&lt;LI&gt;Used application (gst-launch or anything else?)&lt;/LI&gt;&lt;LI&gt;GStreamer pipeline&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Generally I'd guess your pipeline is invalid. If using a USB camera, did you try to launch it on PC?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Jan 2016 16:39:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-camera-gstream-error/m-p/491976#M78975</guid>
      <dc:creator>kubiznak_petr</dc:creator>
      <dc:date>2016-01-14T16:39:49Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6Q camera gstream error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-camera-gstream-error/m-p/491977#M78976</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;its a camera sensor gc0309 galaxy on ipu0/csi0 and its recognized and attached as the driver loads ok (or so it seems..)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i used gst-launch-1.0 and another camera app that worked with a usb webcam for testing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;when doing cat on dev/video0 i can see raw data running on the screen.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Jan 2016 17:23:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-camera-gstream-error/m-p/491977#M78976</guid>
      <dc:creator>shlomiperlman</dc:creator>
      <dc:date>2016-01-14T17:23:26Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6Q camera gstream error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-camera-gstream-error/m-p/491978#M78977</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi shlomi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can check what sensor format is used: default BSP supports&lt;/P&gt;&lt;P&gt;only YUYV (ov5642 sensor). So for rgb565 one can look at&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-97981"&gt;How to Support RGB565 Gated Mode Input to i.MX6 CSI&lt;/A&gt;&lt;/P&gt;&lt;P&gt;First recommended to try unit tests, refer to attached Linux Manual&lt;/P&gt;&lt;P&gt;sect.5.5.2 Video4Linux API test, Porting Guide Chapter 7 Supporting the&lt;/P&gt;&lt;P&gt;i.MX 6 Camera Sensor Interface CSI0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Jan 2016 01:02:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-camera-gstream-error/m-p/491978#M78977</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-01-18T01:02:38Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6Q camera gstream error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-camera-gstream-error/m-p/491979#M78978</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;my sensor's default (and current) mode is YUYV but when i set&lt;/P&gt;&lt;P&gt;sensor-&amp;gt;pix.pixelformat = V4L2_PIX_FMT_YUYV;&lt;/P&gt;&lt;P&gt;in the driver i get nothing from it, only when&lt;/P&gt;&lt;P&gt;sensor-&amp;gt;pix.pixelformat = V4L2_PIX_FMT_RGB565;&lt;/P&gt;&lt;P&gt;is set, i'm getting the video stream..&lt;/P&gt;&lt;P&gt;any idea?&lt;/P&gt;&lt;P&gt;thanks,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Jan 2016 10:10:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-camera-gstream-error/m-p/491979#M78978</guid>
      <dc:creator>shlomiperlman</dc:creator>
      <dc:date>2016-01-18T10:10:28Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6Q camera gstream error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-camera-gstream-error/m-p/491980#M78979</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;one can check how many cycles per pixel outputs sensor&lt;/P&gt;&lt;P&gt;and compare with&amp;nbsp; Table 66 Camera Input Signal Cross Reference, Format, and Bits Per Cycle&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf" title="http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf"&gt;http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Jan 2016 10:30:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-camera-gstream-error/m-p/491980#M78979</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-01-18T10:30:42Z</dc:date>
    </item>
  </channel>
</rss>