<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic imx6ulevk bitbake issue in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx6ulevk-bitbake-issue/m-p/491963#M78970</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Sir&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I'd like to bitbake imx6ulevk fsl-image-qt5 on ubuntu 15.10 meet an mistake ,hoping you can help.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; before this ,i had finished made core-image-minimal every thing work well.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; after typing bitbake fsl-image-qt5 , meet below error when task run to 936 , please find below log:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ERROR: oe_runmake failed&lt;/P&gt;&lt;P&gt;ERROR: Function failed: do_install (log file is located at /home/andy/freescale/IMX6UL/fsl-release-bsp/buildqt5/tmp/work/x86_64-linux/qemu-native/2.4.0-r1/temp/log.do_install.2499)&lt;/P&gt;&lt;P&gt;ERROR: Logfile of failure stored in: /home/andy/freescale/IMX6UL/fsl-release-bsp/buildqt5/tmp/work/x86_64-linux/qemu-native/2.4.0-r1/temp/log.do_install.2499&lt;/P&gt;&lt;P&gt;Log data follows:&lt;/P&gt;&lt;P&gt;| DEBUG: Executing shell function do_install&lt;/P&gt;&lt;P&gt;| NOTE: make -j 8 DESTDIR=/home/andy/freescale/IMX6UL/fsl-release-bsp/buildqt5/tmp/work/x86_64-linux/qemu-native/2.4.0-r1/image install&lt;/P&gt;&lt;P&gt;| make: *** No rule to make target 'install'.&amp;nbsp; Stop.&lt;/P&gt;&lt;P&gt;| ERROR: oe_runmake failed&lt;/P&gt;&lt;P&gt;| WARNING: exit code 1 from a shell command.&lt;/P&gt;&lt;P&gt;| ERROR: Function failed: do_install (log file is located at /home/andy/freescale/IMX6UL/fsl-release-bsp/buildqt5/tmp/work/x86_64-linux/qemu-native/2.4.0-r1/temp/log.do_install.2499)&lt;/P&gt;&lt;P&gt;ERROR: Task 936 (virtual:native:/home/andy/freescale/IMX6UL/fsl-release-bsp/sources/poky/meta/recipes-devtools/qemu/qemu_2.4.0.bb, do_install) failed with exit code '1'&lt;/P&gt;&lt;P&gt;NOTE: Tasks Summary: Attempted 2680 tasks of which 2640 didn't need to be rerun and 1 failed.&lt;/P&gt;&lt;P&gt;Waiting for 0 running tasks to finish:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Summary: 1 task failed:&lt;/P&gt;&lt;P&gt;&amp;nbsp; virtual:native:/home/andy/freescale/IMX6UL/fsl-release-bsp/sources/poky/meta/recipes-devtools/qemu/qemu_2.4.0.bb, do_install&lt;/P&gt;&lt;P&gt;Summary: There was 1 WARNING message shown.&lt;/P&gt;&lt;P&gt;Summary: There were 2 ERROR messages shown, returning a non-zero exit code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;then i try to find out what happen ,and find log.do_install.2499, the inforamtion as below:&lt;/P&gt;&lt;P&gt;DEBUG: Executing shell function do_install&lt;/P&gt;&lt;P&gt;NOTE: make -j 8 DESTDIR=/home/andy/freescale/IMX6UL/fsl-release-bsp/buildqt5/tmp/work/x86_64-linux/qemu-native/2.4.0-r1/image install&lt;/P&gt;&lt;P&gt;make: *** No rule to make target 'install'.&amp;nbsp; Stop.&lt;/P&gt;&lt;P&gt;ERROR: oe_runmake failed&lt;/P&gt;&lt;P&gt;WARNING: exit code 1 from a shell command.&lt;/P&gt;&lt;P&gt;ERROR: Function failed: do_install (log file is located at /home/andy/freescale/IMX6UL/fsl-release-bsp/buildqt5/tmp/work/x86_64-linux/qemu-native/2.4.0-r1/temp/log.do_install.2499)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the local.conf set as below:&lt;/P&gt;&lt;P&gt;MACHINE ??= 'imx6ulevk'&lt;/P&gt;&lt;P&gt;DISTRO ?= 'fsl-imx-x11'&lt;/P&gt;&lt;P&gt;PACKAGE_CLASSES ?= "package_rpm"&lt;/P&gt;&lt;P&gt;EXTRA_IMAGE_FEATURES = "debug-tweaks"&lt;/P&gt;&lt;P&gt;USER_CLASSES ?= "buildstats image-mklibs"&lt;/P&gt;&lt;P&gt;PATCHRESOLVE = "noop"&lt;/P&gt;&lt;P&gt;BB_DISKMON_DIRS = "\&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; STOPTASKS,${TMPDIR},1G,100K \&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; STOPTASKS,${DL_DIR},1G,100K \&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; STOPTASKS,${SSTATE_DIR},1G,100K \&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; STOPTASKS,/tmp,100M,100K \&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ABORT,${TMPDIR},100M,1K \&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ABORT,${DL_DIR},100M,1K \&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ABORT,${SSTATE_DIR},100M,1K \&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ABORT,/tmp,10M,1K"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PACKAGECONFIG_append_pn-qemu-native = " sdl"&lt;/P&gt;&lt;P&gt;PACKAGECONFIG_append_pn-nativesdk-qemu = " sdl"&lt;/P&gt;&lt;P&gt;ASSUME_PROVIDED += "libsdl-native"&lt;/P&gt;&lt;P&gt;CONF_VERSION = "1"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;DL_DIR ?= "${BSPDIR}/downloads/"&lt;/P&gt;&lt;P&gt;ACCEPT_FSL_EULA = "1"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Coule you help me to fix this issue??&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Many thanks for your help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 23 May 2016 10:06:46 GMT</pubDate>
    <dc:creator>andyyang730</dc:creator>
    <dc:date>2016-05-23T10:06:46Z</dc:date>
    <item>
      <title>imx6ulevk bitbake issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6ulevk-bitbake-issue/m-p/491963#M78970</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Sir&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I'd like to bitbake imx6ulevk fsl-image-qt5 on ubuntu 15.10 meet an mistake ,hoping you can help.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; before this ,i had finished made core-image-minimal every thing work well.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; after typing bitbake fsl-image-qt5 , meet below error when task run to 936 , please find below log:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ERROR: oe_runmake failed&lt;/P&gt;&lt;P&gt;ERROR: Function failed: do_install (log file is located at /home/andy/freescale/IMX6UL/fsl-release-bsp/buildqt5/tmp/work/x86_64-linux/qemu-native/2.4.0-r1/temp/log.do_install.2499)&lt;/P&gt;&lt;P&gt;ERROR: Logfile of failure stored in: /home/andy/freescale/IMX6UL/fsl-release-bsp/buildqt5/tmp/work/x86_64-linux/qemu-native/2.4.0-r1/temp/log.do_install.2499&lt;/P&gt;&lt;P&gt;Log data follows:&lt;/P&gt;&lt;P&gt;| DEBUG: Executing shell function do_install&lt;/P&gt;&lt;P&gt;| NOTE: make -j 8 DESTDIR=/home/andy/freescale/IMX6UL/fsl-release-bsp/buildqt5/tmp/work/x86_64-linux/qemu-native/2.4.0-r1/image install&lt;/P&gt;&lt;P&gt;| make: *** No rule to make target 'install'.&amp;nbsp; Stop.&lt;/P&gt;&lt;P&gt;| ERROR: oe_runmake failed&lt;/P&gt;&lt;P&gt;| WARNING: exit code 1 from a shell command.&lt;/P&gt;&lt;P&gt;| ERROR: Function failed: do_install (log file is located at /home/andy/freescale/IMX6UL/fsl-release-bsp/buildqt5/tmp/work/x86_64-linux/qemu-native/2.4.0-r1/temp/log.do_install.2499)&lt;/P&gt;&lt;P&gt;ERROR: Task 936 (virtual:native:/home/andy/freescale/IMX6UL/fsl-release-bsp/sources/poky/meta/recipes-devtools/qemu/qemu_2.4.0.bb, do_install) failed with exit code '1'&lt;/P&gt;&lt;P&gt;NOTE: Tasks Summary: Attempted 2680 tasks of which 2640 didn't need to be rerun and 1 failed.&lt;/P&gt;&lt;P&gt;Waiting for 0 running tasks to finish:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Summary: 1 task failed:&lt;/P&gt;&lt;P&gt;&amp;nbsp; virtual:native:/home/andy/freescale/IMX6UL/fsl-release-bsp/sources/poky/meta/recipes-devtools/qemu/qemu_2.4.0.bb, do_install&lt;/P&gt;&lt;P&gt;Summary: There was 1 WARNING message shown.&lt;/P&gt;&lt;P&gt;Summary: There were 2 ERROR messages shown, returning a non-zero exit code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;then i try to find out what happen ,and find log.do_install.2499, the inforamtion as below:&lt;/P&gt;&lt;P&gt;DEBUG: Executing shell function do_install&lt;/P&gt;&lt;P&gt;NOTE: make -j 8 DESTDIR=/home/andy/freescale/IMX6UL/fsl-release-bsp/buildqt5/tmp/work/x86_64-linux/qemu-native/2.4.0-r1/image install&lt;/P&gt;&lt;P&gt;make: *** No rule to make target 'install'.&amp;nbsp; Stop.&lt;/P&gt;&lt;P&gt;ERROR: oe_runmake failed&lt;/P&gt;&lt;P&gt;WARNING: exit code 1 from a shell command.&lt;/P&gt;&lt;P&gt;ERROR: Function failed: do_install (log file is located at /home/andy/freescale/IMX6UL/fsl-release-bsp/buildqt5/tmp/work/x86_64-linux/qemu-native/2.4.0-r1/temp/log.do_install.2499)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the local.conf set as below:&lt;/P&gt;&lt;P&gt;MACHINE ??= 'imx6ulevk'&lt;/P&gt;&lt;P&gt;DISTRO ?= 'fsl-imx-x11'&lt;/P&gt;&lt;P&gt;PACKAGE_CLASSES ?= "package_rpm"&lt;/P&gt;&lt;P&gt;EXTRA_IMAGE_FEATURES = "debug-tweaks"&lt;/P&gt;&lt;P&gt;USER_CLASSES ?= "buildstats image-mklibs"&lt;/P&gt;&lt;P&gt;PATCHRESOLVE = "noop"&lt;/P&gt;&lt;P&gt;BB_DISKMON_DIRS = "\&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; STOPTASKS,${TMPDIR},1G,100K \&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; STOPTASKS,${DL_DIR},1G,100K \&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; STOPTASKS,${SSTATE_DIR},1G,100K \&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; STOPTASKS,/tmp,100M,100K \&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ABORT,${TMPDIR},100M,1K \&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ABORT,${DL_DIR},100M,1K \&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ABORT,${SSTATE_DIR},100M,1K \&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ABORT,/tmp,10M,1K"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PACKAGECONFIG_append_pn-qemu-native = " sdl"&lt;/P&gt;&lt;P&gt;PACKAGECONFIG_append_pn-nativesdk-qemu = " sdl"&lt;/P&gt;&lt;P&gt;ASSUME_PROVIDED += "libsdl-native"&lt;/P&gt;&lt;P&gt;CONF_VERSION = "1"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;DL_DIR ?= "${BSPDIR}/downloads/"&lt;/P&gt;&lt;P&gt;ACCEPT_FSL_EULA = "1"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Coule you help me to fix this issue??&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Many thanks for your help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 May 2016 10:06:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6ulevk-bitbake-issue/m-p/491963#M78970</guid>
      <dc:creator>andyyang730</dc:creator>
      <dc:date>2016-05-23T10:06:46Z</dc:date>
    </item>
    <item>
      <title>Re: imx6ulevk bitbake issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6ulevk-bitbake-issue/m-p/491964#M78971</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Andy Yang,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Did you resolved your issue?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would recommend using Ubuntu 14.04 if at all possible, as NXP BSP Release dependencies may be different in newer Ubuntu releases. It should be possible to look for the equivalent host packages but I haven’t tried it myself. (The core-image-minimal uses only packages from the Yocto Project, so it is possible that the dependencies for the Yocto Project are met but not for the NXP BSP Release layers)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Other than that I see no errors on your conf file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You may always try using a clean in order to see if that helps, at a last resort.&lt;/P&gt;&lt;P&gt;bitbake -c cleanall fsl-image-qt5&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards, &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Jun 2016 17:01:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6ulevk-bitbake-issue/m-p/491964#M78971</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2016-06-22T17:01:40Z</dc:date>
    </item>
    <item>
      <title>Re: imx6ulevk bitbake issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6ulevk-bitbake-issue/m-p/491965#M78972</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Andy&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The Yocto Project User's Guide specifies that fsl-image-qt5 are not supported on the i.MX 6UltraLite and i.MX 7Dual.&lt;BR /&gt;Hope this help you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Jul 2016 17:19:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6ulevk-bitbake-issue/m-p/491965#M78972</guid>
      <dc:creator>alexishernandez</dc:creator>
      <dc:date>2016-07-01T17:19:02Z</dc:date>
    </item>
    <item>
      <title>Re: imx6ulevk bitbake issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6ulevk-bitbake-issue/m-p/491966#M78973</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Der Gusarambula&lt;/P&gt;&lt;P&gt;yes, I changed to use 14.04, everything is ok now.&lt;/P&gt;&lt;P&gt;thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Sep 2016 02:49:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6ulevk-bitbake-issue/m-p/491966#M78973</guid>
      <dc:creator>andyyang730</dc:creator>
      <dc:date>2016-09-09T02:49:43Z</dc:date>
    </item>
  </channel>
</rss>