<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: I.MX6UL: Which USB-Interface is bootable ?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6UL-Which-USB-Interface-is-bootable/m-p/491897#M78962</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thx! That helps a lot !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 05 Feb 2016 08:42:22 GMT</pubDate>
    <dc:creator>wowa</dc:creator>
    <dc:date>2016-02-05T08:42:22Z</dc:date>
    <item>
      <title>I.MX6UL: Which USB-Interface is bootable ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6UL-Which-USB-Interface-is-bootable/m-p/491895#M78960</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Community, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i am looking after the USB-Interface. I want to boot and flash from the USB. I think this is the best way to debug this device.&lt;/P&gt;&lt;P&gt;Please can anyone tell me which USB-Port (1 or 2) has the highest priority for this task ? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and best regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Feb 2016 07:41:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6UL-Which-USB-Interface-is-bootable/m-p/491895#M78960</guid>
      <dc:creator>wowa</dc:creator>
      <dc:date>2016-02-05T07:41:57Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX6UL: Which USB-Interface is bootable ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6UL-Which-USB-Interface-is-bootable/m-p/491896#M78961</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Walter&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;only USB OTG1 is used according to Figure 8-2. Serial Download Boot Flow&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;i.MX6UL Reference Manual &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6ULRM.pdf" rel="nofollow"&gt;http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6ULRM.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Feb 2016 08:37:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6UL-Which-USB-Interface-is-bootable/m-p/491896#M78961</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-02-05T08:37:10Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX6UL: Which USB-Interface is bootable ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6UL-Which-USB-Interface-is-bootable/m-p/491897#M78962</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thx! That helps a lot !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Feb 2016 08:42:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6UL-Which-USB-Interface-is-bootable/m-p/491897#M78962</guid>
      <dc:creator>wowa</dc:creator>
      <dc:date>2016-02-05T08:42:22Z</dc:date>
    </item>
  </channel>
</rss>