<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How do I use UART? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-do-I-use-UART/m-p/491180#M78822</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I figured out reading the data at least!&amp;nbsp; The baud rate was simply not right.&amp;nbsp; Instead of using 9600, as is the documented default, I had to use 115200.&amp;nbsp; Then I could read the output as it boot!&amp;nbsp; Thank god.&amp;nbsp; There's something at least.&amp;nbsp; I still don;t know if I can have an interactive session though?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 21 May 2016 19:35:46 GMT</pubDate>
    <dc:creator>jonathantaylor</dc:creator>
    <dc:date>2016-05-21T19:35:46Z</dc:date>
    <item>
      <title>How do I use UART?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-do-I-use-UART/m-p/491179#M78821</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I see posts about seeing console output via uart, but don't understand how that works.&amp;nbsp; If I use putty, or hyper terminal (on Windows), I can connect to the device.&amp;nbsp; My PC then receives unreadable garbage on the screen.&amp;nbsp; Now what? The user manual for my board &lt;A href="http://www.nxp.com/files/32bit/doc/user_guide/MX53UG.pdf" title="http://www.nxp.com/files/32bit/doc/user_guide/MX53UG.pdf"&gt;http://www.nxp.com/files/32bit/doc/user_guide/MX53UG.pdf&lt;/A&gt; says to test uart by entering: echo “test” &amp;gt; /dev/ttymxc2 on the device.&amp;nbsp; I assume the result of that should be seeing "test" on my PC?&amp;nbsp; That doesn't happen.&amp;nbsp; Nothing appears to happen in fact.&amp;nbsp; Further, I don't see how I can send a command to the device.&amp;nbsp; I would really love to have a terminal interaction on my PC with the board.&amp;nbsp; Is that possible?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 21 May 2016 16:57:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-do-I-use-UART/m-p/491179#M78821</guid>
      <dc:creator>jonathantaylor</dc:creator>
      <dc:date>2016-05-21T16:57:09Z</dc:date>
    </item>
    <item>
      <title>Re: How do I use UART?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-do-I-use-UART/m-p/491180#M78822</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I figured out reading the data at least!&amp;nbsp; The baud rate was simply not right.&amp;nbsp; Instead of using 9600, as is the documented default, I had to use 115200.&amp;nbsp; Then I could read the output as it boot!&amp;nbsp; Thank god.&amp;nbsp; There's something at least.&amp;nbsp; I still don;t know if I can have an interactive session though?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 21 May 2016 19:35:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-do-I-use-UART/m-p/491180#M78822</guid>
      <dc:creator>jonathantaylor</dc:creator>
      <dc:date>2016-05-21T19:35:46Z</dc:date>
    </item>
  </channel>
</rss>