<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: VPU Timeout causes? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/VPU-Timeout-causes/m-p/490845#M78722</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mark&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;timeout may be caused by vpu performance limits described on p.6&lt;/P&gt;&lt;P&gt;presentation&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-95595"&gt;Q&amp;amp;amp;A: MX6 VPU H.264 Dual Stream Encode Limits&lt;/A&gt; &lt;/P&gt;&lt;P&gt;Depending on system configuration limit may vary.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 08 Apr 2016 10:56:41 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2016-04-08T10:56:41Z</dc:date>
    <item>
      <title>VPU Timeout causes?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/VPU-Timeout-causes/m-p/490844#M78721</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;I am using the VPU to encode 6 streams of NV12, 640x480x30fps video into H.264. I'm using the MX6Q at 800Mhz.&lt;/P&gt;&lt;P&gt;I am occasionally getting "VPU Timeout", this seems to occur more when a USB Flash drive is inserted into the USB port on my device.&amp;nbsp; What can cause the VPU timeout error to occur when encoding H.264? (1250bps).&amp;nbsp; This is using Linux 3.10&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Apr 2016 07:06:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/VPU-Timeout-causes/m-p/490844#M78721</guid>
      <dc:creator>road-iq</dc:creator>
      <dc:date>2016-04-08T07:06:28Z</dc:date>
    </item>
    <item>
      <title>Re: VPU Timeout causes?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/VPU-Timeout-causes/m-p/490845#M78722</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mark&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;timeout may be caused by vpu performance limits described on p.6&lt;/P&gt;&lt;P&gt;presentation&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-95595"&gt;Q&amp;amp;amp;A: MX6 VPU H.264 Dual Stream Encode Limits&lt;/A&gt; &lt;/P&gt;&lt;P&gt;Depending on system configuration limit may vary.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Apr 2016 10:56:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/VPU-Timeout-causes/m-p/490845#M78722</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-04-08T10:56:41Z</dc:date>
    </item>
    <item>
      <title>Re: VPU Timeout causes?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/VPU-Timeout-causes/m-p/490846#M78723</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;So, per that presentation, I should not be having a problem.&amp;nbsp; I am running the VPU at 352Mhz, I am running 6 streams at 30fps, 640x480 resolution.&amp;nbsp; There should be ample headroom..&amp;nbsp; My encoder parameters are: "gop_size": 0, "bit_rate": 1250, "quant": 23.&amp;nbsp; Horz = 640, Vert = 480, fps = 30.&amp;nbsp; Everything else is default.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Interesting note: I've been tinkering with the MMDC arbitration priorities for VPU, IPU and PCIe (where our video frames come in).&amp;nbsp; I set their priorities as follows:&lt;/P&gt;&lt;P&gt;# first set PCIe write priority so that TW6869 can get its data to RAM. Highest Priority&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; devmem 0xC4A104 32 0x0000000F&lt;BR /&gt;# next set VPU write priorities. Third Highest Priority&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; devmem 0xC49104 32 0x00000006&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; devmem 0x844104 32 0x00000006&lt;BR /&gt;# finally set IPU1 &amp;amp; IPU2. Second Highest Priority.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; devmem 0x20e0018 32 0x77777777&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; devmem 0x20e001C 32 0x77777777&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've left the default read priorities as default (2) for VPU and PCIe. Changing the read priorities to make write make the failure occur more frequently.&amp;nbsp; Setting all priorities equal causes the problem to occur more frequently.&lt;/P&gt;&lt;P&gt;My memory bus load is at 82%&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Apr 2016 17:17:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/VPU-Timeout-causes/m-p/490846#M78723</guid>
      <dc:creator>road-iq</dc:creator>
      <dc:date>2016-04-08T17:17:38Z</dc:date>
    </item>
    <item>
      <title>Re: VPU Timeout causes?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/VPU-Timeout-causes/m-p/490847#M78724</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;figures given in presentation are for OSless case (baremetal).&lt;/P&gt;&lt;P&gt;memory bus load&amp;nbsp; 82% is heavy loaded bus, please try to diminish it.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 09 Apr 2016 03:47:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/VPU-Timeout-causes/m-p/490847#M78724</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-04-09T03:47:00Z</dc:date>
    </item>
    <item>
      <title>Re: VPU Timeout causes?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/VPU-Timeout-causes/m-p/490848#M78725</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Not possible to reduce memory bus load short of upgrading to iMX6Q+.&amp;nbsp; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 23 Apr 2016 19:50:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/VPU-Timeout-causes/m-p/490848#M78725</guid>
      <dc:creator>road-iq</dc:creator>
      <dc:date>2016-04-23T19:50:49Z</dc:date>
    </item>
    <item>
      <title>Re: VPU Timeout causes?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/VPU-Timeout-causes/m-p/490849#M78726</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;please check that ahb and ipg clocks are running at max. values&lt;/P&gt;&lt;P&gt;also one can tweak GPV QoS in Table 45-5. QoS and tidemark parameters&lt;/P&gt;&lt;P&gt;i.MX6DQ RM, IOMUXC_GPR6,7. Try to increase cma size.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 24 Apr 2016 00:22:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/VPU-Timeout-causes/m-p/490849#M78726</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-04-24T00:22:32Z</dc:date>
    </item>
  </channel>
</rss>